Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages

In this section you can find all the projects related to the USB Device Interface (UDI) for Personal Healthcare.

Example(s)

USB Device CDC Example for ATxmega128a1u on STK600

Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface.

USB Device CDC Example for ATxmega128a4u on STK600

Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface.

USB Device CDC Example for ATxmega256a3bu on STK600

Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface.

USB Device CDC Example for ATxmega32a4u on STK600

Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface.

USB Device CDC Example for XMEGA-A1U Xplained Pro

Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface.

USB Device CDC Example for XMEGA-A3BU Xplained

Provide an application example of USB Communication Device Class (CDC) implementation: a bridge between USART and USB CDC interface.

USB Device HID Generic for ATxmega32a4u on STK600

Provide an application example of USB Device HID Generic implementation. Relies on the native HID driver and uses buttons and LEDs available on the board.

USB Device HID Keyboard for ATxmega128a1u on STK600

Provide an application example of USB Device HID Keyboard implementation. Relies on the native HID driver and uses buttons available on the board as a keyboard interfaces.

USB Device HID Keyboard for ATxmega128a4u on STK600

Provide an application example of USB Device HID Keyboard implementation. Relies on the native HID driver and uses buttons available on the board as a keyboard interfaces.

USB Device HID Keyboard for ATxmega256a3bu on STK600

Provide an application example of USB Device HID Keyboard implementation. Relies on the native HID driver and uses buttons available on the board as a keyboard interfaces.

USB Device HID Keyboard for ATxmega32a4u on STK600

Provide an application example of USB Device HID Keyboard implementation. Relies on the native HID driver and uses buttons available on the board as a keyboard interfaces.

USB Device HID Keyboard for XMEGA-A3BU Xplained

Provide an application example of USB Device HID Keyboard implementation. Relies on the native HID driver and uses buttons available on the board as a keyboard interfaces.

USB Device HID Mouse for ATxmega128a1u on STK600

Provide an application example of USB Device HID Mouse implementation. Relies on the native HID driver and uses buttons available on the board as a mouse interfaces.

USB Device HID Mouse for ATxmega128a4u on STK600

Provide an application example of USB Device HID Mouse implementation. Relies on the native HID driver and uses buttons available on the board as a mouse interfaces.

USB Device HID Mouse for ATxmega256a3bu on STK600

Provide an application example of USB Device HID Mouse implementation. Relies on the native HID driver and uses buttons available on the board as a mouse interfaces.

USB Device HID Mouse for ATxmega32a4u on STK600

Provide an application example of USB Device HID Mouse implementation. Relies on the native HID driver and uses buttons available on the board as a mouse interfaces.

USB Device HID Mouse for XMEGA-A3BU Xplained

Provide an application example of USB Device HID Mouse implementation. Relies on the native HID driver and uses buttons available on the board as a mouse interfaces.

USB Device Mass Storage for ATxmega128a1u on STK600

Provide an application example of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98).

USB Device Mass Storage for ATxmega128a4u on STK600

Provide an application example of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98).

USB Device Mass Storage for ATxmega256a3bu on STK600

Provide an application example of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98).

USB Device Mass Storage for ATxmega32a4u on STK600

Provide an application example of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98).

USB Device Mass Storage for XMEGA-A3BU Xplained

Provide an application example of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98).

USB Device PHDC for XMEGA-A3BU Xplained

Provide an application example of USB Device PHDC implementation. Relies on the PHDC driver and uses buttons available on the board as a sensor interfaces.

USB Device Vendor Class example for ATxmega256a3bu on STK600

Provide an application example of USB Vendor Class implementation. The example implements a look back application between IN and OUT enpoints of interrupt, bulk and isochronous types. Note that this example relies on a specific driver on the Host Operating System. For more detail documentation and PC drivers and application, please refer to AVR4001 application note.

USB Device Vendor Class example for ATxmega32a4u on STK600

Provide an application example of USB Vendor Class implementation. The example implements a look back application between IN and OUT enpoints of interrupt, bulk and isochronous types. Note that this example relies on a specific driver on the Host Operating System. For more detail documentation and PC drivers and application, please refer to AVR4001 application note.

USB Device Vendor Class example for XMEGA-A3BU Xplained

Provide an application example of USB Vendor Class implementation. The example implements a look back application between IN and OUT enpoints of interrupt, bulk and isochronous types. Note that this example relies on a specific driver on the Host Operating System. For more detail documentation and PC drivers and application, please refer to AVR4001 application note.

USB QTouch Device HID Generic Example for ATxmega256A3BU on XMEGA-A3BU Xplained

Provide an application example of USB Device HID Generic implementation that uses QTouch key. Relies on the native HID driver and uses buttons and LEDs available on the board.

Unit-test(s)

USB Device CDC unit tests for ATxmega128a1u on STK600

Provide an unit test of USB Device CDC implementation.

USB Device CDC unit tests for ATxmega32a4u on STK600

Provide an unit test of USB Device CDC implementation.

USB Device CDC unit tests for XMEGA-A3BU Xplained

Provide an unit test of USB Device CDC implementation.

USB Device HID Mouse unit tests for ATxmega128a1u on STK600

Provide an unit test of USB Device HID keyboard implementation.

USB Device HID Mouse unit tests for ATxmega128a1u on STK600

Provide an unit test of USB Device HID Mouse implementation.

USB Device HID Mouse unit tests for ATxmega256a3bu on STK600

Provide an unit test of USB Device HID Mouse implementation.

USB Device HID Mouse unit tests for ATxmega32a4u on STK600

Provide an unit test of USB Device HID keyboard implementation.

USB Device HID Mouse unit tests for ATxmega32a4u on STK600

Provide an unit test of USB Device HID Mouse implementation.

USB Device HID Mouse unit tests for XMEGA-A3BU Xplained

Provide an unit test of USB Device HID keyboard implementation.

USB Device HID Mouse unit tests for XMEGA-A3BU Xplained

Provide an unit test of USB Device HID Mouse implementation.

USB Device Mass Storage unit tests for ATxmega128a1u on STK600

Provide a unit test of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98).

USB Device Mass Storage unit tests for ATxmega128a4u on STK600

Provide a unit test of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98).

USB Device Mass Storage unit tests for XMEGA-A3BU Xplained

Provide a unit test of USB Device Mass Storage implementation. Relies on the native MSC driver on OS*, displays all available memories of the board as removable disk* (*except for Windows 98).