Settings for the interrupt monitor.
Macros | |
#define | CLASSB_STRICT_INTMON |
Behavior for re-enabling or re-disabling monitoring of interrupts. More... | |
Enumerations | |
enum | classb_int_identifiers { TEMP_SANITY_TEST, PER_CLASSB_TESTS, N_INTERRUPTS } |
Enumeration of interrupt identifiers. More... | |
#define CLASSB_STRICT_INTMON |
Behavior for re-enabling or re-disabling monitoring of interrupts.
If this is defined, enabling an interrupt that is in ON
state or disabling an interrupt that is in OFF
state will call the error handler.
Enumeration of interrupt identifiers.
This enumeration holds the identifiers for the interrupts that should be monitored. These identifiers are used in the interrupt when calling functions related to the interrupt monitor: classb_intmon_reg_int(), classb_intmon_increase() and classb_intmon_set_state(). Interrupt identifiers are included before N_INTERRUPTS, so that it will hold the total number of registered interrupts.
Enumerator | |
---|---|
TEMP_SANITY_TEST | |
PER_CLASSB_TESTS | |
N_INTERRUPTS |
Number of registered interrupts. |