This is a driver for the AVR XMEGA Quadrature Decoder module (QDEC).
It provides functions for enabling, disabling and configuring the QDEC module.
See Quick Start Guide for the XMEGA QDEC Driver
Modules | |
Quick Start Guide(s) | |
In this section you can find a list of all Quick Start guides related to the XMEGA Quadrature Decoder (QDEC). | |
Data Structures | |
struct | qdec_config |
Typedefs | |
typedef struct qdec_config | qdec_config_t |
Enumerations | |
enum | QDec_index_rec_state { QDEC_STATE_NO_PH0_NO_PH90 = (0x00 << 0), QDEC_STATE_NO_PH0_PH90 = (0x01 << 0), QDEC_STATE_PH0_NO_PH90 = (0x02 << 0), QDEC_STATE_PH0_PH90 = (0x03 << 0) } |
Functions | |
void | qdec_config_disable_index_pin (qdec_config_t *config) |
Disables index line. More... | |
void | qdec_config_enable_freq (qdec_config_t *config, uint32_t unit) |
Defines frequency option. More... | |
void | qdec_config_enable_index_pin (qdec_config_t *config, bool pin_invert, enum QDec_index_rec_state state) |
Defines index line to enable the automaticaly position reset. More... | |
void | qdec_config_event_channel (qdec_config_t *config, uint8_t event_channel) |
Selects the event channel to use for quadrature decoder. More... | |
void | qdec_config_freq_event_channel (qdec_config_t *config, uint8_t event_channel) |
Selects the event channel to use for frequency quadrature decoder. More... | |
void | qdec_config_freq_tc (qdec_config_t *config, volatile void *timer) |
Selects the event channel to use for frequency quadrature decoder. More... | |
void | qdec_config_phase_pins (qdec_config_t *config, PORT_t *port, uint8_t pins_base, bool pins_invert, uint16_t filter_us) |
This function set up the needed configuration to the port, used for the quadrature decoding. More... | |
void | qdec_config_revolution (qdec_config_t *config, uint16_t revolution) |
Defines the revolution of quadrature decoder. More... | |
void | qdec_config_tc (qdec_config_t *config, volatile void *timer) |
Selects the event channel to use for quadrature decoder. More... | |
void | qdec_enabled (qdec_config_t *config) |
Loads and enables QDec system. More... | |
void | qdec_get_config_defaults (qdec_config_t *config) |
This function initializes the configuration structure with the identified as commonly use case. More... | |
bool | qdec_get_direction (qdec_config_t *config) |
Returns the direction of the quadrature decoding counter. More... | |
uint16_t | qdec_get_frequency (qdec_config_t *config) |
Returns the frequency of quadrature encoder. More... | |
uint16_t | qdec_get_position (qdec_config_t *config) |
Returns the position of quadrature encoder. More... | |
void | qdec_reset_position (qdec_config_t *config) |
Returns the position of quadrature encoder. More... | |
typedef struct qdec_config qdec_config_t |
Quadrature encoder configuration structure
enum QDec_index_rec_state |
void qdec_config_disable_index_pin | ( | qdec_config_t * | config | ) |
Disables index line.
config | Handle on a QDec configuration structure |
References qdec_config::enabled, and qdec_config::index.
void qdec_config_enable_freq | ( | qdec_config_t * | config, |
uint32_t | unit | ||
) |
Defines frequency option.
This option allows to compute automaticaly through an event and timer the frequency rotation. The system will be configurated with a resolution at least as high as the one specified. The resolution of a TC is synonymous with its clock frequency.
config | Handle on a QDec configuration structure |
unit | Desired unit used by qdec_get_frequency() in mHz. |
References qdec_config::enabled, qdec_config::freq_opt, and qdec_config::unit.
void qdec_config_enable_index_pin | ( | qdec_config_t * | config, |
bool | pin_invert, | ||
enum QDec_index_rec_state | state | ||
) |
Defines index line to enable the automaticaly position reset.
config | Handle on a QDec configuration structure |
pin_invert | True if IO pins should be inverted |
state | Recognition states of index pin |
References qdec_config::enabled, qdec_config::index, qdec_config::pin_invert, qdec_config::rec_state, and state.
void qdec_config_event_channel | ( | qdec_config_t * | config, |
uint8_t | event_channel | ||
) |
Selects the event channel to use for quadrature decoder.
config | Handle on a QDec configuration structure |
event_channel | Which event channel to use for quadrature decoder XMEGA B, E authorizes channel 0. XMEGA D authorizes channel 0, 2. XMEGA A, C authorizes channel 0, 2, 4. |
References qdec_config::event_channel.
void qdec_config_freq_event_channel | ( | qdec_config_t * | config, |
uint8_t | event_channel | ||
) |
Selects the event channel to use for frequency quadrature decoder.
config | Handle on a QDec configuration structure |
event_channel | Which event channel to use for frequency QDec XMEGA B, E authorizes channel 0. XMEGA D authorizes channel 0, 2. XMEGA A, C authorizes channel 0, 2, 4. Note: If |
References qdec_config::event_channel, and qdec_config::freq_opt.
void qdec_config_freq_tc | ( | qdec_config_t * | config, |
volatile void * | timer | ||
) |
Selects the event channel to use for frequency quadrature decoder.
config | Handle on a QDec configuration structure |
timer | Pointer to timer module used for frequency QDec XMEGA E authorizes &TC4 or &TC5. other XMEGA authorizes &TC0, ... |
References qdec_config::freq_opt, and qdec_config::timer.
void qdec_config_phase_pins | ( | qdec_config_t * | config, |
PORT_t * | port, | ||
uint8_t | pins_base, | ||
bool | pins_invert, | ||
uint16_t | filter_us | ||
) |
This function set up the needed configuration to the port, used for the quadrature decoding.
config | Handle on a QDec configuration structure |
port | Pointer to PORT module, which is used for quadrature |
pins_base | First pin number to be used for QDPH0 input from port pins_base+1 for QDPH90 and pins_base+2 for QDINDX |
pins_invert | True if IO pins should be inverted |
filter_us | Pin stable timing requested to validate level |
References qdec_config::phases, qdec_config::pins_base, qdec_config::pins_filter_us, qdec_config::pins_invert, and qdec_config::port.
void qdec_config_revolution | ( | qdec_config_t * | config, |
uint16_t | revolution | ||
) |
Defines the revolution of quadrature decoder.
config | Handle on a QDec configuration structure |
revolution | Number of position for a revolution |
References Assert, and qdec_config::revolution.
void qdec_config_tc | ( | qdec_config_t * | config, |
volatile void * | timer | ||
) |
Selects the event channel to use for quadrature decoder.
config | Handle on a QDec configuration structure |
timer | Pointer to timer module used for Quadrature decoding XMEGA E authorizes &TC4 or &TC5. other XMEGA authorizes &TC0, ... |
References qdec_config::timer.
void qdec_enabled | ( | qdec_config_t * | config | ) |
Loads and enables QDec system.
config | Handle on a QDec configuration structure |
References Assert, qdec_config::enabled, qdec_config::event_channel, qdec_config::freq_opt, qdec_config::port, qdec_enabled_evsys(), qdec_enabled_pins(), qdec_enabled_tc(), qdec_enabled_tc_freq(), and qdec_config::rotary.
void qdec_get_config_defaults | ( | qdec_config_t * | config | ) |
This function initializes the configuration structure with the identified as commonly use case.
config | Handle on a QDec configuration structure |
References qdec_config::enabled, qdec_config::event_channel, qdec_config::freq_opt, qdec_config::index, qdec_config::phases, qdec_config::pins_base, qdec_config::pins_filter_us, qdec_config::pins_invert, qdec_config::port, qdec_config::revolution, qdec_config::rotary, qdec_config::timer, and qdec_config::unit.
bool qdec_get_direction | ( | qdec_config_t * | config | ) |
Returns the direction of the quadrature decoding counter.
config | Handle on a QDec configuration structure |
References qdec_config::timer.
uint16_t qdec_get_frequency | ( | qdec_config_t * | config | ) |
Returns the frequency of quadrature encoder.
config | Handle on a QDec configuration structure |
References qdec_config::coef, qdec_config::freq_opt, qdec_config::last_freq, TC_CCA, tc_is_cc_interrupt(), tc_read_cc(), and qdec_config::timer.
uint16_t qdec_get_position | ( | qdec_config_t * | config | ) |
Returns the position of quadrature encoder.
config | Handle on a QDec configuration structure |
Note: The origin position is reseted:
References tc_read_count(), and qdec_config::timer.
void qdec_reset_position | ( | qdec_config_t * | config | ) |
Returns the position of quadrature encoder.
config | Handle on a QDec configuration structure |
References tc_write_count(), and qdec_config::timer.