Class B Oven settings.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | oven_wdt_periodic_reset() |
Reset the WDT when OVEN_WDT_RESET_PERIOD has passed. More... | |
Timing configurations | |
#define | OVEN_WDT_RESET_PERIOD 1250 |
Number of RTC ticks between WDT resets. More... | |
#define | OVEN_SIM_STEP_TIME 100 |
How often a simulation step should be executed [ms]. More... | |
#define | OVEN_CTL_STEP_TIME 20 |
How often a control step should be executed [ms]. More... | |
Simulation control signal timers selection | |
#define | OVEN_FREQ_TC TCC0 |
Timer used to output frequency signal controlling the induction element. More... | |
#define | FREQ_TIMER_PERIOD_INIT 0x100 |
Initial period for the frequency timer. More... | |
#define | OVEN_FREQ_CAPT_TC TCC1 |
Timer used to capture the generated frequency signal. More... | |
Test timer selection | |
#define | CLASSB_FREQTEST_TC TCD1 |
Timer used by the Class B frequency consistency test of the CPU clock. More... | |
#define | OVEN_PERIODIC_TEMPTEST_TC TCE1 |
Timer used to execute periodic temperature sanity test. More... | |
#define | OVEN_PERIODIC_CLASSB_TC TCE0 |
Timer used to execute periodic Class B tests. More... | |
Display configuration | |
#define | OVEN_PLOT_OFFSET_X 5 |
X offset for the plot window. More... | |
#define | OVEN_PLOT_MAX_X 112 |
Rightmost X coordinate of the plot window. More... | |
#define | OVEN_PLOT_MAX_Y 29 |
Lowest Y coordinate in the plot window. More... | |
#define | OVEN_PLOT_MIN_Y 0 |
Topmost Y coordinate in the plot window. More... | |
#define | OVEN_DISP_MAX_Y 32 |
Display height. More... | |
#define | MAX_WATTAGE 15 |
Maximum watt level. More... | |
Enumerations | |
Oven state enumerations | |
enum | ovenctl_plate_state { POWER_OFF, ON_NO_POT, ON_ACTUATING } |
Current state of the oven. More... | |
enum | status_led { S_ORANGE, S_GREEN, S_RED, S_OFF } |
Status LED color enumerations. More... | |
enum | pot_t { POT_OFF, POT_ON } |
Pot status on or off plate enumeration. More... | |
Functions | |
void | main_init_adc_dac (void) |
Initialize ADC and DAC used to simulate a temperature sensor. More... | |
void | main_init_tc (void) |
Initialize Timer/Counters used to simulate oven actuation signal. More... | |
Variables | |
volatile uint32_t | classb_last_wdt_reset |
Global container for last WDT reset time. More... | |
#define CLASSB_FREQTEST_TC TCD1 |
Timer used by the Class B frequency consistency test of the CPU clock.
Referenced by oven_classb_init_tests().
#define FREQ_TIMER_PERIOD_INIT 0x100 |
Initial period for the frequency timer.
Referenced by main_init_tc().
#define MAX_WATTAGE 15 |
Maximum watt level.
Referenced by oven_ui_update_graphics().
#define OVEN_CTL_STEP_TIME 20 |
How often a control step should be executed [ms].
Referenced by main().
#define OVEN_DISP_MAX_Y 32 |
Display height.
Referenced by oven_ui_draw_plot_step().
#define OVEN_FREQ_CAPT_TC TCC1 |
Timer used to capture the generated frequency signal.
Referenced by main_init_tc(), and oven_plant_read_signal_period().
#define OVEN_FREQ_TC TCC0 |
Timer used to output frequency signal controlling the induction element.
Referenced by main_init_tc(), and ovenctl_actuate_induction_element().
#define OVEN_PERIODIC_CLASSB_TC TCE0 |
Timer used to execute periodic Class B tests.
Referenced by main(), ovenctl_turn_off_plate(), and ovenctl_turn_on_plate().
#define OVEN_PERIODIC_TEMPTEST_TC TCE1 |
Timer used to execute periodic temperature sanity test.
Referenced by main(), oven_classb_error_insertion(), ovenctl_turn_off_plate(), and ovenctl_turn_on_plate().
#define OVEN_PLOT_MAX_X 112 |
Rightmost X coordinate of the plot window.
Referenced by oven_ui_draw_plot_step().
#define OVEN_PLOT_MAX_Y 29 |
Lowest Y coordinate in the plot window.
Referenced by oven_ui_draw_plot_step().
#define OVEN_PLOT_MIN_Y 0 |
Topmost Y coordinate in the plot window.
Referenced by oven_ui_draw_plot_step().
#define OVEN_PLOT_OFFSET_X 5 |
X offset for the plot window.
Referenced by oven_ui_draw_plot_step().
#define OVEN_SIM_STEP_TIME 100 |
How often a simulation step should be executed [ms].
Referenced by main().
#define oven_wdt_periodic_reset | ( | ) |
Reset the WDT when OVEN_WDT_RESET_PERIOD has passed.
This macro depends on the ASF RTC driver and that the timer is running because it is used to get correct timing of watchdog resets in windowed mode.
Referenced by main(), oven_classb_error_insertion(), oven_classb_flash_corrupter(), show_button_splash(), and show_explain_splash().
#define OVEN_WDT_RESET_PERIOD 1250 |
Number of RTC ticks between WDT resets.
Should be in the middle of the open window period of the WDT, e.g. at 625 ticks if WPER is 500CLK and PER is 250CLK.
enum ovenctl_plate_state |
enum pot_t |
enum status_led |
void main_init_adc_dac | ( | void | ) |
Initialize ADC and DAC used to simulate a temperature sensor.
DACB is used by the simulation plant to output a temperature reading of the oven plate. It is set up to output a voltage on pin B2 which is marked as ADC2 on header J2.
ADCA is used in the control step and graphical interface to show the current temperature of the oven plate. It is set up to read a voltage on pin A4 which is marked as ADC4 on header J2.
ADC2 and ADC4 should be connected together, so that the ADC samples the DAC directly.
References ADC_CH0, adc_enable(), adc_read_configuration(), ADC_REF_BANDGAP, ADC_RES_12, adc_set_clock_rate(), adc_set_conversion_parameters(), adc_set_conversion_trigger(), ADC_SIGN_ON, adc_start_conversion(), ADC_TRIG_MANUAL, adc_write_configuration(), ADCCH_NEG_NONE, ADCCH_POS_PIN4, adcch_read_configuration(), adcch_set_input(), adcch_write_configuration(), DAC_ADJ_RIGHT, DAC_CH0, dac_enable(), dac_read_configuration(), DAC_REF_BANDGAP, dac_set_active_channel(), dac_set_conversion_parameters(), dac_write_configuration(), IOPORT_DIR_INPUT, IOPORT_MODE_PULLDOWN, ioport_set_pin_dir(), and ioport_set_pin_mode().
Referenced by main(), and ovenctl_turn_on_plate().
void main_init_tc | ( | void | ) |
Initialize Timer/Counters used to simulate oven actuation signal.
TCC0 is set up to generate a dual variable frequency signal with dead-time insertion using the AWEX module. This is similar to how heating elements are actuated in real induction ovens. Its output is on pin C2 which is marked as RXD on header J1.
TCC1 is set up to capture a frequency signal via a pin change event using the XMEGA Event System. Its input is pin C4 which is marked as SS on header J1.
References FREQ_TIMER_PERIOD_INIT, IOPORT_BOTHEDGES, ioport_configure_pin(), IOPORT_DIR_INPUT, IOPORT_DIR_OUTPUT, OVEN_FREQ_CAPT_TC, OVEN_FREQ_TC, tc_awex_enable_ccb_deadtime(), tc_awex_set_dti_high(), tc_awex_set_dti_low(), tc_awex_set_output_override(), TC_CCA, TC_CCAEN, tc_enable(), tc_enable_cc_channels(), TC_EVACT_FRQ_gc, tc_set_input_capture(), tc_set_wgm(), TC_WG_FRQ, tc_write_cc(), and tc_write_clock_source().
Referenced by main(), and ovenctl_turn_on_plate().
volatile uint32_t classb_last_wdt_reset |
Global container for last WDT reset time.
Global container for last WDT reset time.
Referenced by main(), and main_init_rtc32().