User interface for mXT143E Xplained trackpad demo.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | trace_info |
Information for one trace point. More... | |
Macros | |
Touch trace settings | |
#define | TRACE_RECT_SIZE 10 |
Size (width/height) of trace-rectangle. More... | |
#define | NUM_TRACES 150 |
Number of rectangles in the touch trace. More... | |
Functions | |
static void | draw_frame (const uint8_t start, const uint8_t thickness, const gfx_color_t color) |
Draw a frame. More... | |
static void | handle_trace (gfx_coord_t x, gfx_coord_t y) |
Handle finger traces on display. More... | |
void | ui_init (void) |
Initialize the user interface. More... | |
void | ui_powerdown (void) |
Put the user interface in power down. More... | |
void | ui_process (uint16_t framenumber) |
Process the user interface. More... | |
void | ui_wakeup (void) |
Wake the user interface up. More... | |
void | ui_wakeup_disable (void) |
Disable asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enable asynchronous interrupts of the user interface. More... | |
Variables | |
static struct trace_info | trace [NUM_TRACES] |
Array to hold all trace points. More... | |
bool | ui_new_touch_event |
Flag that a new touch event is pending. More... | |
struct mxt_touch_event | ui_touch_event |
Struct to hold touch events to process. More... | |
Display size containers | |
To avoid fetching the display size multiple times from the graphics service, store them in these two variables upon initialization. | |
static uint16_t | display_w |
Display width. More... | |
static uint16_t | display_h |
Display height. More... | |
#define NUM_TRACES 150 |
Number of rectangles in the touch trace.
Referenced by handle_trace(), and ui_init().
#define TRACE_RECT_SIZE 10 |
Size (width/height) of trace-rectangle.
Referenced by handle_trace().
|
static |
Draw a frame.
This function draws a frame with the specified thickness and color on the display, at the specified start offset from the edges.
start | Start offset (x and y, from 0) of frame |
thickness | Thickness (in pixels) of frame |
color | Color of frame |
References display_h, display_w, and gfx_draw_rect.
Referenced by ui_process().
|
static |
Handle finger traces on display.
This function updates the traces, drawing a new one at the specified coordinates and clearing the oldest one. It must be called at regular intervals to give a smooth trace animation.
x | X-coordinate of finger touch |
y | Y-coordinate of finger touch |
References display_h, display_w, GFX_COLOR_WHITE, gfx_draw_rect, max, min, NUM_TRACES, trace, TRACE_RECT_SIZE, trace_info::x, and trace_info::y.
Referenced by ui_process().
void ui_init | ( | void | ) |
Initialize the user interface.
Initializes the user interface.
References display_h, display_w, gfx_get_height(), gfx_get_width(), NUM_TRACES, trace, ui_new_touch_event, trace_info::x, and trace_info::y.
Referenced by main().
void ui_powerdown | ( | void | ) |
Put the user interface in power down.
Enters the user interface in power down mode.
Referenced by main(), main_hid_set_feature(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
Process the user interface.
This process is called each 1ms It is called only if the USB interface is enabled.
This function processes user touch events and updates the display.
The first registered touch is used to control the cursor. Its presence is indicated with a red frame around the display. When the cursor touch moves, its movement is visualized with a trace on the display.
The second registered touch is used to control mouse buttons, and is indicated with an inner frame of which the color depends on which side the touch is for: blue for left and green for right button click. The frame is shown until the touch is released. To detect which side click it is, the position relative to the cursor touch is used, i.e., a touch to the left of the first touch will cause a left mouse click.
framenumber | Current USB frame number |
References draw_frame(), GFX_COLOR_BLUE, GFX_COLOR_GREEN, GFX_COLOR_RED, handle_trace(), HID_MOUSE_BTN_DOWN, HID_MOUSE_BTN_UP, mxt_touch_event::id, MXT_DETECT_EVENT, MXT_PRESS_EVENT, MXT_RELEASE_EVENT, mxt_touch_event::status, udi_hid_mouse_btnleft(), udi_hid_mouse_btnright(), udi_hid_mouse_moveX(), udi_hid_mouse_moveY(), ui_new_touch_event, ui_touch_event, mxt_touch_event::x, and mxt_touch_event::y.
Referenced by main(), and main_sof_action().
void ui_wakeup | ( | void | ) |
Wake the user interface up.
Exits the user interface of power down mode.
Referenced by main_resume_action().
void ui_wakeup_disable | ( | void | ) |
Disable asynchronous interrupts of the user interface.
Disables the asynchronous interrupts of the user interface.
Referenced by main_remotewakeup_disable().
void ui_wakeup_enable | ( | void | ) |
Enable asynchronous interrupts of the user interface.
Enables the asynchronous interrupts of the user interface.
Referenced by main_remotewakeup_enable().
|
static |
Display height.
Referenced by draw_frame(), handle_trace(), and ui_init().
|
static |
Display width.
Referenced by draw_frame(), handle_trace(), and ui_init().
|
static |
Array to hold all trace points.
Referenced by handle_trace(), and ui_init().
bool ui_new_touch_event |
Flag that a new touch event is pending.
Referenced by ui_flag_new_touch_event(), ui_init(), and ui_process().
struct mxt_touch_event ui_touch_event |
Struct to hold touch events to process.
Referenced by main(), and ui_process().