INTC software driver for AVR UC3 devices.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | DECL_INT_LINE_HANDLER_TABLE(GRP, unused) |
Table of interrupt line handlers per interrupt group in order to optimize RAM space. Each line handler table contains a set of pointers to interrupt handlers. More... | |
#define | INSERT_INT_LINE_HANDLER_TABLE(GRP, unused) {AVR32_INTC_NUM_IRQS_PER_GRP##GRP, _int_line_handler_table_##GRP}, |
#define | IPR_INT0 |
Values to store in the interrupt priority registers for the various interrupt priority levels. More... | |
#define | IPR_INT1 |
#define | IPR_INT2 |
#define | IPR_INT3 |
Functions | |
__int_handler | _get_interrupt_handler (uint32_t int_level) |
Gets the interrupt handler of the current event at the int_level interrupt priority level (called from exception.S). More... | |
static void | _unhandled_interrupt (void) |
Default interrupt handler. More... | |
static __inline__ void | INTC_init_evba (void) |
Init EVBA address. This operation may or may not have been done by the C startup process. More... | |
void | INTC_init_interrupts (void) |
Initializes the hardware interrupt controller driver. More... | |
void | INTC_register_interrupt (__int_handler handler, uint32_t irq, uint32_t int_level) |
Registers an interrupt handler. More... | |
MREPEAT (AVR32_INTC_NUM_INT_GRPS, DECL_INT_LINE_HANDLER_TABLE,~) | |
Variables | |
void | _evba |
Import the _evba symbol from exception.S. More... | |
void | _int0 |
Import the symbols _int0, _int1, _int2, _int3 defined in exception.S. More... | |
void | _int1 |
void | _int2 |
void | _int3 |
struct { | |
volatile __int_handler * _int_line_handler_table | |
unsigned int num_irqs | |
} | _int_handler_table [AVR32_INTC_NUM_INT_GRPS] |
Table containing for each interrupt group the number of interrupt request lines and a pointer to the table of interrupt line handlers. More... | |
#define DECL_INT_LINE_HANDLER_TABLE | ( | GRP, | |
unused | |||
) |
Table of interrupt line handlers per interrupt group in order to optimize RAM space. Each line handler table contains a set of pointers to interrupt handlers.
#define INSERT_INT_LINE_HANDLER_TABLE | ( | GRP, | |
unused | |||
) | {AVR32_INTC_NUM_IRQS_PER_GRP##GRP, _int_line_handler_table_##GRP}, |
#define IPR_INT0 |
Values to store in the interrupt priority registers for the various interrupt priority levels.
Referenced by INTC_init_interrupts(), and INTC_register_interrupt().
#define IPR_INT1 |
Referenced by INTC_register_interrupt().
#define IPR_INT2 |
Referenced by INTC_register_interrupt().
#define IPR_INT3 |
Referenced by INTC_register_interrupt().
__int_handler _get_interrupt_handler | ( | uint32_t | int_level | ) |
Gets the interrupt handler of the current event at the int_level interrupt priority level (called from exception.S).
int_level | Interrupt priority level to handle. |
References _int_handler_table, and clz.
|
static |
Default interrupt handler.
Referenced by INTC_init_interrupts().
|
static |
Init EVBA address. This operation may or may not have been done by the C startup process.
References _evba, and Set_system_register.
Referenced by INTC_init_interrupts().
MREPEAT | ( | AVR32_INTC_NUM_INT_GRPS | , |
DECL_INT_LINE_HANDLER_TABLE | , | ||
~ | |||
) |
Referenced by at45dbx_resources_init().
void _evba |
Import the _evba symbol from exception.S.
Referenced by init_exceptions(), and INTC_init_evba().
void _int0 |
Import the symbols _int0, _int1, _int2, _int3 defined in exception.S.
void _int1 |
void _int2 |
void _int3 |
struct { ... } _int_handler_table[AVR32_INTC_NUM_INT_GRPS] |
Table containing for each interrupt group the number of interrupt request lines and a pointer to the table of interrupt line handlers.
Referenced by _get_interrupt_handler(), INTC_init_interrupts(), and INTC_register_interrupt().
volatile __int_handler* _int_line_handler_table |
unsigned int num_irqs |