ICMP - Internet Control Message Protocol.
#include "lwip/opt.h"
#include "lwip/icmp.h"
#include "lwip/inet_chksum.h"
#include "lwip/ip.h"
#include "lwip/def.h"
#include "lwip/stats.h"
#include "lwip/snmp.h"
#include <string.h>
Macros | |
#define | ICMP_DEST_UNREACH_DATASIZE 8 |
#define | LWIP_ICMP_ECHO_CHECK_INPUT_PBUF_LEN 1 |
Small optimization: set to 0 if incoming PBUF_POOL pbuf always can be used to modify and send a response packet (and to 1 if this is not the case, e.g. More... | |
Functions | |
void | icmp_dest_unreach (struct pbuf *p, enum icmp_dur_type t) |
Send an icmp 'destination unreachable' packet, called from ip_input() if the transport layer protocol is unknown and from udp_input() if the local port is not bound. More... | |
void | icmp_input (struct pbuf *p, struct netif *inp) |
Processes ICMP input packets, called from ip_input(). More... | |
static void | icmp_send_response (struct pbuf *p, u8_t type, u8_t code) |
Send an icmp packet in response to an incoming packet. More... | |
#define ICMP_DEST_UNREACH_DATASIZE 8 |
Referenced by icmp_send_response().
#define LWIP_ICMP_ECHO_CHECK_INPUT_PBUF_LEN 1 |
Small optimization: set to 0 if incoming PBUF_POOL pbuf always can be used to modify and send a response packet (and to 1 if this is not the case, e.g.
when link header is stripped of when receiving)
void icmp_dest_unreach | ( | struct pbuf * | p, |
enum icmp_dur_type | t | ||
) |
Send an icmp 'destination unreachable' packet, called from ip_input() if the transport layer protocol is unknown and from udp_input() if the local port is not bound.
p | the input packet for which the 'unreachable' should be sent, p->payload pointing to the IP header |
t | type of the 'unreachable' packet |
References ICMP_DUR, and icmp_send_response().
Referenced by ip_input().
Processes ICMP input packets, called from ip_input().
Currently only processes icmp echo requests and sends out the echo response.
p | the icmp echo request packet, p->payload pointing to the ip header |
inp | the netif on which this packet was received |
References current_iphdr_dest, ERR_OK, ICMP_DEBUG, ICMP_ECHO, ICMP_ER, ICMP_STATS_INC, ICMP_TTL, ICMPH_TYPE_SET, if(), inet_chksum(), inet_chksum_pbuf(), ip_addr_copy, ip_addr_isbroadcast, ip_addr_ismulticast, ip_current_dest_addr, ip_current_src_addr, IP_HDRINCL, IP_HLEN, ip_output_if(), IP_PROTO_ICMP, IPH_CHKSUM_SET, IPH_HL, IPH_TTL_SET, iphdr, pbuf::len, LWIP_ASSERT, LWIP_DEBUGF, NULL, pbuf::payload, pbuf_alloc(), pbuf_copy(), pbuf_free(), pbuf_header(), PBUF_IP_HLEN, PBUF_LINK, PBUF_LINK_HLEN, PBUF_RAM, PP_HTONS, S16_F, snmp_inc_icmpinerrors, snmp_inc_icmpinmsgs, snmp_inc_icmpoutechoreps, snmp_inc_icmpoutmsgs, pbuf::tot_len, and U16_F.
Referenced by ip_input().
Send an icmp packet in response to an incoming packet.
p | the input packet for which the 'unreachable' should be sent, p->payload pointing to the IP header |
type | Type of the ICMP header |
code | Code of the ICMP header |
References ICMP_DEBUG, ICMP_DEST_UNREACH_DATASIZE, ICMP_STATS_INC, ICMP_TTL, inet_chksum(), ip_addr_copy, ip_addr_debug_print, IP_HLEN, ip_output(), IP_PROTO_ICMP, iphdr, pbuf::len, LWIP_ASSERT, LWIP_DEBUGF, NULL, pbuf::payload, pbuf_alloc(), pbuf_free(), PBUF_IP, PBUF_RAM, SMEMCPY, snmp_inc_icmpoutmsgs, and snmp_inc_icmpouttimeexcds.
Referenced by icmp_dest_unreach().