Modules | |
Plot widget options | |
These options can be ORed together to specify the behaviour of a plot widget when creating it with wtk_plot_create. | |
Plot widget grid options | |
These options can be ORed together to specify the behaviour of a plot widget grid when adjusting it via wtk_plot_set_grid. | |
Functions | |
bool | wtk_plot_add_value (struct wtk_plot *plot, uint8_t value) |
Add a value to the end of the plot. More... | |
struct win_window * | wtk_plot_as_child (struct wtk_plot *plot) |
Get pointer to plot window. More... | |
struct wtk_plot * | wtk_plot_create (struct win_window *parent, struct win_area const *area, uint8_t maximum, uint8_t datapoints, gfx_color_t draw_color, struct gfx_bitmap *background, uint8_t option) |
Create a new plot widget. More... | |
void | wtk_plot_set_colors (struct wtk_plot *plot, gfx_color_t draw_color, struct gfx_bitmap *background) |
Set new plot colors. More... | |
void | wtk_plot_set_grid (struct wtk_plot *plot, uint8_t axis_option, uint8_t axis_spacing_x, uint8_t axis_offset_x, uint8_t axis_spacing_y, uint8_t axis_offset_y, gfx_color_t axis_color, gfx_color_t axis_zero_color) |
Set grid/axis parameters. More... | |
static void | wtk_plot_grid_draw (struct wtk_plot *plot, struct win_area const *area, struct win_clip_region const *clip) |
Grid draw function. More... | |
static void | wtk_plot_draw (struct wtk_plot *plot, struct win_area const *area, struct win_clip_region const *clip) |
Plot draw function. More... | |
static bool | wtk_plot_handler (struct win_window *win, enum win_event_type type, void const *data) |
plot event handler. More... | |
Add a value to the end of the plot.
Scales the input value to fit the plot dimensions and adds it to the end of the ring buffer.
plot | Pointer to wtk_plot struct to set new value for. |
value | New value for the plot. |
References Assert, wtk_plot::buffer_start, wtk_plot::container, wtk_plot::maximum, wtk_plot::num_datapoints, wtk_plot::plot_buffer, win_area::size, win_get_area(), wtk_rescale_value(), and win_point::y.
struct win_window* wtk_plot_as_child | ( | struct wtk_plot * | plot | ) |
Get pointer to plot window.
Returns a reference to the window that should be used when managing the widget, such as destroying, moving or reparenting it.
plot | Pointer to wtk_plot struct to manage. |
References Assert, and wtk_plot::container.
struct wtk_plot* wtk_plot_create | ( | struct win_window * | parent, |
struct win_area const * | area, | ||
uint8_t | maximum, | ||
uint8_t | num_datapoints, | ||
gfx_color_t | draw_color, | ||
struct gfx_bitmap * | background, | ||
uint8_t | option | ||
) |
Create a new plot widget.
Allocates the necessary memory and intializes the window and data for plot widgets. If there is not enough memory, the function returns NULL.
To destroy a plot widget and all its contents, and free its memory, call win_destroy() on the plot's child reference, given by wtk_plot_as_child(), similar to:
The plotted graph will shift from right to left as new data values are added. Data values will be overwritten in the ring buffer as they shift out of the plot window. The maximum parameter scales the input value to fit the plot dimensions.
The num_datapoints parameter must not exceed the maximum membag size, and never over 255.
Refer to <gfx/wtk.h> for available configuration options.
parent | Pointer to parent win_window struct. |
area | Pointer to win_area struct with position and size of the plot. Minimum size in both x and y direction is 4 pixels. |
maximum | Maximum value of the plot. |
num_datapoints | Number of datapoints of the plot. |
draw_color | Plot drawing color. |
background | Pointer to background bitmap for frame. NULL for transparent background. When background is transparent the parent window will automatically be redrawn when the basic frame is drawn. |
option | Configuration options for plot. |
References win_attributes::area, Assert, wtk_plot::axis_color, wtk_plot::axis_offset_x, wtk_plot::axis_offset_y, wtk_plot::axis_option, wtk_plot::axis_spacing_x, wtk_plot::axis_spacing_y, wtk_plot::axis_zero_color, wtk_plot::background, win_attributes::background, win_attributes::behavior, wtk_plot::buffer_start, wtk_plot::container, win_attributes::custom, wtk_plot::draw_color, win_attributes::event_handler, wtk_plot::maximum, membag_alloc(), membag_free(), wtk_plot::num_datapoints, wtk_plot::option, wtk_plot::plot_buffer, win_area::size, wtk_plot::spacing, wtk_plot::spacing_error, WIN_BEHAVIOR_REDRAW_PARENT, win_create(), WTK_PLOT_DONT_REDRAW_PARENT, wtk_plot_handler(), WTK_PLOT_SCALE_FACTOR, win_point::x, and win_point::y.
|
static |
Plot draw function.
Draws the plot itself.
plot | Pointer to wtk_plot struct to draw. |
area | Pointer to win_area struct with position and size of the plot. |
clip | Pointer to win_clip_region. |
Called by the event handler to draw the plot.
References wtk_plot::buffer_start, wtk_plot::draw_color, gfx_draw_line, wtk_plot::num_datapoints, wtk_plot::option, win_clip_region::origin, wtk_plot::plot_buffer, win_area::size, wtk_plot::spacing, wtk_plot::spacing_error, WTK_PLOT_INVERT, WTK_PLOT_RIGHT_TO_LEFT, WTK_PLOT_SCALE_FACTOR, win_point::x, and win_point::y.
Referenced by wtk_plot_handler().
|
static |
Grid draw function.
Draws the grid or axis, and zero line based on options.
plot | Pointer to wtk_plot struct to draw. |
area | Pointer to win_area struct with position and size of the plot. |
clip | Pointer to win_clip_region. |
Called by the event handler to draw the grid.
References wtk_plot::axis_color, wtk_plot::axis_offset_x, wtk_plot::axis_offset_y, wtk_plot::axis_option, wtk_plot::axis_spacing_x, wtk_plot::axis_spacing_y, wtk_plot::axis_zero_color, gfx_draw_line, win_clip_region::origin, win_area::size, WTK_PLOT_GRID_HORIZONTAL, WTK_PLOT_GRID_VERTICAL, WTK_PLOT_TICK_MARKER_LENGTH, WTK_PLOT_TICKS_HORIZONTAL, WTK_PLOT_TICKS_VERTICAL, WTK_PLOT_ZERO, win_point::x, and win_point::y.
Referenced by wtk_plot_handler().
|
static |
plot event handler.
This is the window event handler for plot widgets. It handles the two relevant event types sent to a plot's container window, i.e., drawing, and destroy events.
win | Window receiving the event. |
type | The event type. |
data | Custom data, depending on event type. |
References Assert, wtk_plot::background, wtk_plot::container, gfx_draw_rect, membag_free(), win_clip_region::origin, wtk_plot::plot_buffer, win_area::size, WIN_EVENT_DESTROY, WIN_EVENT_DRAW, win_get_area(), win_get_custom_data(), WTK_PLOT_BORDER_COLOR, wtk_plot_draw(), wtk_plot_grid_draw(), win_point::x, and win_point::y.
Referenced by wtk_plot_create().
void wtk_plot_set_colors | ( | struct wtk_plot * | plot, |
gfx_color_t | draw_color, | ||
struct gfx_bitmap * | background | ||
) |
Set new plot colors.
This sets new draw and background colors for the plot.
plot | Pointer to wtk_plot struct to set colors for. |
draw_color | Draw color to set for plot. |
background | Background color to set for plot. |
References Assert, wtk_plot::background, and wtk_plot::draw_color.
void wtk_plot_set_grid | ( | struct wtk_plot * | plot, |
uint8_t | axis_option, | ||
uint8_t | axis_spacing_x, | ||
uint8_t | axis_offset_x, | ||
uint8_t | axis_spacing_y, | ||
uint8_t | axis_offset_y, | ||
gfx_color_t | axis_color, | ||
gfx_color_t | axis_zero_color | ||
) |
Set grid/axis parameters.
This function sets the grid and axis options, colors for the plot. The axis_spacing_y and axis_offset_y parameter is rescaled to fit the plot. Both grid and axis can not be used on the same plot.
Refer to <gfx/wtk.h> for available configuration options.
plot | Pointer to wtk_plot struct to set colors for. |
axis_option | Configuration of axis, grid and zero-line behaviour. |
axis_spacing_x | Space between x-axis grid lines/tick marks. |
axis_offset_x | Grid/axis offset along the x-axis. |
axis_spacing_y | Space between y-axis grid lines/tick marks. |
axis_offset_y | Grid/axis offset along the y-axis. |
axis_color | Color for the tick marks and grid lines. |
axis_zero_color | Color for the zero line. |
References Assert, wtk_plot::axis_color, wtk_plot::axis_offset_x, wtk_plot::axis_offset_y, wtk_plot::axis_option, wtk_plot::axis_spacing_x, wtk_plot::axis_spacing_y, wtk_plot::axis_zero_color, wtk_plot::container, wtk_plot::maximum, win_area::size, win_get_area(), wtk_rescale_value(), and win_point::y.