This structure contains the parameters for the sha204m_check_mac function.
#include <sha204_command_marshaling.h>
Data Fields | |
uint8_t * | client_challenge |
pointer to challenge that host had sent to client More... | |
uint8_t * | client_response |
pointer to challenge response received from client More... | |
uint8_t | key_id |
what key to use for the MAC calculation More... | |
uint8_t | mode |
what to include in the MAC calculation More... | |
uint8_t * | other_data |
pointer to 13 bytes of data that were used by client to calculate MAC More... | |
uint8_t * | rx_buffer |
pointer to receive buffer More... | |
uint8_t * | tx_buffer |
pointer to send buffer More... | |
uint8_t* sha204_check_mac_parameters::client_challenge |
pointer to challenge that host had sent to client
Referenced by sha204m_check_mac().
uint8_t* sha204_check_mac_parameters::client_response |
pointer to challenge response received from client
Referenced by sha204m_check_mac().
uint8_t sha204_check_mac_parameters::key_id |
what key to use for the MAC calculation
Referenced by sha204m_check_mac().
uint8_t sha204_check_mac_parameters::mode |
what to include in the MAC calculation
Referenced by sha204m_check_mac().
uint8_t* sha204_check_mac_parameters::other_data |
pointer to 13 bytes of data that were used by client to calculate MAC
Referenced by sha204m_check_mac().
uint8_t* sha204_check_mac_parameters::rx_buffer |
pointer to receive buffer
Referenced by sha204m_check_mac().
uint8_t* sha204_check_mac_parameters::tx_buffer |
pointer to send buffer
Referenced by sha204m_check_mac().