Microchip® Advanced Software Framework

unit_tests.c File Reference

Unit tests for NAND Flash component.

Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.

#include <stdint.h>
#include <stdbool.h>
#include <asf.h>
#include <board.h>
#include <sysclk.h>
#include "nand_flash_raw.h"
#include "nand_flash_ecc.h"
#include <string.h>
#include <unit_test/suite.h>
#include <stdio_serial.h>
#include <conf_test.h>
#include <conf_board.h>

Functions

int main (void)
 Run NAND Flash component unit tests. More...
 
static void run_test_initialization (const struct test_case *test)
 Test NAND Flash initialization. More...
 
static void run_test_raw_read_write (const struct test_case *test)
 Test raw read/write functions. More...
 
static void run_test_software_ecc (const struct test_case *test)
 Test software ECC read/write functions. More...
 

Variables

static uint32_t addr_address = BOARD_NF_ADDRESS_ADDR
 
volatile uint32_t block
 
static uint32_t cmd_address = BOARD_NF_COMMAND_ADDR
 
static uint32_t data_address = BOARD_NF_DATA_ADDR
 
volatile uint32_t error_code
 
volatile uint32_t flash_id
 
static struct nand_flash_ecc nf_ecc
 
static struct nand_flash_raw nf_raw
 
static uint32_t num_block
 
static uint32_t page_size
 
static uint8_t read_buffer [2048]
 
static uint8_t spare_buffer [NAND_COMMON_MAX_PAGE_SPARE_SIZE]
 
static uint8_t write_buffer [2048]
 

static void run_test_initialization ( const struct test_case test)
static

Test NAND Flash initialization.

This test call the initialization function and check the flash id.

Parameters
testCurrent test case.

References addr_address, cmd_address, data_address, error_code, flash_id, nand_flash_raw::model, nand_flash_model_get_device_size_in_blocks(), nand_flash_model_get_page_data_size(), nand_flash_raw_initialize(), nand_flash_raw_read_id(), nf_ecc, nf_raw, num_block, page_size, nand_flash_ecc::raw, and test_assert_true.

Referenced by main().

static void run_test_raw_read_write ( const struct test_case test)
static

Test raw read/write functions.

This test call the raw read/write functions and check the data value.

Parameters
testCurrent test case.

References block, error_code, nand_flash_raw_erase_block(), nand_flash_raw_read_page(), nand_flash_raw_write_page(), nf_raw, num_block, page_size, read_buffer, test_assert_true, and write_buffer.

Referenced by main().

static void run_test_software_ecc ( const struct test_case test)
static

Test software ECC read/write functions.

This test call the software ECC read/write functions and check the data value.

Parameters
testCurrent test case.

References block, error_code, nand_flash_ecc_read_page(), nand_flash_ecc_write_page(), nand_flash_raw_erase_block(), nand_flash_raw_read_page(), nf_ecc, nf_raw, num_block, page_size, read_buffer, spare_buffer, test_assert_true, and write_buffer.

Referenced by main().

uint32_t addr_address = BOARD_NF_ADDRESS_ADDR
static

Referenced by run_test_initialization().

volatile uint32_t block
uint32_t cmd_address = BOARD_NF_COMMAND_ADDR
static

Referenced by run_test_initialization().

uint32_t data_address = BOARD_NF_DATA_ADDR
static
volatile uint32_t error_code
volatile uint32_t flash_id

Referenced by run_test_initialization().

struct nand_flash_ecc nf_ecc
static
uint32_t num_block
static
uint8_t read_buffer[2048]
static
uint8_t write_buffer[2048]
static