SAMV70/SAMV71/SAME70/SAMS70-XULTRA board mpu config.
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
#include "compiler.h"
Macros | |
#define | ARM_MODE_USR 0x10 |
#define | DTCM_END_ADDRESS 0x203FFFFFUL |
#define | DTCM_START_ADDRESS 0x20000000UL |
#define | EXT_EBI_END_ADDRESS 0x6FFFFFFFUL |
#define | EXT_EBI_START_ADDRESS 0x60000000UL |
#define | IFLASH_END_ADDRESS 0x005FFFFFUL |
#define | IFLASH_PRIVILEGE_END_ADDRESS (IFLASH_START_ADDRESS + 0xFFF) |
#define | IFLASH_PRIVILEGE_START_ADDRESS (IFLASH_START_ADDRESS) |
#define | IFLASH_START_ADDRESS 0x00400000UL |
#define | IFLASH_UNPRIVILEGE_END_ADDRESS (IFLASH_END_ADDRESS) |
#define | IFLASH_UNPRIVILEGE_START_ADDRESS (IFLASH_PRIVILEGE_END_ADDRESS + 1) |
#define | INNER_NORMAL_WB_NWA_TYPE(x) (( 0x04 << MPU_RASR_TEX_Pos ) | ( ENABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos ) | ( x << MPU_RASR_S_Pos )) |
#define | INNER_NORMAL_WB_RWA_TYPE(x) (( 0x04 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos ) | ( x << MPU_RASR_S_Pos )) |
#define | INNER_OUTER_NORMAL_NOCACHE_TYPE(x) ((0x01 << MPU_RASR_TEX_Pos) | (DISABLE << MPU_RASR_C_Pos) | (DISABLE << MPU_RASR_B_Pos) | (x << MPU_RASR_S_Pos)) |
#define | ITCM_END_ADDRESS 0x003FFFFFUL |
#define | ITCM_START_ADDRESS 0x00000000UL |
#define | MPU_AP_FULL_ACCESS ( 0x03 << MPU_RASR_AP_Pos ) |
#define | MPU_AP_NO_ACCESS ( 0x00 << MPU_RASR_AP_Pos ) |
#define | MPU_AP_PRIVILEGED_READ_WRITE ( 0x01 << MPU_RASR_AP_Pos ) |
#define | MPU_AP_PRIVILEGED_READONLY ( 0x05 << MPU_RASR_AP_Pos ) |
#define | MPU_AP_READONLY ( 0x06 << MPU_RASR_AP_Pos ) |
#define | MPU_AP_READONLY2 ( 0x07 << MPU_RASR_AP_Pos ) |
#define | MPU_AP_RES ( 0x04 << MPU_RASR_AP_Pos ) |
#define | MPU_AP_UNPRIVILEGED_READONLY ( 0x02 << MPU_RASR_AP_Pos ) |
#define | MPU_DEFAULT_DTCM_REGION ( 3 ) |
#define | MPU_DEFAULT_IFLASH_REGION ( 2 ) |
#define | MPU_DEFAULT_ITCM_REGION ( 1 ) |
#define | MPU_DEFAULT_SDRAM_REGION ( 8 ) |
#define | MPU_DEFAULT_SRAM_REGION_1 ( 4 ) |
#define | MPU_DEFAULT_SRAM_REGION_2 ( 5 ) |
#define | MPU_ENABLE ( 0x1 << MPU_CTRL_ENABLE_Pos) |
#define | MPU_EXT_EBI_REGION ( 7 ) |
#define | MPU_HFNMIENA ( 0x1 << MPU_CTRL_HFNMIENA_Pos ) |
#define | MPU_PERIPHERALS_REGION ( 6 ) |
#define | MPU_PRIVDEFENA ( 0x1 << MPU_CTRL_PRIVDEFENA_Pos ) |
#define | MPU_QSPIMEM_REGION ( 9 ) |
#define | MPU_REGION_BUFFERABLE ( 0x01 << MPU_RASR_B_Pos ) |
#define | MPU_REGION_CACHEABLE ( 0x01 << MPU_RASR_C_Pos ) |
#define | MPU_REGION_DISABLE ( 0x0 ) |
#define | MPU_REGION_ENABLE ( 0x01 ) |
#define | MPU_REGION_EXECUTE_NEVER ( 0x01 << MPU_RASR_XN_Pos ) |
#define | MPU_REGION_SHAREABLE ( 0x01 << MPU_RASR_S_Pos ) |
#define | MPU_REGION_VALID ( 0x10 ) |
#define | MPU_TEX_B000 ( 0x00 << MPU_RASR_TEX_Pos ) |
#define | MPU_TEX_B001 ( 0x01 << MPU_RASR_TEX_Pos ) |
#define | MPU_TEX_B010 ( 0x02 << MPU_RASR_TEX_Pos ) |
#define | MPU_TEX_B011 ( 0x03 << MPU_RASR_TEX_Pos ) |
#define | MPU_TEX_B100 ( 0x04 << MPU_RASR_TEX_Pos ) |
#define | MPU_TEX_B101 ( 0x05 << MPU_RASR_TEX_Pos ) |
#define | MPU_TEX_B110 ( 0x06 << MPU_RASR_TEX_Pos ) |
#define | MPU_TEX_B111 ( 0x07 << MPU_RASR_TEX_Pos ) |
#define | MPU_USBHSRAM_REGION ( 10 ) |
#define | NON_SHAREABLE 0 |
#define | PERIPHERALS_END_ADDRESS 0x5FFFFFFFUL |
#define | PERIPHERALS_START_ADDRESS 0x40000000UL |
#define | PRIVILEGE_MODE 0 |
#define | QSPI_END_ADDRESS 0x9FFFFFFFUL |
#define | QSPI_START_ADDRESS 0x80000000UL |
#define | SDRAM_END_ADDRESS 0x7FFFFFFFUL |
#define | SDRAM_START_ADDRESS 0x70000000UL |
#define | SHAREABLE 1 |
#define | SHAREABLE_DEVICE_TYPE (( 0x00 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos )) |
#define | SRAM_END_ADDRESS 0x2045FFFFUL |
#define | SRAM_FIRST_END_ADDRESS (SRAM_FIRST_START_ADDRESS + 0x3FFFF) |
#define | SRAM_FIRST_START_ADDRESS (SRAM_START_ADDRESS) |
#define | SRAM_SECOND_END_ADDRESS (SRAM_END_ADDRESS) |
#define | SRAM_SECOND_START_ADDRESS (SRAM_FIRST_END_ADDRESS + 1) |
#define | SRAM_START_ADDRESS 0x20400000UL |
#define | STRONGLY_ORDERED_SHAREABLE_TYPE (( 0x00 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( DISABLE << MPU_RASR_B_Pos )) |
#define | USBHSRAM_END_ADDRESS 0xA01FFFFFUL |
#define | USBHSRAM_START_ADDRESS 0xA0100000UL |
#define | USER_MODE 1 |
Functions | |
uint32_t | mpu_cal_mpu_region_size (uint32_t dw_actual_size_in_bytes) |
Calculate region size for the RASR. More... | |
void | mpu_disable_region (void) |
Disable the current active region. More... | |
void | mpu_enable (uint32_t dw_mpu_enable) |
Enables the MPU module. More... | |
void | mpu_set_region (uint32_t dw_region_base_addr, uint32_t dw_region_attr) |
Setup a memory region. More... | |
void | mpu_set_region_num (uint32_t dw_region_num) |
Set active memory region. More... | |
void | mpu_update_regions (uint32_t dw_region_num, uint32_t dw_region_base_addr, uint32_t dw_region_attr) |
Update MPU regions. More... | |
#define ARM_MODE_USR 0x10 |
#define DTCM_END_ADDRESS 0x203FFFFFUL |
Referenced by _setup_memory_region().
#define DTCM_START_ADDRESS 0x20000000UL |
Referenced by _setup_memory_region().
#define EXT_EBI_END_ADDRESS 0x6FFFFFFFUL |
Referenced by _setup_memory_region().
#define EXT_EBI_START_ADDRESS 0x60000000UL |
Referenced by _setup_memory_region().
#define IFLASH_END_ADDRESS 0x005FFFFFUL |
Referenced by _setup_memory_region().
#define IFLASH_PRIVILEGE_END_ADDRESS (IFLASH_START_ADDRESS + 0xFFF) |
#define IFLASH_PRIVILEGE_START_ADDRESS (IFLASH_START_ADDRESS) |
#define IFLASH_START_ADDRESS 0x00400000UL |
Referenced by _setup_memory_region().
#define IFLASH_UNPRIVILEGE_END_ADDRESS (IFLASH_END_ADDRESS) |
#define IFLASH_UNPRIVILEGE_START_ADDRESS (IFLASH_PRIVILEGE_END_ADDRESS + 1) |
#define INNER_NORMAL_WB_NWA_TYPE | ( | x | ) | (( 0x04 << MPU_RASR_TEX_Pos ) | ( ENABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos ) | ( x << MPU_RASR_S_Pos )) |
Referenced by _setup_memory_region().
#define INNER_NORMAL_WB_RWA_TYPE | ( | x | ) | (( 0x04 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos ) | ( x << MPU_RASR_S_Pos )) |
Referenced by _setup_memory_region().
#define INNER_OUTER_NORMAL_NOCACHE_TYPE | ( | x | ) | ((0x01 << MPU_RASR_TEX_Pos) | (DISABLE << MPU_RASR_C_Pos) | (DISABLE << MPU_RASR_B_Pos) | (x << MPU_RASR_S_Pos)) |
Referenced by _setup_memory_region().
#define ITCM_END_ADDRESS 0x003FFFFFUL |
Referenced by _setup_memory_region().
#define ITCM_START_ADDRESS 0x00000000UL |
Referenced by _setup_memory_region().
#define MPU_AP_FULL_ACCESS ( 0x03 << MPU_RASR_AP_Pos ) |
Referenced by _setup_memory_region().
#define MPU_AP_NO_ACCESS ( 0x00 << MPU_RASR_AP_Pos ) |
#define MPU_AP_PRIVILEGED_READ_WRITE ( 0x01 << MPU_RASR_AP_Pos ) |
Referenced by _setup_memory_region().
#define MPU_AP_PRIVILEGED_READONLY ( 0x05 << MPU_RASR_AP_Pos ) |
#define MPU_AP_READONLY ( 0x06 << MPU_RASR_AP_Pos ) |
Referenced by _setup_memory_region().
#define MPU_AP_READONLY2 ( 0x07 << MPU_RASR_AP_Pos ) |
#define MPU_AP_RES ( 0x04 << MPU_RASR_AP_Pos ) |
#define MPU_AP_UNPRIVILEGED_READONLY ( 0x02 << MPU_RASR_AP_Pos ) |
#define MPU_DEFAULT_DTCM_REGION ( 3 ) |
Referenced by _setup_memory_region().
#define MPU_DEFAULT_IFLASH_REGION ( 2 ) |
Referenced by _setup_memory_region().
#define MPU_DEFAULT_ITCM_REGION ( 1 ) |
Referenced by _setup_memory_region().
#define MPU_DEFAULT_SDRAM_REGION ( 8 ) |
Referenced by _setup_memory_region().
#define MPU_DEFAULT_SRAM_REGION_1 ( 4 ) |
Referenced by _setup_memory_region().
#define MPU_DEFAULT_SRAM_REGION_2 ( 5 ) |
Referenced by _setup_memory_region().
#define MPU_ENABLE ( 0x1 << MPU_CTRL_ENABLE_Pos) |
Referenced by _setup_memory_region().
#define MPU_EXT_EBI_REGION ( 7 ) |
Referenced by _setup_memory_region().
#define MPU_HFNMIENA ( 0x1 << MPU_CTRL_HFNMIENA_Pos ) |
#define MPU_PERIPHERALS_REGION ( 6 ) |
Referenced by _setup_memory_region().
#define MPU_PRIVDEFENA ( 0x1 << MPU_CTRL_PRIVDEFENA_Pos ) |
Referenced by _setup_memory_region().
#define MPU_QSPIMEM_REGION ( 9 ) |
Referenced by _setup_memory_region().
#define MPU_REGION_BUFFERABLE ( 0x01 << MPU_RASR_B_Pos ) |
#define MPU_REGION_CACHEABLE ( 0x01 << MPU_RASR_C_Pos ) |
#define MPU_REGION_DISABLE ( 0x0 ) |
#define MPU_REGION_ENABLE ( 0x01 ) |
Referenced by _setup_memory_region().
#define MPU_REGION_EXECUTE_NEVER ( 0x01 << MPU_RASR_XN_Pos ) |
Referenced by _setup_memory_region().
#define MPU_REGION_SHAREABLE ( 0x01 << MPU_RASR_S_Pos ) |
#define MPU_REGION_VALID ( 0x10 ) |
Referenced by _setup_memory_region().
#define MPU_TEX_B000 ( 0x00 << MPU_RASR_TEX_Pos ) |
#define MPU_TEX_B001 ( 0x01 << MPU_RASR_TEX_Pos ) |
#define MPU_TEX_B010 ( 0x02 << MPU_RASR_TEX_Pos ) |
#define MPU_TEX_B011 ( 0x03 << MPU_RASR_TEX_Pos ) |
#define MPU_TEX_B100 ( 0x04 << MPU_RASR_TEX_Pos ) |
#define MPU_TEX_B101 ( 0x05 << MPU_RASR_TEX_Pos ) |
#define MPU_TEX_B110 ( 0x06 << MPU_RASR_TEX_Pos ) |
#define MPU_TEX_B111 ( 0x07 << MPU_RASR_TEX_Pos ) |
#define MPU_USBHSRAM_REGION ( 10 ) |
Referenced by _setup_memory_region().
#define NON_SHAREABLE 0 |
Referenced by _setup_memory_region().
#define PERIPHERALS_END_ADDRESS 0x5FFFFFFFUL |
Referenced by _setup_memory_region().
#define PERIPHERALS_START_ADDRESS 0x40000000UL |
Referenced by _setup_memory_region().
#define PRIVILEGE_MODE 0 |
#define QSPI_END_ADDRESS 0x9FFFFFFFUL |
Referenced by _setup_memory_region().
#define QSPI_START_ADDRESS 0x80000000UL |
Referenced by _setup_memory_region().
#define SDRAM_END_ADDRESS 0x7FFFFFFFUL |
Referenced by _setup_memory_region().
#define SDRAM_START_ADDRESS 0x70000000UL |
Referenced by _setup_memory_region().
#define SHAREABLE 1 |
Referenced by _setup_memory_region().
#define SHAREABLE_DEVICE_TYPE (( 0x00 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( ENABLE << MPU_RASR_B_Pos )) |
Referenced by _setup_memory_region().
#define SRAM_END_ADDRESS 0x2045FFFFUL |
#define SRAM_FIRST_END_ADDRESS (SRAM_FIRST_START_ADDRESS + 0x3FFFF) |
Referenced by _setup_memory_region().
#define SRAM_FIRST_START_ADDRESS (SRAM_START_ADDRESS) |
Referenced by _setup_memory_region().
#define SRAM_SECOND_END_ADDRESS (SRAM_END_ADDRESS) |
Referenced by _setup_memory_region().
#define SRAM_SECOND_START_ADDRESS (SRAM_FIRST_END_ADDRESS + 1) |
Referenced by _setup_memory_region().
#define SRAM_START_ADDRESS 0x20400000UL |
#define STRONGLY_ORDERED_SHAREABLE_TYPE (( 0x00 << MPU_RASR_TEX_Pos ) | ( DISABLE << MPU_RASR_C_Pos ) | ( DISABLE << MPU_RASR_B_Pos )) |
Referenced by _setup_memory_region().
#define USBHSRAM_END_ADDRESS 0xA01FFFFFUL |
Referenced by _setup_memory_region().
#define USBHSRAM_START_ADDRESS 0xA0100000UL |
Referenced by _setup_memory_region().
#define USER_MODE 1 |