API driver for AT25DFx SerialFlash component.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | AT25_BLOCK_ERASE_32K 0x52 |
Block erase command code (32K block) More... | |
#define | AT25_BLOCK_ERASE_4K 0x20 |
Block erase command code (4K block) More... | |
#define | AT25_BLOCK_ERASE_64K 0xD8 |
Block erase command code (64K block) More... | |
#define | AT25_BYTE_PAGE_PROGRAM 0x02 |
Byte/page program command code. More... | |
#define | AT25_CHIP_ERASE_1 0x60 |
Chip erase command code 1. More... | |
#define | AT25_CHIP_ERASE_2 0xC7 |
Chip erase command code 2. More... | |
#define | AT25_DEEP_PDOWN 0xB9 |
Deep power-down command code. More... | |
#define | AT25_GLOBAL_PROTECT_VALUE 0x3C |
Global protection data. More... | |
#define | AT25_PROTECT_SECTOR 0x36 |
Protect sector command code. More... | |
#define | AT25_READ_ARRAY 0x0B |
Read array command code. More... | |
#define | AT25_READ_ARRAY_LF 0x03 |
Read array (low frequency) command code. More... | |
#define | AT25_READ_JEDEC_ID 0x9F |
Read manufacturer and device ID command code. More... | |
#define | AT25_READ_SECTOR_PROT 0x3C |
Read sector protection registers command code. More... | |
#define | AT25_READ_STATUS 0x05 |
Read status register command code. More... | |
#define | AT25_RES_DEEP_PDOWN 0xAB |
Resume from deep power-down command code. More... | |
#define | AT25_SECTOR_PROTECTED_VALUE 0xff |
Sector Protection Register value is 1 (sector is protected) More... | |
#define | AT25_SECTOR_UNPROTECTED_VALUE 0x0 |
Sector Protection Register value is 0 (sector is unprotected) More... | |
#define | AT25_SEQUENTIAL_PROGRAM_1 0xAD |
Sequential program mode command code 1. More... | |
#define | AT25_SEQUENTIAL_PROGRAM_2 0xAF |
Sequential program mode command code 2. More... | |
#define | AT25_STATUS_EPE (1 << 5) |
Erase/program error bit. More... | |
#define | AT25_STATUS_EPE_ERROR (1 << 5) |
Erase or program error is detected. More... | |
#define | AT25_STATUS_EPE_SUCCESS (0 << 5) |
Erase or program operation was successful. More... | |
#define | AT25_STATUS_RDYBSY (1 << 0) |
Device ready/busy status bit. More... | |
#define | AT25_STATUS_RDYBSY_BUSY (1 << 0) |
Device is busy with internal operations. More... | |
#define | AT25_STATUS_RDYBSY_READY (0 << 0) |
Device is ready. More... | |
#define | AT25_STATUS_SPRL (1 << 7) |
Sector protection registers locked bit. More... | |
#define | AT25_STATUS_SPRL_LOCKED (1 << 7) |
Sector protection registers are locked. More... | |
#define | AT25_STATUS_SPRL_UNLOCKED (0 << 7) |
Sector protection registers are unlocked. More... | |
#define | AT25_STATUS_SWP (3 << 2) |
Software protection status bitfield. More... | |
#define | AT25_STATUS_SWP_PROTALL (3 << 2) |
All sectors are software protected. More... | |
#define | AT25_STATUS_SWP_PROTNONE (0 << 2) |
No sector is software protected. More... | |
#define | AT25_STATUS_SWP_PROTSOME (1 << 2) |
Some sectors are software protected. More... | |
#define | AT25_STATUS_WEL (1 << 1) |
Write enable latch status bit. More... | |
#define | AT25_STATUS_WEL_DISABLED (0 << 1) |
Device is not write enabled. More... | |
#define | AT25_STATUS_WEL_ENABLED (1 << 1) |
Device is write enabled. More... | |
#define | AT25_STATUS_WPP (1 << 4) |
Write protect pin status bit. More... | |
#define | AT25_STATUS_WPP_ASSERTED (1 << 4) |
Write protect signal is asserted. More... | |
#define | AT25_STATUS_WPP_NOTASSERTED (0 << 4) |
Write protect signal is not asserted. More... | |
#define | AT25_TYPE_PROTECT 0x1 |
Protect type code. More... | |
#define | AT25_TYPE_UNPROTECT 0x0 |
Unprotect type code. More... | |
#define | AT25_UNPROTECT_SECTOR 0x39 |
Unprotect sector command code. More... | |
#define | AT25_WRITE_DISABLE 0x04 |
Write disable command code. More... | |
#define | AT25_WRITE_ENABLE 0x06 |
Write enable command code. More... | |
#define | AT25_WRITE_STATUS 0x01 |
Write status register command code. More... | |
#define | AT25DFX_0161 3 /* AT26DF0161 */ |
#define | AT25DFX_021 8 /* AT25DF021 */ |
#define | AT25DFX_041A 0 /* AT25DF041A */ |
Supporting AT25 device type. More... | |
#define | AT25DFX_081A 2 /* AT26DF081A */ |
#define | AT25DFX_161 1 /* AT25DF161 */ |
#define | AT25DFX_161A 4 /* AT26DF161A */ |
#define | AT25DFX_321 5 /* AT25DF321 */ |
#define | AT25DFX_321A 6 /* AT25DF321A */ |
#define | AT25DFX_512B 7 /* AT25DF512B */ |
#define | AT25DFX_641A 9 /* AT25DF641A */ |
Typedefs | |
typedef enum at25_status | at25_status_t |
AT25 operation status, each operation returns one of the following status. More... | |
Enumerations | |
enum | at25_status { AT25_SUCCESS = 0, AT25_SECTOR_PROTECTED, AT25_SECTOR_UNPROTECTED, AT25_ERROR_INIT, AT25_ERROR_NOT_FOUND, AT25_ERROR_WRITE, AT25_ERROR_BUSY, AT25_ERROR_PROTECTED, AT25_ERROR_SPI, AT25_ERROR } |
AT25 operation status, each operation returns one of the following status. More... | |
Functions | |
at25_status_t | at25dfx_erase_block (uint32_t address) |
Erase the specified block of the SerialFlash. More... | |
at25_status_t | at25dfx_erase_chip (void) |
Erase all the content of the memory chip. More... | |
at25_status_t | at25dfx_initialize (void) |
Initialize the SerialFlash. More... | |
at25_status_t | at25dfx_mem_check (void) |
Check if the SerialFlash is valid. More... | |
at25_status_t | at25dfx_protect_chip (uint8_t protect_type) |
Protect the SerialFlash device. More... | |
at25_status_t | at25dfx_protect_sector (uint32_t address, uint8_t protect_type) |
Protect/unprotect the specific sector. More... | |
at25_status_t | at25dfx_read (uint8_t *data, uint16_t size, uint32_t address) |
Read data from the specified address on the SerialFlash. More... | |
at25_status_t | at25dfx_read_sector_protect_status (uint32_t address) |
Read sector protection status. More... | |
at25_status_t | at25dfx_read_status (uint8_t *status) |
Read and return the status register of the SerialFlash. More... | |
void | at25dfx_set_mem_active (uint8_t cs) |
Select the SerialFlash by the corresponding chip select. More... | |
at25_status_t | at25dfx_write (uint8_t *data, uint16_t size, uint32_t address) |
Write data at the specified address on the serial firmware SerialFlash. More... | |
at25_status_t | at25dfx_write_status (uint8_t status) |
Write the given value in the status register of the SerialFlash device. More... | |
#define AT25_BLOCK_ERASE_32K 0x52 |
Block erase command code (32K block)
#define AT25_BLOCK_ERASE_4K 0x20 |
Block erase command code (4K block)
#define AT25_BLOCK_ERASE_64K 0xD8 |
Block erase command code (64K block)
#define AT25_BYTE_PAGE_PROGRAM 0x02 |
Byte/page program command code.
Referenced by at25dfx_send_command(), and at25dfx_write().
#define AT25_CHIP_ERASE_1 0x60 |
Chip erase command code 1.
#define AT25_CHIP_ERASE_2 0xC7 |
Chip erase command code 2.
Referenced by at25dfx_erase_chip().
#define AT25_DEEP_PDOWN 0xB9 |
Deep power-down command code.
#define AT25_GLOBAL_PROTECT_VALUE 0x3C |
Global protection data.
Referenced by at25dfx_protect_chip().
#define AT25_PROTECT_SECTOR 0x36 |
Protect sector command code.
Referenced by at25dfx_protect_sector().
#define AT25_READ_ARRAY 0x0B |
Read array command code.
#define AT25_READ_ARRAY_LF 0x03 |
Read array (low frequency) command code.
Referenced by at25dfx_read().
#define AT25_READ_JEDEC_ID 0x9F |
Read manufacturer and device ID command code.
Referenced by at25dfx_read_dev_id().
#define AT25_READ_SECTOR_PROT 0x3C |
Read sector protection registers command code.
Referenced by at25dfx_read_sector_protect_status().
#define AT25_READ_STATUS 0x05 |
Read status register command code.
Referenced by at25dfx_read_status().
#define AT25_RES_DEEP_PDOWN 0xAB |
Resume from deep power-down command code.
#define AT25_SECTOR_PROTECTED_VALUE 0xff |
Sector Protection Register value is 1 (sector is protected)
Referenced by at25dfx_read_sector_protect_status().
#define AT25_SECTOR_UNPROTECTED_VALUE 0x0 |
Sector Protection Register value is 0 (sector is unprotected)
Referenced by at25dfx_read_sector_protect_status().
#define AT25_SEQUENTIAL_PROGRAM_1 0xAD |
Sequential program mode command code 1.
#define AT25_SEQUENTIAL_PROGRAM_2 0xAF |
Sequential program mode command code 2.
#define AT25_STATUS_EPE (1 << 5) |
Erase/program error bit.
Referenced by at25dfx_write().
#define AT25_STATUS_EPE_ERROR (1 << 5) |
Erase or program error is detected.
Referenced by at25dfx_write().
#define AT25_STATUS_EPE_SUCCESS (0 << 5) |
Erase or program operation was successful.
#define AT25_STATUS_RDYBSY (1 << 0) |
Device ready/busy status bit.
Referenced by at25dfx_erase_block(), and at25dfx_wait_ready().
#define AT25_STATUS_RDYBSY_BUSY (1 << 0) |
Device is busy with internal operations.
#define AT25_STATUS_RDYBSY_READY (0 << 0) |
Device is ready.
Referenced by at25dfx_erase_block(), and at25dfx_wait_ready().
#define AT25_STATUS_SPRL (1 << 7) |
Sector protection registers locked bit.
Referenced by at25dfx_protect_chip().
#define AT25_STATUS_SPRL_LOCKED (1 << 7) |
Sector protection registers are locked.
#define AT25_STATUS_SPRL_UNLOCKED (0 << 7) |
Sector protection registers are unlocked.
#define AT25_STATUS_SWP (3 << 2) |
Software protection status bitfield.
Referenced by at25dfx_erase_block(), at25dfx_erase_chip(), at25dfx_protect_chip(), and run_test_at25dfx_protect().
#define AT25_STATUS_SWP_PROTALL (3 << 2) |
All sectors are software protected.
#define AT25_STATUS_SWP_PROTNONE (0 << 2) |
No sector is software protected.
Referenced by at25dfx_erase_block(), at25dfx_erase_chip(), and run_test_at25dfx_protect().
#define AT25_STATUS_SWP_PROTSOME (1 << 2) |
Some sectors are software protected.
#define AT25_STATUS_WEL (1 << 1) |
Write enable latch status bit.
#define AT25_STATUS_WEL_DISABLED (0 << 1) |
Device is not write enabled.
#define AT25_STATUS_WEL_ENABLED (1 << 1) |
Device is write enabled.
#define AT25_STATUS_WPP (1 << 4) |
Write protect pin status bit.
#define AT25_STATUS_WPP_ASSERTED (1 << 4) |
Write protect signal is asserted.
#define AT25_STATUS_WPP_NOTASSERTED (0 << 4) |
Write protect signal is not asserted.
#define AT25_TYPE_PROTECT 0x1 |
Protect type code.
Referenced by at25dfx_protect_chip(), at25dfx_protect_sector(), and run_test_at25dfx_protect().
#define AT25_TYPE_UNPROTECT 0x0 |
Unprotect type code.
Referenced by run_test_at25dfx_data_access(), and run_test_at25dfx_protect().
#define AT25_UNPROTECT_SECTOR 0x39 |
Unprotect sector command code.
Referenced by at25dfx_protect_sector().
#define AT25_WRITE_DISABLE 0x04 |
Write disable command code.
#define AT25_WRITE_ENABLE 0x06 |
Write enable command code.
Referenced by at25dfx_enable_write().
#define AT25_WRITE_STATUS 0x01 |
Write status register command code.
Referenced by at25dfx_send_command(), and at25dfx_write_status().
#define AT25DFX_0161 3 /* AT26DF0161 */ |
#define AT25DFX_021 8 /* AT25DF021 */ |
#define AT25DFX_041A 0 /* AT25DF041A */ |
Supporting AT25 device type.
#define AT25DFX_081A 2 /* AT26DF081A */ |
#define AT25DFX_161 1 /* AT25DF161 */ |
#define AT25DFX_161A 4 /* AT26DF161A */ |
#define AT25DFX_321 5 /* AT25DF321 */ |
#define AT25DFX_321A 6 /* AT25DF321A */ |
#define AT25DFX_512B 7 /* AT25DF512B */ |
#define AT25DFX_641A 9 /* AT25DF641A */ |
typedef enum at25_status at25_status_t |
AT25 operation status, each operation returns one of the following status.
enum at25_status |
AT25 operation status, each operation returns one of the following status.