Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
AT30TS Temperature Sensor Example Documentation

Introduction

This is an example application for the AT30TS Temperature Sensor. The TEMPSENSORX kit has got an AT30TSE758 device and an AT30TSE002B. Here, we've selected AT30TSE758 as test device in this example

Main Files

Device Info

All AVR devices with TWI Master driver support in ASF can be used. This example has been tested with the following setup:

  • XMEGA-A3BU Xplained with ATAVRTEMPSENSORX

Description of the example application

The example application test the different driver functions for the selected AT30TS temperature sensor device. It indicates test Success/Failure on the LEDs available on ATAVRTEMPSENSORX and displays corresponding messages on the LCD screen of XMEGA-A3BU Xplained

Dependencies

This driver depends on the following modules:

Compilation info

This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.

Contact Information

For further information, visit Microchip.