Microchip® Advanced Software Framework

ip6.c File Reference

IPv6 layer.

#include "lwip/opt.h"
#include "lwip/def.h"
#include "lwip/mem.h"
#include "lwip/netif.h"
#include "lwip/ip6.h"
#include "lwip/ip6_addr.h"
#include "lwip/ip6_frag.h"
#include "lwip/icmp6.h"
#include "lwip/raw.h"
#include "lwip/udp.h"
#include "lwip/tcp_impl.h"
#include "lwip/dhcp6.h"
#include "lwip/nd6.h"
#include "lwip/mld6.h"
#include "lwip/debug.h"
#include "lwip/stats.h"

Functions

err_t ip6_input (struct pbuf *p, struct netif *inp)
 This function is called by the network interface device driver when an IPv6 packet is received. More...
 
err_t ip6_options_add_hbh_ra (struct pbuf *p, u8_t nexth, u8_t value)
 Add a hop-by-hop options header with a router alert option and padding. More...
 
err_t ip6_output (struct pbuf *p, ip6_addr_t *src, ip6_addr_t *dest, u8_t hl, u8_t tc, u8_t nexth)
 Simple interface to ip6_output_if. More...
 
err_t ip6_output_if (struct pbuf *p, ip6_addr_t *src, ip6_addr_t *dest, u8_t hl, u8_t tc, u8_t nexth, struct netif *netif)
 Sends an IPv6 packet on a network interface. More...
 
err_t ip6_output_if_src (struct pbuf *p, ip6_addr_t *src, ip6_addr_t *dest, u8_t hl, u8_t tc, u8_t nexth, struct netif *netif)
 Same as ip6_output_if() but 'src' address is not replaced by netif address when it is 'any'. More...
 
struct netifip6_route (struct ip6_addr *src, struct ip6_addr *dest)
 Finds the appropriate network interface for a given IPv6 address. More...
 
ip6_addr_tip6_select_source_address (struct netif *netif, ip6_addr_t *dest)
 Select the best IPv6 source address for a given destination IPv6 address. More...
 

err_t ip6_input ( struct pbuf p,
struct netif inp 
)

This function is called by the network interface device driver when an IPv6 packet is received.

The function does the basic checks of the IP header such as packet size being at least larger than the header size etc. If the packet was not destined for us, the packet is forwarded (using ip6_forward).

Finally, the packet is sent to the upper layer protocol input function.

Parameters
pthe received IPv6 packet (p->payload points to IPv6 header)
inpthe netif on which this packet was received
Returns
ERR_OK if the packet was processed (could return ERR_* if it wasn't processed, but currently always returns ERR_OK)

References ip_globals::current_ip6_header, ip_globals::current_ip_header_tot_len, ip_globals::current_iphdr_dest, ip_globals::current_iphdr_src, ip_globals::current_netif, ERR_OK, icmp6_input(), icmp6_param_problem(), ICMP6_PP_HEADER, if(), ipX_addr_t::ip6, ip6_addr_cmp, ip6_addr_cmp_solicitednode, ip6_addr_copy, ip6_addr_isallnodes_iflocal, ip6_addr_isallnodes_linklocal, ip6_addr_isany, ip6_addr_islinklocal, ip6_addr_ismulticast, ip6_addr_issolicitednode, ip6_addr_isvalid, ip6_addr_set_any, ip6_current_dest_addr, ip6_current_src_addr, ip6_debug_print, IP6_FRAG_MORE_FLAG, IP6_FRAG_OFFSET_MASK, IP6_FRAG_STATS_INC, IP6_HLEN, IP6_NEXTH_DESTOPTS, IP6_NEXTH_FRAGMENT, IP6_NEXTH_HOPBYHOP, IP6_NEXTH_ICMP6, IP6_NEXTH_NONE, IP6_NEXTH_ROUTING, IP6_NEXTH_TCP, IP6_NEXTH_UDP, IP6_NEXTH_UDPLITE, ip6_reass(), IP6_STATS_INC, IP6H_NEXTH, IP6H_PLEN, IP6H_V, ip_data, pbuf::len, LWIP_DBG_LEVEL_SERIOUS, LWIP_DBG_LEVEL_WARNING, LWIP_DBG_TRACE, LWIP_DEBUGF, mld6_lookfor_group(), netif::name, netif_ip6_addr, netif_ip6_addr_state, netif_is_up, netif_list, netif::next, NULL, pbuf::payload, pbuf_free(), pbuf_header(), pbuf_realloc(), raw_input(), tcp_input(), pbuf::tot_len, U16_F, U32_F, and udp_input().

Referenced by ethernet_input(), and tcpip_thread().

err_t ip6_options_add_hbh_ra ( struct pbuf p,
u8_t  nexth,
u8_t  value 
)

Add a hop-by-hop options header with a router alert option and padding.

Used by MLD when sending a Multicast listener report/done message.

Parameters
pthe packet to which we will prepend the options header
nexththe next header protocol number (e.g. IP6_NEXTH_ICMP6)
valuethe value of the router alert option data (e.g. IP6_ROUTER_ALERT_VALUE_MLD)
Returns
ERR_OK if hop-by-hop header was added, ERR_* otherwise

References ERR_BUF, ERR_OK, IP6_PADN_ALERT_OPTION, IP6_ROUTER_ALERT_OPTION, IP6_STATS_INC, LWIP_DEBUGF, pbuf::payload, and pbuf_header().

Referenced by mld6_send().

err_t ip6_output ( struct pbuf p,
ip6_addr_t src,
ip6_addr_t dest,
u8_t  hl,
u8_t  tc,
u8_t  nexth 
)

Simple interface to ip6_output_if.

It finds the outgoing network interface and calls upon ip6_output_if to do the actual work.

Parameters
pthe packet to send (p->payload points to the data, e.g. next protocol header; if dest == IP_HDRINCL, p already includes an IPv6 header and p->payload points to that IPv6 header)
srcthe source IPv6 address to send from (if src == IP6_ADDR_ANY, an IP address of the netif is selected and used as source address. if src == NULL, IP6_ADDR_ANY is used as source)
destthe destination IPv6 address to send the packet to
hlthe Hop Limit value to be set in the IPv6 header
tcthe Traffic Class value to be set in the IPv6 header
nexththe Next Header to be set in the IPv6 header
Returns
ERR_RTE if no route is found see ip_output_if() for more return values

References ERR_RTE, IP6_ADDR_BLOCK1, IP6_ADDR_BLOCK2, IP6_ADDR_BLOCK3, IP6_ADDR_BLOCK4, IP6_ADDR_BLOCK5, IP6_ADDR_BLOCK6, IP6_ADDR_BLOCK7, IP6_ADDR_BLOCK8, ip6_addr_copy, ip6_output_if(), ip6_route(), IP6_STATS_INC, IP_HDRINCL, LWIP_DEBUGF, LWIP_IP_CHECK_PBUF_REF_COUNT_FOR_TX, NULL, and pbuf::payload.

err_t ip6_output_if ( struct pbuf p,
ip6_addr_t src,
ip6_addr_t dest,
u8_t  hl,
u8_t  tc,
u8_t  nexth,
struct netif netif 
)

Sends an IPv6 packet on a network interface.

This function constructs the IPv6 header. If the source IPv6 address is NULL, the IPv6 "ANY" address is used as source (usually during network startup). If the source IPv6 address it IP6_ADDR_ANY, the most appropriate IPv6 address of the outgoing network interface is filled in as source address. If the destination IPv6 address is IP_HDRINCL, p is assumed to already include an IPv6 header and p->payload points to it instead of the data.

Parameters
pthe packet to send (p->payload points to the data, e.g. next protocol header; if dest == IP_HDRINCL, p already includes an IPv6 header and p->payload points to that IPv6 header)
srcthe source IPv6 address to send from (if src == IP6_ADDR_ANY, an IP address of the netif is selected and used as source address. if src == NULL, IP6_ADDR_ANY is used as source)
destthe destination IPv6 address to send the packet to
hlthe Hop Limit value to be set in the IPv6 header
tcthe Traffic Class value to be set in the IPv6 header
nexththe Next Header to be set in the IPv6 header
netifthe netif on which to send this packet
Returns
ERR_OK if the packet was sent OK ERR_BUF if p doesn't have enough space for IPv6/LINK headers returns errors returned by netif->output

References ERR_RTE, ip6_addr_isany, ip6_output_if_src(), ip6_select_source_address(), IP6_STATS_INC, IP_HDRINCL, LWIP_DBG_LEVEL_SERIOUS, LWIP_DEBUGF, and NULL.

Referenced by icmp6_input(), icmp6_send_response(), ip6_output(), mld6_send(), nd6_send_na(), nd6_send_ns(), and nd6_send_rs().

struct netif* ip6_route ( struct ip6_addr src,
struct ip6_addr dest 
)

Finds the appropriate network interface for a given IPv6 address.

It tries to select a netif following a sequence of heuristics: 1) if there is only 1 netif, return it 2) if the destination is a link-local address, try to match the src address to a netif. this is a tricky case because with multiple netifs, link-local addresses only have meaning within a particular subnet/link. 3) tries to match the destination subnet to a configured address 4) tries to find a router 5) tries to match the source address to the netif 6) returns the default netif, if configured

Parameters
srcthe source IPv6 address, if known
destthe destination IPv6 address for which to find the route
Returns
the netif on which to send to reach dest

References default_router_list, ip6_addr_cmp, ip6_addr_isany, ip6_addr_islinklocal, ip6_addr_isvalid, ip6_addr_netcmp, nd6_select_router(), nd6_router_list_entry::neighbor_entry, nd6_neighbor_cache_entry::netif, netif_default, netif_ip6_addr, netif_ip6_addr_state, netif_list, netif::next, and NULL.

Referenced by icmp6_send_response(), and ip6_output().

ip6_addr_t* ip6_select_source_address ( struct netif netif,
ip6_addr_t dest 
)

Select the best IPv6 source address for a given destination IPv6 address.

Loosely follows RFC 3484. "Strong host" behavior is assumed.

Parameters
netifthe netif on which to send a packet
destthe destination we are trying to reach
Returns
the most suitable source address to use, or NULL if no suitable source address is found

References ip6_addr_isglobal, ip6_addr_islinklocal, ip6_addr_ismulticast_global, ip6_addr_ismulticast_iflocal, ip6_addr_ismulticast_linklocal, ip6_addr_ismulticast_orglocal, ip6_addr_ismulticast_sitelocal, ip6_addr_issitelocal, ip6_addr_isuniquelocal, ip6_addr_isvalid, ip6_addr_netcmp, netif_ip6_addr, netif_ip6_addr_state, and NULL.

Referenced by icmp6_input(), icmp6_send_response(), and ip6_output_if().