Data Structures | |
struct | tstrEthInitParam |
Structure to hold ethernet interface parameters. More... | |
struct | tstrM2MDataBufCtrl |
Structure holding the incoming buffer's data size information, indicating the data size of the buffer and the remaining buffer's data size . The data of the buffer which holds the packet sent to the host is placed in the tstrEthInitParam structure in the au8ethRcvBuf attribute. This following information is retreived in the host when an event M2M_WIFI_RESP_ETHERNET_RX_PACKET is received in the wi-fi callback function tpfAppWifiCb. More... | |
struct | tstrWifiInitParam |
Structure, holding the Wi-Fi configuration attributes such as the Wi-Fi callback, monitoring mode callback and Ethernet parameter initialization structure.More... | |
union | tuCtrlStruct |
Typedefs | |
typedef void(* | tpfAppEthCb )(uint8 u8MsgType, void *pvMsg, void *pvCtrlBuf) |
Ethernet notification callback function receiving events as defined in the Wi-Fi reponses enumeration tenuM2mStaCmd. More... | |
typedef void(* | tpfAppMonCb )(tstrM2MWifiRxPacketInfo *pstrWifiRxPacket, uint8 *pu8Payload, uint16 u16PayloadSize) |
Wi-Fi monitoring mode callback function. This function delivers all received wi-Fi packets through the Wi-Fi interface. Applications requiring to operate in the monitoring should call the asynchronous function m2m_wifi_enable_monitoring_mode and expect to receive the wi-fi packets through this callback function, when the event ....is received. To disable the monitoring mode a call to m2m_wifi_disable_monitoring_mode should be made. More... | |
typedef void(* | tpfAppWifiCb )(uint8 u8MsgType, void *pvMsg) |
Wi-Fi's main callback function handler, for handling the M2M_WIFI events received on the Wi-Fi interface. Such notifications are received in response to Wi-Fi/P2P operations such as m2m_wifi_request_scan, m2m_wifi_connect. Wi-Fi/P2P operations are implemented in an asynchronous mode, and all incoming information/status are to be handled through this callback function when the corresponding notification is received. Applications are expected to assign this wi-fi callback function by calling m2m_wifi_init. More... | |
Enumerations | |
enum | tenuSubTypes { ASSOC_REQ = 0x00, ASSOC_RSP = 0x10, REASSOC_REQ = 0x20, REASSOC_RSP = 0x30, PROBE_REQ = 0x40, PROBE_RSP = 0x50, BEACON = 0x80, ATIM = 0x90, DISASOC = 0xA0, AUTH = 0xB0, DEAUTH = 0xC0, ACTION = 0xD0, PS_POLL = 0xA4, RTS = 0xB4, CTS = 0xC4, ACK = 0xD4, CFEND = 0xE4, CFEND_ACK = 0xF4, BLOCKACK_REQ = 0x84, BLOCKACK = 0x94, DATA = 0x08, DATA_ACK = 0x18, DATA_POLL = 0x28, DATA_POLL_ACK = 0x38, NULL_FRAME = 0x48, CFACK = 0x58, CFPOLL = 0x68, CFPOLL_ACK = 0x78, QOS_DATA = 0x88, QOS_DATA_ACK = 0x98, QOS_DATA_POLL = 0xA8, QOS_DATA_POLL_ACK = 0xB8, QOS_NULL_FRAME = 0xC8, QOS_CFPOLL = 0xE8, QOS_CFPOLL_ACK = 0xF8 } |
Enumeration for Wi-Fi MAC Frame subtype code (6-bit). The frame subtypes fall into one of the three frame type groups as defined in tenuWifiFrameType (MANAGEMENT, CONTROL & DATA). Values are defined as per the IEEE 802.11 standard. More... | |
enum | tenuWifiFrameType { MANAGEMENT = 0x00, CONTROL = 0x04, DATA_BASICTYPE = 0x08, RESERVED = 0x0C } |
Enumeration for Wi-Fi MAC frame type codes (2-bit) The following types are used to identify the type of frame sent or received. Each frame type constitues a number of frame subtypes as defined in tenuSubTypes to specify the exact type of frame. Values are defined as per the IEEE 802.11 standard. More... | |
Functions | |
NMI_API sint8 | m2m_wifi_allow_p2p_connection () |
NMI_API sint8 | m2m_wifi_ap_add_black_list (uint8 bAddNewEntry, uint8 *mac_addr) |
NMI_API sint8 | m2m_wifi_ap_get_assoc_info (void) |
Request the status information of the currently connected stations to the WILC1000 AP. The result is passed to the Wi-Fi notification callback with the event M2M_WIFI_RESP_AP_ASSOC_INFO. More... | |
NMI_API sint8 | m2m_wifi_change_monitoring_channel (uint8 u8ChannelID) |
NMI_API sint8 | m2m_wifi_connect (char *pcSsid, uint8 u8SsidLen, uint8 u8SecType, tuniM2MWifiAuth *puniAuthInfo, uint16 u16Ch) |
NMI_API sint8 | m2m_wifi_deinit (void *arg) |
NMI_API sint8 | m2m_wifi_disable_ap (void) |
NMI_API sint8 | m2m_wifi_disable_monitoring_mode (void) |
NMI_API sint8 | m2m_wifi_disconnect (void) |
NMI_API sint8 | m2m_wifi_enable_ap (CONST tstrM2MAPConfig *pstrM2MAPConfig) |
NMI_API sint8 | m2m_wifi_enable_monitoring_mode (tstrM2MWifiMonitorModeCtrl *pstrMtrCtrl) |
NMI_API sint8 | m2m_wifi_get_connection_info (void) |
Request the status information of the currently connected Wi-Fi AP. The result is passed to the Wi-Fi notification callback with the event M2M_WIFI_RESP_CONN_INFO. More... | |
NMI_API sint8 | m2m_wifi_get_mac_address (uint8 *pu8MacAddr0, uint8 *pu8MacAddr1) |
Request the current MAC addresses of the device (the working mac addresses). (the function is Blocking until response received) More... | |
NMI_API uint8 | m2m_wifi_get_num_ap_found (void) |
Reads the number of AP's found in the last Scan Request, The function read the number of AP's from global variable which updated in the wifi_cb in M2M_WIFI_RESP_SCAN_DONE. More... | |
NMI_API sint8 | m2m_wifi_get_otp_mac_address (uint8 *pu8MacAddr, uint8 *pu8IsValid) |
Request the MAC address stored on the OTP (one time programmable) memory of the device. (the function is Blocking until response received) More... | |
NMI_API uint8 | m2m_wifi_get_sleep_mode (void) |
Get the current Power save mode. More... | |
NMI_API sint8 | m2m_wifi_handle_events (void *arg) |
NMI_API sint8 | m2m_wifi_init (tstrWifiInitParam *pWifiInitParam) |
NMI_API sint8 | m2m_wifi_p2p (uint8 u8Channel, tenuP2PTrigger enuTrigger, uint16 u16WPS_CfgMehods) |
NMI_API sint8 | m2m_wifi_p2p_disconnect (void) |
NMI_API sint8 | m2m_wifi_req_curr_rssi (void) |
Request the current RSSI for the current connected AP, the response received in wifi_cb M2M_WIFI_RESP_CURRENT_RSSI. More... | |
NMI_API sint8 | m2m_wifi_req_scan_result (uint8 index) |
Reads the AP information from the Scan Result list with the given index, the response received in wifi_cb M2M_WIFI_RESP_SCAN_RESULT, the response pointer should be casted with tstrM2mWifiscanResult structure. More... | |
NMI_API sint8 | m2m_wifi_request_scan (uint8 ch) |
NMI_API sint8 | m2m_wifi_request_scan_ssid (uint8 ch, char *pcssid) |
NMI_API sint8 | m2m_wifi_send_ethernet_pkt (uint8 *pu8Packet, uint16 u16PacketSize, uint8 u8IfcId) |
NMI_API sint8 | m2m_wifi_send_wlan_pkt (uint8 *pu8WlanPacket, uint16 u16WlanHeaderLength, uint16 u16WlanPktSize) |
NMI_API sint8 | m2m_wifi_set_lsn_int (tstrM2mLsnInt *pstrM2mLsnInt) |
Set the Wi-Fi listen interval for power save operation. It is represented in units of AP Beacon periods. More... | |
NMI_API sint8 | m2m_wifi_set_mac_address (uint8 au8MacAddress0[6], uint8 au8MacAddress1[6]) |
Assign MAC addresses to the WILC device. More... | |
NMI_API sint8 | m2m_wifi_set_p2p_pin (uint8 *pu8PinNumber, uint8 u8PinLength) |
NMI_API sint8 | m2m_wifi_set_scan_list (tstrM2MScanList *pstrScanList) |
NMI_API sint8 | m2m_wifi_set_scan_options (uint8 u8NumOfSlot, uint8 u8SlotTime) |
NMI_API sint8 | m2m_wifi_set_scan_region (uint8 ScanRegion) |
NMI_API sint8 | m2m_wifi_set_sleep_mode (uint8 PsTyp, uint8 BcastEn) |
Set the power saving mode for the WILC1000. More... | |
NMI_API sint8 | m2m_wifi_wps (uint8 u8TriggerType, const char *pcPinNumber) |
NMI_API sint8 | m2m_wifi_wps_disable (void) |
Disable the WILC WPS operation. More... | |
NMI_API sint8 | m2m_wifi_set_device_name (uint8 *pu8DeviceName, uint8 u8DeviceNameLength) |
Set the WILC1000 device name which is used as P2P device name. More... | |
[in] | None |
References m2m_wifi_set_p2p_pin().