Microchip® Advanced Software Framework

application.c File Reference
#include "application.h"
#include "FreeRTOS.h"
#include "osprintf.h"
#include "os/include/net_init.h"
#include "os/include/m2m_wifi_ex.h"

Data Structures

struct  s_msg_wifi_product
 Message format definitions. More...
 

Typedefs

typedef struct s_msg_wifi_product t_msg_wifi_product
 Message format definitions. More...
 

Functions

void http_connection (char *host_name, uint16 port)
 
void tcp_client ()
 
void tcp_server ()
 
void udp_client ()
 
void udp_server ()
 
static void wifi_cb (uint8_t u8MsgType, void *pvMsg)
 Callback to get the Wi-Fi status update. More...
 
static void wifi_monitoring_cb (tstrM2MWifiRxPacketInfo *pstrWifiRxPacket, uint8 *pu8Payload, uint16 u16PayloadSize)
 
void wilc_task_1 (void *argument)
 AT commands main function. More...
 

Variables

xSemaphoreHandle at_cmd_task1_sem
 
static xSemaphoreHandle firmware_start_sem = NULL
 Firmware start event. More...
 
tstrMonstats gstrMonitorControlStats
 
tstrMonstats gstrMonitorDataStats
 
tstrMonstats gstrMonitorMangementStats
 
uint32_t local_ip
 
static t_msg_wifi_product msg_wifi_product
 Message format declarations. More...
 
static int npkt =0
 
uint8 u8ControlSubtype [AT_MAX_CONTROL_SUBTYPE]
 
uint8 u8DataSubType [AT_MAX_DATA_SUBTYPE]
 
uint8 u8MangmentSubtype [AT_MAX_MANGEMENT_SUBTYPE]
 

Message format definitions.

static void wifi_cb ( uint8_t  u8MsgType,
void pvMsg 
)
static

Callback to get the Wi-Fi status update.

Parameters
[in]u8MsgTypetype of Wi-Fi notification. Possible types are:
[in]pvMsgA pointer to a buffer containing the notification parameters (if any). It should be casted to the correct data type corresponding to the notification type.

References tstrM2MConnInfo::acSSID, AP_INTERFACE, AT_INDEX_RSSI, AT_MAX_CMD_LENGTH, AT_SEND_OK, tstrM2mWifiscanResult::au8BSSID, tstrM2MWPSInfo::au8PSK, tstrM2MWPSInfo::au8SSID, tstrM2mWifiscanResult::au8SSID, CONF_METHOD_DISPLAY, CONF_METHOD_KEYPAD, firmware_start_sem, get_cmd_txt(), gstrAllStatus, htons, IP4_ADDR, local_ip, M2M_INFO, m2m_strlen(), M2M_SUCCESS, m2m_wifi_allow_p2p_connection(), M2M_WIFI_CONNECTED, M2M_WIFI_DISCONNECTED, m2m_wifi_get_mac_address(), M2M_WIFI_REQ_P2P_AUTH, m2m_wifi_req_scan_result(), m2m_wifi_request_dhcp_client_ex(), m2m_wifi_request_static_client_ex(), M2M_WIFI_RES_WPS, M2M_WIFI_RESP_CON_STATE_CHANGED, M2M_WIFI_RESP_CONN_INFO, M2M_WIFI_RESP_CURRENT_RSSI, M2M_WIFI_RESP_FIRMWARE_STRTED, M2M_WIFI_RESP_SCAN_DONE, M2M_WIFI_RESP_SCAN_RESULT, NET_IF_REQ_DHCP_CONF, NET_IF_STA, net_interface_down(), net_interface_up(), net_set_interface_address(), NULL, os_m2m_wifi_connect(), os_m2m_wifi_get_num_ap_found(), os_m2m_wifi_set_p2p_pin(), osprintf(), P2P_INTERFACE, tstrM2mWifiscanResult::s8rssi, tstrM2MConnInfo::s8RSSI, tstrM2mScanDone::s8ScanState, SERVICE_IS_RUNNING, SERVICE_IS_STOPPED, StaticIPcfg, STATION_INTERFACE, tstrM2MP2pDevInfo::u16CfgMethods, tstrM2MIPConfig::u32Gateway, tstrM2MIPConfig::u32StaticIP, connect_status::u8Ap_status, tstrM2MWPSInfo::u8AuthType, tstrM2mWifiscanResult::u8AuthType, tstrM2MWPSInfo::u8Ch, tstrM2mWifiscanResult::u8ch, tstrM2mWifiStateChanged::u8CurrState, tstrM2mWifiStateChanged::u8IfcId, tstrM2mWifiscanResult::u8index, tstrM2mWifiStateChanged::u8MAcAddr, tstrM2mScanDone::u8NumofCh, tstrM2MConnInfo::u8SecType, connect_status::u8Sta_status, tstrM2MIPConfig2::u8StaticIP, tstrM2MIPConfig2::u8StaticIPv6, use_static_IP, vTaskDelay(), and xSemaphoreGive.

Referenced by wilc_task_1().

xSemaphoreHandle firmware_start_sem = NULL
static

Firmware start event.

Referenced by wifi_cb(), and wilc_task_1().

tstrMonstats gstrMonitorControlStats
tstrMonstats gstrMonitorDataStats
tstrMonstats gstrMonitorMangementStats
t_msg_wifi_product msg_wifi_product
static
Initial value:
= {
}
#define MAIN_WIFI_M2M_PRODUCT_NAME
Definition: application.h:44

Message format declarations.

int npkt =0
static

Referenced by wifi_monitoring_cb().

uint8 u8ControlSubtype[AT_MAX_CONTROL_SUBTYPE]

Referenced by wifi_monitoring_cb().

uint8 u8DataSubType[AT_MAX_DATA_SUBTYPE]

Referenced by wifi_monitoring_cb().

uint8 u8MangmentSubtype[AT_MAX_MANGEMENT_SUBTYPE]

Referenced by wifi_monitoring_cb().