WILC Application Interface Internal Types.
Copyright (c) 2016-2021 Microchip Technology Inc. and its subsidiaries.
#include "common/include/nm_common.h"
Data Structures | |
struct | tstr1xAuthCredentials |
Credentials for the user to authenticate with the AAA server (WPA-Enterprise Mode IEEE802.1x). More... | |
struct | tstrM2mAntDivParams |
struct | tstrM2MAPAssocInfo |
M2M association information of the connected station in the AP mode. More... | |
struct | tstrM2MAPConfig |
AP Configuration. More... | |
struct | tstrM2MAssocEntryInfo |
M2M association information of of an assoicated entry in the AP mode. More... | |
struct | tstrM2MConnInfo |
M2M Provisioning Information obtained from the HTTP Provisioning server. More... | |
struct | tstrM2MDeviceNameConfig |
Device name. More... | |
struct | tstrM2MIfId |
Set Intrface ID. More... | |
struct | tstrM2MIPConfig |
Static IP configuration. More... | |
struct | tstrM2mIpRsvdPkt |
Received Packet Size and Data Offset. More... | |
struct | tstrM2mLsnInt |
Listen interval. More... | |
struct | tstrM2MMulticastMac |
M2M add/remove multicast mac address. More... | |
struct | tstrM2MP2PConnect |
Set the device to operate in the Wi-Fi Direct (P2P) mode. More... | |
struct | tstrM2MP2pDevInfo |
P2P Pin. More... | |
struct | tstrM2MPinInfo |
PIN Number (input) More... | |
struct | tstrM2mPsType |
Power Save Configuration. More... | |
struct | tstrM2mReqHTEnable |
HT (High Throughput) enable (default) or disable. More... | |
struct | tstrM2mReqScanResult |
Scan Result Request. More... | |
struct | tstrM2MScan |
Wi-Fi Scan Request. More... | |
struct | tstrM2mScanDone |
Wi-Fi Scan Result. More... | |
struct | tstrM2MScanList |
Wi-Fi channel list regulation. More... | |
struct | tstrM2MScanOption |
struct | tstrM2MScanRegion |
Wi-Fi channel regulation region information. More... | |
struct | tstrM2mSetMacAddress |
Sets the MAC address from application. It is only intended for testing purpose. This method is not used for production SW. Production SW reads MAC Address from EFUSE. More... | |
struct | tstrM2mTxPwrLevel |
Tx power level. More... | |
struct | tstrM2MUserMaxTxRate |
User specified Max Tx Rate. More... | |
struct | tstrM2mWifiConnect |
Wi-Fi Connect Request. More... | |
struct | tstrM2MWifiMonitorModeCtrl |
Wi-Fi Monitor Mode Filter. More... | |
struct | tstrM2MWifiRxPacketInfo |
Wi-Fi RX Frame Header. More... | |
struct | tstrM2mWifiscanResult |
Wi-Fi Scan Result. More... | |
struct | tstrM2MWifiSecInfo |
Authentication credentials to connect to a Wi-Fi network. More... | |
struct | tstrM2mWifiStateChanged |
Wi-Fi Connection State. More... | |
struct | tstrM2MWifiTxPacketInfo |
Wi-Fi Tx Packet Info. More... | |
struct | tstrM2mWifiWepParams |
WEP security key parameters. More... | |
struct | tstrM2MWPSConnect |
WPS Configuration parameters. More... | |
struct | tstrM2MWPSInfo |
WPS Result. More... | |
struct | tstrSystemTime |
Used for time storage. More... | |
union | tuniM2MWifiAuth |
Wi-Fi Security Parameters for all supported security modes. More... | |