#include "AWS_SDK/aws_iot_src/utils/aws_iot_error.h"
#include "AWS_SDK/aws_iot_src/utils/aws_iot_log.h"
#include "aws_iot_shadow_actions.h"
#include "aws_iot_shadow_json.h"
#include "aws_iot_shadow_key.h"
#include "aws_iot_shadow_records.h"
Functions | |
IoT_Error_t | aws_iot_shadow_connect (MQTTClient_t *pClient, ShadowParameters_t *pParams) |
Connect to the AWS IoT Thing Shadow service over MQTT. More... | |
IoT_Error_t | aws_iot_shadow_delete (MQTTClient_t *pClient, const char *pThingName, fpActionCallback_t callback, void *pContextData, uint8_t timeout_seconds, bool isPersistentSubscribe) |
This function is the one used to perform an Delete action to a Thing Name's Shadow. More... | |
void | aws_iot_shadow_disable_discard_old_delta_msgs (void) |
Disable the ignoring of delta messages with old version number. More... | |
IoT_Error_t | aws_iot_shadow_disconnect (MQTTClient_t *pClient) |
Disconnect from the AWS IoT Thing Shadow service over MQTT. More... | |
void | aws_iot_shadow_enable_discard_old_delta_msgs (void) |
Enable the ignoring of delta messages with old version number. More... | |
IoT_Error_t | aws_iot_shadow_get (MQTTClient_t *pClient, const char *pThingName, fpActionCallback_t callback, void *pContextData, uint8_t timeout_seconds, bool isPersistentSubscribe) |
This function is the one used to perform an Get action to a Thing Name's Shadow. More... | |
uint32_t | aws_iot_shadow_get_last_received_version (void) |
Version of a document is received with every accepted/rejected and the SDK keeps track of the last received version of the JSON document of AWS_IOT_MY_THING_NAME shadow. More... | |
IoT_Error_t | aws_iot_shadow_init (MQTTClient_t *pClient) |
Initialize the Thing Shadow before use. More... | |
IoT_Error_t | aws_iot_shadow_register_delta (MQTTClient_t *pClient, jsonStruct_t *pStruct) |
This function is used to listen on the delta topic of AWS_IOT_MY_THING_NAME mentioned in the aws_iot_config.h file. More... | |
void | aws_iot_shadow_reset_last_received_version (void) |
Reset the last received version number to zero. More... | |
IoT_Error_t | aws_iot_shadow_update (MQTTClient_t *pClient, const char *pThingName, char *pJsonString, fpActionCallback_t callback, void *pContextData, uint8_t timeout_seconds, bool isPersistentSubscribe) |
This function is the one used to perform an Update action to a Thing Name's Shadow. More... | |
IoT_Error_t | aws_iot_shadow_yield (MQTTClient_t *pClient, int timeout) |
Yield function to let the background tasks of MQTT and Shadow. More... | |
Variables | |
const ShadowParameters_t | ShadowParametersDefault |
IoT_Error_t aws_iot_shadow_connect | ( | MQTTClient_t * | pClient, |
ShadowParameters_t * | pParams | ||
) |
Connect to the AWS IoT Thing Shadow service over MQTT.
This function does the TLSv1.2 handshake and establishes the MQTT connection
pClient | MQTT Client used as the protocol layer |
pParams | Shadow Conenction parameters like TLS cert location |
References MQTTClient_t::connect, DEBUG, MQTTConnectParams::disconnectHandler, initializeRecords(), MQTTConnectParams::isCleansession, MQTTConnectParams::isSSLHostnameVerify, MQTTConnectParams::isWillMsgPresent, MQTTConnectParams::KeepAliveInterval_sec, MAX_SIZE_OF_THING_NAME, MAX_SIZE_OF_UNIQUE_CLIENT_ID_BYTES, MQTT_3_1_1, mqttClientID, MQTTConnectParams::mqttCommandTimeout_ms, MQTTConnectParamsDefault, MQTTConnectParams::MQTTVersion, myThingName, NONE_ERROR, NULL, NULL_VALUE_ERROR, ShadowParameters_t::pClientCRT, MQTTConnectParams::pClientID, ShadowParameters_t::pClientKey, MQTTConnectParams::pDeviceCertLocation, MQTTConnectParams::pDevicePrivateKeyLocation, ShadowParameters_t::pHost, MQTTConnectParams::pHostURL, ShadowParameters_t::pMqttClientId, ShadowParameters_t::pMyThingName, ShadowParameters_t::port, MQTTConnectParams::port, MQTTConnectParams::pPassword, ShadowParameters_t::pRootCA, MQTTConnectParams::pRootCALocation, MQTTConnectParams::pUserName, and MQTTConnectParams::tlsHandshakeTimeout_ms.
IoT_Error_t aws_iot_shadow_delete | ( | MQTTClient_t * | pClient, |
const char * | pThingName, | ||
fpActionCallback_t | callback, | ||
void * | pContextData, | ||
uint8_t | timeout_seconds, | ||
bool | isPersistentSubscriptions | ||
) |
This function is the one used to perform an Delete action to a Thing Name's Shadow.
This is not a very common use case for device. It is generally the responsibility of the accompanying app to do the delete. It is similar to the Update function internally except it does not take a JSON document as the input. The Thing Shadow referred by the ThingName will be deleted.
pClient | MQTT Client used as the protocol layer |
pThingName | Thing Name of the Shadow that should be deleted |
callback | This is the callback that will be used to inform the caller of the response from the AWS IoT Shadow service.Callback could be set to NULL if response is not important |
pContextData | This is an extra parameter that could be passed along with the callback. It should be set to NULL if not used |
timeout_seconds | It is the time the SDK will wait for the response on either accepted/rejected before declaring timeout on the action |
isPersistentSubscribe | As mentioned above, every time if a device deletes the same Sahdow (JSON document) then this should be set to true to avoid repeated subscription and un-subscription. If the Thing Name is one off delete then this should be set to false |
References CONNECTION_ERROR, iot_shadow_action(), iot_shadow_delete_request_json(), MQTTClient_t::isConnected, MAX_SIZE_CLIENT_TOKEN_CLIENT_SEQUENCE, NONE_ERROR, and SHADOW_DELETE.
void aws_iot_shadow_disable_discard_old_delta_msgs | ( | void | ) |
Disable the ignoring of delta messages with old version number.
References shadowDiscardOldDeltaFlag.
IoT_Error_t aws_iot_shadow_disconnect | ( | MQTTClient_t * | pClient | ) |
Disconnect from the AWS IoT Thing Shadow service over MQTT.
This will close the underlying TCP connection, MQTT connection will also be closed
pClient | MQTT Client used as the protocol layer |
References MQTTClient_t::disconnect.
void aws_iot_shadow_enable_discard_old_delta_msgs | ( | void | ) |
Enable the ignoring of delta messages with old version number.
As we use MQTT underneath, there could be more than 1 of the same message if we use QoS 0. To avoid getting called for the same message, this functionality should be enabled. All the old message will be ignored
References shadowDiscardOldDeltaFlag.
IoT_Error_t aws_iot_shadow_get | ( | MQTTClient_t * | pClient, |
const char * | pThingName, | ||
fpActionCallback_t | callback, | ||
void * | pContextData, | ||
uint8_t | timeout_seconds, | ||
bool | isPersistentSubscribe | ||
) |
This function is the one used to perform an Get action to a Thing Name's Shadow.
One use of this function is usually to get the config of a device at boot up. It is similar to the Update function internally except it does not take a JSON document as the input. The entire JSON document will be sent over the accepted topic
pClient | MQTT Client used as the protocol layer |
pThingName | Thing Name of the JSON document that is needed |
callback | This is the callback that will be used to inform the caller of the response from the AWS IoT Shadow service.Callback could be set to NULL if response is not important |
pContextData | This is an extra parameter that could be passed along with the callback. It should be set to NULL if not used |
timeout_seconds | It is the time the SDK will wait for the response on either accepted/rejected before declaring timeout on the action |
isPersistentSubscribe | As mentioned above, every time if a device gets the same Sahdow (JSON document) then this should be set to true to avoid repeated subscription and un-subscription. If the Thing Name is one off get then this should be set to false |
References CONNECTION_ERROR, iot_shadow_action(), iot_shadow_get_request_json(), MQTTClient_t::isConnected, MAX_SIZE_CLIENT_TOKEN_CLIENT_SEQUENCE, NONE_ERROR, and SHADOW_GET.
uint32_t aws_iot_shadow_get_last_received_version | ( | void | ) |
Version of a document is received with every accepted/rejected and the SDK keeps track of the last received version of the JSON document of AWS_IOT_MY_THING_NAME shadow.
One exception to this version tracking is that, the SDK will ignore the version from update/accepted topic. Rest of the responses will be scanned to update the version number. Accepting version change for update/accepted may cause version conflicts for delta message if the update message is received before the delta.
References shadowJsonVersionNum.
IoT_Error_t aws_iot_shadow_init | ( | MQTTClient_t * | pClient | ) |
Initialize the Thing Shadow before use.
This function takes care of initializing the internal book-keeping data structures
pClient | MQTT Client used as the protocol layer |
References aws_iot_shadow_reset_last_received_version(), initDeltaTokens(), NONE_ERROR, NULL, NULL_VALUE_ERROR, and resetClientTokenSequenceNum().
IoT_Error_t aws_iot_shadow_register_delta | ( | MQTTClient_t * | pClient, |
jsonStruct_t * | pStruct | ||
) |
This function is used to listen on the delta topic of AWS_IOT_MY_THING_NAME mentioned in the aws_iot_config.h file.
Any time a delta is published the Json document will be delivered to the pStruct->cb. If you don't want the parsing done by the SDK then use the jsonStruct_t key set to "state". A good example of this is displayed in the sample_apps/shadow_console_echo.c
pClient | MQTT Client used as the protocol layer |
pStruct | The struct used to parse JSON value |
References CONNECTION_ERROR, MQTTClient_t::isConnected, NONE_ERROR, and registerJsonTokenOnDelta().
void aws_iot_shadow_reset_last_received_version | ( | void | ) |
Reset the last received version number to zero.
This will be useful if the Thing Shadow is deleted and would like to to reset the local version
References shadowJsonVersionNum.
Referenced by aws_iot_shadow_init().
IoT_Error_t aws_iot_shadow_update | ( | MQTTClient_t * | pClient, |
const char * | pThingName, | ||
char * | pJsonString, | ||
fpActionCallback_t | callback, | ||
void * | pContextData, | ||
uint8_t | timeout_seconds, | ||
bool | isPersistentSubscribe | ||
) |
This function is the one used to perform an Update action to a Thing Name's Shadow.
update is one of the most frequently used functionality by a device. In most cases the device may be just reporting few params to update the thing shadow in the cloud Update Action if no callback or if the JSON document does not have a client token then will just publish the update and not track it.
aws_iot_shadow_yield()
function the response will be handled. In case of timeout or if the response is received, the subscription to shadow response topics are un-subscribed from. On the contrary if the persistent subscription is set to true then the un-subscribe will not be done. The topics will always be listened to.pClient | MQTT Client used as the protocol layer |
pThingName | Thing Name of the shadow that needs to be Updated |
pJsonString | The update action expects a JSON document to send. The JSO String should be a null terminated string. This JSON document should adhere to the AWS IoT Thing Shadow specification. To help in the process of creating this document- SDK provides apis in aws_iot_shadow_json_data.h |
callback | This is the callback that will be used to inform the caller of the response from the AWS IoT Shadow service.Callback could be set to NULL if response is not important |
pContextData | This is an extra parameter that could be passed along with the callback. It should be set to NULL if not used |
timeout_seconds | It is the time the SDK will wait for the response on either accepted/rejected before declaring timeout on the action |
isPersistentSubscribe | As mentioned above, every time if a device updates the same shadow then this should be set to true to avoid repeated subscription and unsubscription. If the Thing Name is one off update then this should be set to false |
References CONNECTION_ERROR, iot_shadow_action(), MQTTClient_t::isConnected, NONE_ERROR, and SHADOW_UPDATE.
IoT_Error_t aws_iot_shadow_yield | ( | MQTTClient_t * | pClient, |
int | timeout | ||
) |
Yield function to let the background tasks of MQTT and Shadow.
This function could be use in a separate thread waiting for the incoming messages, ensuring the connection is kept alive with the AWS Service. It also ensures the expired requests of Shadow actions are cleared and Timeout callback is executed.
pClient | MQTT Client used as the protocol layer |
timeout | in milliseconds, This is the maximum time the yield function will wait for a message and/or read the messages from the TLS buffer |
References HandleExpiredResponseCallbacks(), and MQTTClient_t::yield.
|
related |