Specific Enumeration-typedefs used for socket operations.
Modules | |
Asynchronous Events | |
Specific Enumeration used for asynchronous operations. | |
Data Structures | |
struct | in_addr |
For compatibility with BSD code. More... | |
struct | sockaddr |
Generic socket address structure. More... | |
struct | sockaddr_in |
Socket address structure for IPV4 addresses. Used to specify socket address information to connect to. Can be cast to sockaddr structure. More... | |
struct | tstrSockErr |
Detail about socket failures. Used with get_error_detail. More... | |
Typedefs | |
typedef sint8 | SOCKET |
Definition for socket handler data type. Socket ID,used with all socket operations to uniquely identify the socket handler. The ID is uniquely assigned at socket creation when calling socket operation. More... | |
typedef sint8 | SOCKET |
Enumerations | |
enum | tenuSockErrSource { SOCKET_ERR_UNKNOWN = 0, SOCKET_ERR_TLS_REMOTE, SOCKET_ERR_TLS_LOCAL } |
Source of socket error (local, remote or unknown). More... | |
Definition for socket handler data type. Socket ID,used with all socket operations to uniquely identify the socket handler. The ID is uniquely assigned at socket creation when calling socket operation.
enum tenuSockErrSource |
Source of socket error (local, remote or unknown).
Enumerator | |
---|---|
SOCKET_ERR_UNKNOWN |
No detail available (also used when there is no error). |
SOCKET_ERR_TLS_REMOTE |
TLS Error Alert received from peer. |
SOCKET_ERR_TLS_LOCAL |
TLS Error Alert generated locally. |