The function performs the necessary initializations for the socket library through the following steps:
Functions | |
NMI_API sint8 | accept (SOCKET sock, struct sockaddr *addr, uint8 *addrlen) |
NMI_API sint8 | bind (SOCKET sock, struct sockaddr *pstrAddr, uint8 u8AddrLen) |
NMI_API sint8 | close (SOCKET sock) |
Synchronous close function, releases all the socket assigned resources. More... | |
NMI_API sint8 | connect (SOCKET sock, struct sockaddr *pstrAddr, uint8 u8AddrLen) |
sint8 | get_alpn_index (SOCKET sock) |
sint8 | get_error_detail (SOCKET sock, tstrSockErr *pstrErr) |
NMI_API sint8 | gethostbyname (uint8 *pcHostName) |
NMI_API sint8 | getsockopt (SOCKET sock, uint8 u8Level, uint8 u8OptName, const void *pvOptValue, uint8 *pu8OptLen) |
Get socket options retrieves. This Function isn't implemented yet but this is the form that will be released later. More... | |
NMI_API uint8 | IsSocketReady (void) |
NMI_API sint8 | listen (SOCKET sock, uint8 backlog) |
NMI_API sint8 | m2m_ping_req (uint32 u32DstIP, uint8 u8TTL, tpfPingCb fpPingCb) |
The function request to send ping request to the given IP Address. More... | |
NMI_API uint32 | nmi_inet_addr (char *pcIpAddr) |
NMI_API sint16 | recv (SOCKET sock, void *pvRecvBuf, uint16 u16BufLen, uint32 u32Timeoutmsec) |
NMI_API sint16 | recvfrom (SOCKET sock, void *pvRecvBuf, uint16 u16BufLen, uint32 u32Timeoutmsec) |
NMI_API void | registerSocketCallback (tpfAppSocketCb socket_cb, tpfAppResolveCb resolve_cb) |
sint8 | secure (SOCKET sock) |
NMI_API sint16 | send (SOCKET sock, void *pvSendBuffer, uint16 u16SendLength, uint16 u16Flags) |
NMI_API sint16 | sendto (SOCKET sock, void *pvSendBuffer, uint16 u16SendLength, uint16 flags, struct sockaddr *pstrDestAddr, uint8 u8AddrLen) |
Asynchronous sending function, used to send data on a UDP socket. Called by the application code when there is data required to be sent on a UDP socket. More... | |
sint8 | set_alpn_list (SOCKET sock, const char *pcProtocolList) |
NMI_API sint8 | setsockopt (SOCKET socket, uint8 u8Level, uint8 option_name, const void *option_value, uint16 u16OptionLen) |
NMI_API SOCKET | socket (uint16 u16Domain, uint8 u8Type, uint8 u8Config) |
NMI_API void | socketDeinit (void) |
Socket Layer De-initialization. More... | |
NMI_API void | socketInit (void) |
The function has no current implementation. An empty declaration is used to prevent errors when legacy application code is used. As it has no effect, it can be safely removed from any application using it.
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | addr | Not used in the current implementation. |
[in] | addrlen | Not used in the current implementation. |
References MAX_SOCKET, SOCK_ERR_INVALID_ARG, and SOCK_ERR_NO_ERROR.
Referenced by tcp_accept().
Asynchronous bind function associates the provided address and local port to the socket. The function can be used with both TCP and UDP sockets. It is mandatory to call the @ref bind function before starting any UDP or TCP server operation. Upon socket bind completion, the application will receive a @ref SOCKET_MSG_BIND message in the socket callback.
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | pstrAddr | Pointer to socket address structure "sockaddr_in" sockaddr_in |
[in] | u8AddrLen | Size of the given socket address structure in bytes. |
This example demonstrates the call of the bind socket operation after a successful socket operation.
References m2m_memcpy(), MAX_SOCKET, NULL, tstrBindCmd::sock, SOCK_ERR_INVALID, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_CMD_BIND, SOCKET_REQUEST, tstrBindCmd::strAddr, tstrSockAddr::u16Family, tstrSockAddr::u16Port, tstrSocket::u16SessionID, tstrBindCmd::u16SessionID, and tstrSockAddr::u32IPAddr.
Synchronous close function, releases all the socket assigned resources.
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
References M2M_INFO, m2m_memset(), MAX_SOCKET, NULL, tstrCloseCmd::sock, SOCK_ERR_INVALID, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_CMD_CLOSE, SOCKET_CMD_SSL_CLOSE, SOCKET_REQUEST, SSL_FLAGS_ACTIVE, tstrCloseCmd::u16SessionID, and tstrSocket::u16SessionID.
Referenced by lwip_netconn_do_close_internal().
Establishes a TCP connection with a remote server. The asynchronous connect function must be called after receiving a valid socket ID from the @ref socket function. The application socket callback function is notified of the result of the connection attempt through the event @ref SOCKET_MSG_CONNECT, along with a structure @ref tstrSocketConnectMsg. If socket connection fails, the application should call @ref close(). A successful connect means the TCP session is active. The application is then required to make a call to the @ref recv function to receive any packets transmitted by the remote server, unless the application is interrupted by a notification of socket connection termination.
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | pstrAddr | Address of the remote server. |
[in] | u8AddrLen | Size of the given socket address structure in bytes. Not currently used, implemented for BSD compatibility only. |
The example demonstrates a TCP application, showing how the asynchronous call to the connect function is made through the main function and how the callback function handles the SOCKET_MSG_CONNECT event.
References m2m_memcpy(), MAX_SOCKET, NULL, tstrConnectCmd::sock, SOCK_ERR_INVALID, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_CMD_CONNECT, SOCKET_CMD_SSL_CONNECT, SOCKET_REQUEST, SSL_FLAGS_ACTIVE, tstrConnectCmd::strAddr, tstrSocket::u16SessionID, tstrConnectCmd::u16SessionID, tstrSocket::u8SSLFlags, and tstrConnectCmd::u8SslFlags.
This function gets the index of the protocol negotiated via ALPN. It should be called when a SSL socket connection succeeds, in order to determine which application-layer protocol must be used.
[in] | sock | Socket ID obtained by a call to socket. This is the SSL socket to which the ALPN applies. |
References SOCK_ERR_INVALID_ARG, SSL_FLAGS_ACTIVE, TCP_SOCK_MAX, and tstrSocket::u8AlpnStatus.
sint8 get_error_detail | ( | SOCKET | sock, |
tstrSockErr * | pstrErr | ||
) |
This function gets detail about a socket failure. The application can call this when notified of a socket failure via SOCKET_MSG_CONNECT or SOCKET_MSG_RECV. If used, it must be called before close.
[in] | sock | Socket ID obtained by a call to socket. |
[out] | pstrErr | Pointer to structure to be populated with the details of the socket failure. |
References tstrSockErr::enuErrSource, NULL, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, TCP_SOCK_MAX, tstrSocket::u8ErrCode, tstrSockErr::u8ErrCode, and tstrSocket::u8ErrSource.
Asynchronous DNS resolving function. This function uses DNS to resolve a domain name to the corresponding IP address. A call to this function will cause a DNS request to be sent and the response will be delivered to the DNS callback function registered using registerSocketCallback.
[in] | pcHostName | NULL terminated string containing the domain name for the remote host. Its size must not exceed HOSTNAME_MAX_SIZE. |
References HOSTNAME_MAX_SIZE, M2M_REQ_DATA_PKT, m2m_strlen(), NULL, SOCK_ERR_INVALID, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_CMD_DNS_RESOLVE, and SOCKET_REQUEST.
NMI_API sint8 getsockopt | ( | SOCKET | sock, |
uint8 | u8Level, | ||
uint8 | u8OptName, | ||
const void * | pvOptValue, | ||
uint8 * | pu8OptLen | ||
) |
Get socket options retrieves. This Function isn't implemented yet but this is the form that will be released later.
[in] | sock | Socket Identifier. |
[in] | u8Level | The protocol level of the option. |
[in] | u8OptName | The u8OptName argument specifies a single option to get. |
[out] | pvOptValue | The pvOptValue argument contains pointer to a buffer containing the option value. |
[out] | pu8OptLen | Option value buffer length. |
References SOCK_ERR_INVALID_ARG.
References gbSocketInit.
After successfully binding a socket to an IP address and port on the system, start listening passively for incoming connections. The socket must be bound on a local port or the listen operation fails. Upon the call to the asynchronous listen function, response is received through the event @ref SOCKET_MSG_LISTEN in the socket callback. A successful listen means the TCP server operation is active. If a connection is accepted, then the application socket callback function is notified with the new connected socket through the event @ref SOCKET_MSG_ACCEPT. Hence there is no need to call the @ref accept function after calling @ref listen. After a connection is accepted, the user is then required to call @ref recv to receive any packets transmitted by the remote host or to receive notification of socket connection termination.
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | backlog | Not used by the current implementation. |
This example demonstrates the call of the listen socket operation after a successful socket operation.
References MAX_SOCKET, NULL, tstrListenCmd::sock, SOCK_ERR_INVALID, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_CMD_LISTEN, SOCKET_REQUEST, tstrSocket::u16SessionID, tstrListenCmd::u16SessionID, and tstrListenCmd::u8BackLog.
The function request to send ping request to the given IP Address.
[in] | u32DstIP | Target Destination IP Address for the ping request. It must be represented in Network byte order. The function nmi_inet_addr could be used to translate the dotted decimal notation IP to its Network bytes order integer representative. |
[in] | u8TTL | IP TTL value for the ping request. If set to ZERO, the default value SHALL be used. |
[in] | fpPingCb | Callback will be called to deliver the ping statistics. |
References gfpPingCb, gu32PingId, M2M_ERR_INVALID_ARG, NULL, SOCKET_CMD_PING, SOCKET_REQUEST, tstrPingCmd::u16PingCount, tstrPingCmd::u32CmdPrivate, tstrPingCmd::u32DestIPAddr, and tstrPingCmd::u8TTL.
Synchronous function which returns a BSD socket compliant Internet Protocol (IPv4) socket address. This IPv4 address in the input string parameter could either be specified as a hostname, or as a numeric string representation like n.n.n.n known as the IPv4 dotted-decimal format (i.e. "192.168.10.1"). This function is used whenever an ip address needs to be set in the proper format (i.e. for the @ref tstrM2MIPConfig structure).
[in] | pcIpAddr | A null terminated string containing the IP address in IPv4 dotted-decimal address. |
References m2m_memcpy().
An asynchronous receive function, used to retrieve data from a TCP stream. Before calling the recv function, a successful socket connection status must have been received through any of the two socket events [SOCKET_MSG_CONNECT] or [SOCKET_MSG_ACCEPT], from the socket callback. Hence, indicating that the socket is already connected to a remote host. The application receives the required data in response to this asynchronous call through the reception of the event @ref SOCKET_MSG_RECV in the socket callback. Receiving the SOCKET_MSG_RECV message in the callback with zero or negative buffer length indicates the following: - @ref SOCK_ERR_NO_ERROR : Socket connection closed. The application should now call @ref close(). - @ref SOCK_ERR_CONN_ABORTED : Socket connection aborted. The application should now call @ref close(). - @ref SOCK_ERR_TIMEOUT : Socket receive timed out. The socket connection remains open.
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | pvRecvBuf | Pointer to a buffer that will hold the received data. The buffer is used in the recv callback to deliver the received data to the caller. The buffer must be resident in memory (heap or global buffer). |
[in] | u16BufLen | The buffer size in bytes. |
[in] | u32Timeoutmsec | Timeout for the recv function in milli-seconds. If the value is set to ZERO, the timeout will be set to infinite (the recv function waits forever). If the timeout period is elapsed with no data received, the socket will get a timeout error. |
The example demonstrates a code snippet for the calling of the recv function in the socket callback upon notification of the accept or connect events, and the parsing of the received data when the SOCKET_MSG_RECV event is received.
References tstrSocket::bIsRecvPending, MAX_SOCKET, NM_BSP_B_L_32, NULL, tstrSocket::pu8UserBuffer, tstrRecvCmd::sock, SOCK_ERR_BUFFER_FULL, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_CMD_RECV, SOCKET_CMD_SSL_RECV, SOCKET_REQUEST, SSL_FLAGS_ACTIVE, SSL_FLAGS_DELAY, tstrRecvCmd::u16BufLen, tstrSocket::u16SessionID, tstrRecvCmd::u16SessionID, tstrSocket::u16UserBufferSize, tstrRecvCmd::u32Timeoutmsec, and tstrSocket::u8SSLFlags.
Referenced by raw_recv(), tcp_recv(), and udp_recv().
Receives data from a UDP Socket. The asynchronous recvfrom function is used to retrieve data from a UDP socket. The socket must already be bound to a local port before a call to the recvfrom function is made (i.e message @ref SOCKET_MSG_BIND is received with successful status in the socket callback). Upon calling the recvfrom function with a successful return code, the application is expected to receive a notification in the socket callback whenever a message is received through the @ref SOCKET_MSG_RECVFROM event. Receiving the SOCKET_MSG_RECVFROM message in the callback with zero, indicates that the socket is closed. Whereby a negative buffer length indicates one of the socket error codes such as socket timeout error @ref SOCK_ERR_TIMEOUT The recvfrom callback can also be used to show the IP address of the remote host that sent the frame by using the "strRemoteAddr" element in the @ref tstrSocketRecvMsg structure. (refer to the code example)
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | pvRecvBuf | Pointer to a buffer that will hold the received data. The buffer shall be used in the recv callback to deliver the received data to the caller. The buffer must be resident in memory (heap or global buffer). |
[in] | u16BufLen | The buffer size in bytes. |
[in] | u32TimeoutSeconds | Timeout for the recv function in milli-seconds. If the value is set to ZERO, the timeout will be set to infinite (the recv function waits forever). |
The example demonstrates a code snippet for the calling of the recvfrom function in the socket callback upon notification of a successful bind event, and the parsing of the received data when the SOCKET_MSG_RECVFROM event is received.
References tstrSocket::bIsRecvPending, MAX_SOCKET, NM_BSP_B_L_32, NULL, tstrSocket::pu8UserBuffer, tstrRecvCmd::sock, SOCK_ERR_BUFFER_FULL, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_CMD_RECVFROM, SOCKET_REQUEST, tstrRecvCmd::u16BufLen, tstrSocket::u16SessionID, tstrRecvCmd::u16SessionID, tstrSocket::u16UserBufferSize, and tstrRecvCmd::u32Timeoutmsec.
NMI_API void registerSocketCallback | ( | tpfAppSocketCb | pfAppSocketCb, |
tpfAppResolveCb | pfAppResolveCb | ||
) |
Register two callback functions one for asynchronous socket events and the other one for DNS callback registering function. The registered callback functions are used to retrieve information in response to the asynchronous socket functions called.
[in] | socket_cb | Assignment of callback function to the global callback tpfAppSocketCb gpfAppSocketCb. Delivers socket messages to the host application. In response to the asynchronous function calls, such as bind listen accept connect |
[in] | resolve_cb | Assignment of callback function to the global callback tpfAppResolveCb gpfAppResolveCb. Used for DNS resolving functionality. The DNS resolving technique is determined by the application registering the callback. NULL is assigned when DNS resolution is not required. |
This example demonstrates the use of the registerSocketCallback to register a socket callback function with DNS resolution CB set to null for a simple UDP server example.
References gpfAppResolveCb, and gpfAppSocketCb.
Converts an (insecure) TCP connection with a remote server into a secure TLS-over-TCP connection. It may be called after both of the following:\n - a TCP socket has been created by the @ref socket function, with u8Config parameter set to @ref SOCKET_CONFIG_SSL_DELAY.\n - a successful connection has been made on the socket via the @ref connect function. This is an asynchronous API; the application socket callback function is notified of the result of the attempt to make the connection secure through the event @ref SOCKET_MSG_SECURE, along with a structure @ref tstrSocketConnectMsg. If the attempt to make the connection secure fails, the application should call @ref close().
[in] | sock | Socket ID, corresponding to a connected TCP socket. |
References MAX_SOCKET, NULL, tstrConnectCmd::sock, SOCK_ERR_INVALID, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_CMD_SECURE, SOCKET_REQUEST, SSL_FLAGS_ACTIVE, SSL_FLAGS_DELAY, tstrSocket::u16SessionID, tstrConnectCmd::u16SessionID, tstrSocket::u8SSLFlags, and tstrConnectCmd::u8SslFlags.
Asynchronous sending function, used to send data on a TCP/UDP socket. Called by the application code when there is outgoing data available required to be sent on a specific socket handler. The only difference between this function and the similar @ref sendto function, is the type of socket the data is sent on and the parameters passed in. @ref send function is most commonly called for sockets in a connected state. After the data is sent, the socket callback function registered using registerSocketCallback(), is expected to receive an event of type @ref SOCKET_MSG_SEND holding information containing the number of data bytes sent.
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | pvSendBuffer | Pointer to a buffer holding data to be transmitted. |
[in] | u16SendLength | The buffer size in bytes. |
[in] | u16Flags | Not used in the current implementation. |
References M2M_REQ_DATA_PKT, MAX_SOCKET, NM_BSP_B_L_16, NULL, tstrSendCmd::sock, SOCK_ERR_BUFFER_FULL, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_BUFFER_MAX_LENGTH, SOCKET_CMD_SEND, SOCKET_CMD_SSL_SEND, SOCKET_REQUEST, SSL_FLAGS_ACTIVE, SSL_FLAGS_DELAY, TCP_SOCK_MAX, TCP_TX_PACKET_OFFSET, tstrSocket::u16DataOffset, tstrSendCmd::u16DataSize, tstrSocket::u16SessionID, tstrSendCmd::u16SessionID, and UDP_TX_PACKET_OFFSET.
NMI_API sint16 sendto | ( | SOCKET | sock, |
void * | pvSendBuffer, | ||
uint16 | u16SendLength, | ||
uint16 | flags, | ||
struct sockaddr * | pstrDestAddr, | ||
uint8 | u8AddrLen | ||
) |
Asynchronous sending function, used to send data on a UDP socket. Called by the application code when there is data required to be sent on a UDP socket.
The application code is expected to receive data from a successfully bound socket node. The only difference between this function and the similar send function, is the type of socket the data is received on. This function works only with UDP sockets. After the data is sent, the socket callback function registered using registerSocketCallback(), is expected to receive an event of type SOCKET_MSG_SENDTO.
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | pvSendBuffer | Pointer to a buffer holding data to be transmitted. A NULL value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | u16SendLength | The buffer size in bytes. It must not exceed SOCKET_BUFFER_MAX_LENGTH. |
[in] | flags | Not used in the current implementation |
[in] | pstrDestAddr | The destination address. |
[in] | u8AddrLen | Destination address length in bytes. Not used in the current implementation, only included for BSD compatibility. |
References IP_PACKET_OFFSET, M2M_HIF_HDR_OFFSET, M2M_HIF_MAX_PACKET_SIZE, m2m_memset(), M2M_REQ_DATA_PKT, MAX_SOCKET, NM_BSP_B_L_16, NULL, RAW_SOCK_ID, in_addr::s_addr, sockaddr_in::sin_addr, sockaddr_in::sin_family, sockaddr_in::sin_port, tstrSendCmd::sock, SOCK_ERR_BUFFER_FULL, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_BUFFER_MAX_LENGTH, SOCKET_CMD_SENDTO, SOCKET_REQUEST, tstrSendCmd::strAddr, tstrSendCmd::u16DataSize, tstrSockAddr::u16Family, tstrSockAddr::u16Port, tstrSocket::u16SessionID, tstrSendCmd::u16SessionID, tstrSockAddr::u32IPAddr, and UDP_TX_PACKET_OFFSET.
This function sets the protocol list used for application-layer protocol negotiation (ALPN). If used, it must be called after creating a SSL socket (using socket) and before connecting/binding (using connect or bind) or securing (using secure).
[in] | sock | Socket ID obtained by a call to socket. This is the SSL socket to which the ALPN list applies. |
[in] | pcProtocolList | Pointer to the list of protocols available in the application. The entries in the list must:
|
The example demonstrates an application using set_alpn_list and get_alpn_index to negotiate secure HTTP/2 (with fallback option of HTTP/1.1).
References ALPN_LIST_MAX_APP_LENGTH, ALPN_LIST_MAX_SIZE, m2m_memcpy(), m2m_strlen(), NULL, setsockopt(), SO_SSL_ALPN, SOCK_ERR_INVALID_ARG, SOL_SSL_SOCKET, and TCP_SOCK_MAX.
NMI_API sint8 setsockopt | ( | SOCKET | sock, |
uint8 | u8Level, | ||
uint8 | option_name, | ||
const void * | option_value, | ||
uint16 | u16OptionLen | ||
) |
The setsockopt() function shall set the option specified by the option_name argument, at the protocol level specified by the level argument, to the value pointed to by the option_value argument for the socket specified by the socket argument.
[in] | socket | Socket handler. |
[in] | u8Level | Protocol level. Supported protocol levels are SOL_SOCKET, SOL_SSL_SOCKET and SOL_RAW. |
[in] | option_name | Option to be set. For protocol level SOL_SOCKET, the supported option names are: SO_SET_UDP_SEND_CALLBACK SO_TCP_KEEPALIVE SO_TCP_KEEPIDLE SO_TCP_KEEPINTVL SO_TCP_KEEPCNT For protocol level SOL_SSL_SOCKET, the supported option names are: SO_SSL_BYPASS_X509_VERIF SO_SSL_SNI SO_SSL_ENABLE_SESSION_CACHING SO_SSL_ENABLE_CERTNAME_VALIDATION SO_SSL_ALPN For protocol level SOL_RAW, the supported option names are: SO_ICMP_FILTER |
[in] | option_value | Pointer to user provided value. |
[in] | u16OptionLen | Length of the option value in bytes. Refer to each option documentation for the required length. |
References MAX_SOCKET, NULL, rawSetSockOpt(), tstrSetSocketOptCmd::sock, SOCK_ERR_INVALID, SOCK_ERR_INVALID_ARG, SOCK_ERR_NO_ERROR, SOCKET_CMD_SET_SOCKET_OPTION, SOCKET_REQUEST, SOL_RAW, SOL_SOCKET, SOL_SSL_SOCKET, sslSetSockOpt(), tstrSocket::u16SessionID, tstrSetSocketOptCmd::u16SessionID, tstrSetSocketOptCmd::u32OptionValue, and tstrSetSocketOptCmd::u8Option.
Referenced by set_alpn_list().
Synchronous socket allocation function based on the specified socket type. Created sockets are non-blocking and their possible types are either TCP or a UDP sockets. The maximum allowed number of TCP sockets is @ref TCP_SOCK_MAX sockets while the maximum number of UDP sockets that can be created simultaneously is @ref UDP_SOCK_MAX sockets.
[in] | u16Domain | Socket family. The only allowed value is AF_INET (IPv4.0) for TCP/UDP sockets. |
[in] | u8Type | Socket type. Allowed values are: |
[in] | u8Config | Used to specify the socket configuration. The interpretation of this parameter depends on the setting of u8Type.
|
This example demonstrates the use of the socket function to allocate the socket, returning the socket handler to be used for other socket operations. Socket creation is dependent on the socket type.
References AF_INET, tstrSocket::bIsUsed, gu16SessionID, M2M_INFO, m2m_memset(), RAW_SOCK_ID, SOCK_DGRAM, SOCK_RAW, SOCK_STREAM, SOCKET_CMD_SSL_CREATE, SOCKET_CONFIG_IPPROTO_RAW, SOCKET_CONFIG_SSL_DELAY, SOCKET_CONFIG_SSL_OFF, SOCKET_REQUEST, SSL_FLAGS_ACTIVE, SSL_FLAGS_DELAY, tstrSSLSocketCreateCmd::sslSock, TCP_SOCK_MAX, tstrSocket::u16SessionID, tstrSocket::u8SSLFlags, and UDP_SOCK_MAX.
Socket Layer De-initialization.
The function performs the necessary cleanup for the socket library static data It must be invoked only after all desired socket operations have been performed on any active sockets.
References gbSocketInit, gpfAppResolveCb, gpfAppSocketCb, hif_register_cb(), m2m_memset(), M2M_REQ_GROUP_IP, MAX_SOCKET, and NULL.
The function performs the necessary initialization for the socket library through the following steps: - A check made by the global variable gbSocketInit, ensuring that initialization for sockets is performed only once, in-order to prevent resetting the socket instances already created in the global socket array (gastrSockets). - Zero initializations to the global socket array (gastrSockets), which holds the list of TCP sockets. - Registers the socket (Host Interface)hif callback function through the call to the hif_register_cb function. This facilitates handling all of the socket related functions received through interrupts from the firmware.
This example demonstrates the use of the socketInit for socket initialization for an mqtt chat application.
References gbSocketInit, gu16SessionID, hif_register_cb(), m2m_ip_cb(), m2m_memset(), M2M_REQ_GROUP_IP, and MAX_SOCKET.