This module contains M2M host interface APIs implementation.
Copyright (c) 2017-2019 Microchip Technology Inc. and its subsidiaries.
#include "common/include/nm_common.h"
Data Structures | |
struct | tstrHifHdr |
Structure to hold HIF header. More... | |
Macros | |
#define | M2M_HIF_HDR_OFFSET (sizeof(tstrHifHdr) + 4) |
#define | M2M_HIF_MAX_PACKET_SIZE (1600 - 4) |
Typedefs | |
typedef void(* | tpfHifCallBack )(uint8 u8OpCode, uint16 u16DataSize, uint32 u32Addr) |
used to point to Wi-Fi call back function depend on Arduino project or other projects. More... | |
Functions | |
sint8 | hif_check_code (uint8 u8Gid, uint8 u8OpCode) |
To check that a particular hif message is supported with the current driver/firmware pair.More... | |
sint8 | hif_check_compatibility (uint16 u16HifInfo) |
To check the compatibility of an image with the current driver.More... | |
NMI_API sint8 | hif_chip_sleep (void) |
To make the chip sleep. More... | |
NMI_API sint8 | hif_chip_wake (void) |
To Wakeup the chip. More... | |
NMI_API sint8 | hif_deinit (void *arg) |
To Deinitialize HIF layer. More... | |
sint8 | hif_enable_access (void) |
To enable access to HIF layer, based on HIF level of Firmware.More... | |
NMI_API uint8 | hif_get_sleep_mode (void) |
Get the sleep mode of the HIF layer. More... | |
NMI_API sint8 | hif_handle_isr (void) |
Handle interrupt received from NMC1500 firmware.More... | |
NMI_API sint8 | hif_init (void *arg) |
To initialize HIF layer. More... | |
NMI_API sint8 | hif_receive (uint32 u32Addr, uint8 *pu8Buf, uint16 u16Sz, uint8 isDone) |
NMI_API sint8 | hif_register_cb (uint8 u8Grp, tpfHifCallBack fn) |
NMI_API sint8 | hif_send (uint8 u8Gid, uint8 u8Opcode, uint8 *pu8CtrlBuf, uint16 u16CtrlBufSize, uint8 *pu8DataBuf, uint16 u16DataSize, uint16 u16DataOffset) |
Send packet using host interface. More... | |
NMI_API void | hif_set_sleep_mode (uint8 u8Pstype) |
Set the sleep mode of the HIF layer. More... | |
NMI_API void | hif_yield (void) |
Yields control from interrupt event handler. More... | |
#define M2M_HIF_HDR_OFFSET (sizeof(tstrHifHdr) + 4) |
Referenced by hif_isr(), hif_send(), m2m_ip_cb(), m2m_wifi_send_ethernet_pkt(), and sendto().
#define M2M_HIF_MAX_PACKET_SIZE (1600 - 4) |
< Include depends on UNO Board is used or not Maximum size of the buffer could be transferred between Host and Firmware.
Referenced by hif_send(), and sendto().
used to point to Wi-Fi call back function depend on Arduino project or other projects.
[in] | u8OpCode | HIF Opcode type. |
[in] | u16DataSize | HIF data length. |
[in] | u32Addr | HIF address. |
[in] | grp | HIF group type. |
To check that a particular hif message is supported with the current driver/firmware pair.
[in] | u8Gid | Group ID. |
[in] | u8Opcode | Operation ID. |
[in] | u8Gid | Group ID. |
[in] | u8Opcode | Operation ID. |
References gau16HifBlacklist, gu8HifBlOffset, HIF_BLACKLIST_SZ, HIFCODE_OTA_RB, HIFCODE_OTA_SW, M2M_ERR, M2M_ERR_SEND, and M2M_SUCCESS.
Referenced by hif_send().
To check the compatibility of an image with the current driver.
[in] | u16HifInfo | HIF info of image to be checked. |
References M2M_ERR_FW_VER_MISMATCH, M2M_GET_HIF_BLOCK, M2M_GET_HIF_MAJOR, M2M_HIF_BLOCK_VALUE, M2M_HIF_MAJOR_VALUE, and M2M_SUCCESS.
Referenced by hif_enable_access(), and m2m_wifi_check_ota_rb().
To make the chip sleep.
To make the chip sleep.
References chip_sleep(), M2M_NO_PS, M2M_SUCCESS, tstrHifContext::u8ChipMode, and tstrHifContext::u8ChipSleep.
Referenced by gpio_ioctl(), hif_init(), hif_send(), m2m_ota_get_firmware_version(), m2m_wifi_get_firmware_version(), m2m_wifi_get_mac_address(), and m2m_wifi_get_otp_mac_address().
To Wakeup the chip.
To Wakeup the chip.
References chip_wake(), M2M_NO_PS, M2M_SUCCESS, tstrHifContext::u8ChipMode, tstrHifContext::u8ChipSleep, and tstrHifContext::u8HifRXDone.
Referenced by gpio_ioctl(), hif_deinit(), hif_send(), m2m_ota_get_firmware_version(), m2m_wifi_get_firmware_version(), m2m_wifi_get_mac_address(), and m2m_wifi_get_otp_mac_address().
To Deinitialize HIF layer.
To Deinitialize HIF layer.
[in] | arg | Pointer to the arguments. |
[in] | arg | Pointer to the arguments. |
References hif_chip_wake(), m2m_memset(), and M2M_SUCCESS.
Referenced by m2m_wifi_deinit().
To enable access to HIF layer, based on HIF level of Firmware.
This function reads HIF level directly from a register written by Firmware.
References gu8HifBlOffset, HIF_BLACKLIST_SZ, hif_check_compatibility(), M2M_ERR, M2M_GET_HIF_MINOR, M2M_SUCCESS, nm_get_hif_info(), and NULL.
Referenced by m2m_wifi_init_start().
Get the sleep mode of the HIF layer.
References tstrHifContext::u8ChipMode.
Referenced by m2m_wifi_get_sleep_mode(), and m2m_wifi_request_sleep().
Handle interrupt received from NMC1500 firmware.
References hif_isr(), M2M_ERR, M2M_SUCCESS, nm_bsp_interrupt_ctrl(), tstrHifContext::u8Interrupt, and tstrHifContext::u8Yield.
Referenced by m2m_wifi_handle_events().
To initialize HIF layer.
To initialize HIF layer.
[in] | arg | Pointer to the arguments. |
[in] | arg | Pointer to the arguments. |
References hif_chip_sleep(), hif_register_cb(), isr(), m2m_hif_cb(), m2m_memset(), M2M_REQ_GROUP_HIF, M2M_SUCCESS, and nm_bsp_register_isr().
Referenced by m2m_wifi_init_start().
References hif_set_rx_done(), M2M_ERR, M2M_ERR_FAIL, M2M_SUCCESS, nm_read_block(), NULL, tstrHifContext::u32RxAddr, and tstrHifContext::u32RxSize.
Referenced by m2m_ip_cb(), m2m_ota_cb(), m2m_ssl_cb(), m2m_ssl_retrieve_hash(), m2m_ssl_retrieve_next_for_verifying(), m2m_ssl_stop_retrieving(), m2m_wifi_cb(), and Socket_ReadSocketData().
NMI_API sint8 hif_register_cb | ( | uint8 | u8Grp, |
tpfHifCallBack | fn | ||
) |
References M2M_ERR, M2M_ERR_FAIL, M2M_REQ_GROUP_HIF, M2M_REQ_GROUP_IP, M2M_REQ_GROUP_OTA, M2M_REQ_GROUP_SIGMA, M2M_REQ_GROUP_SSL, M2M_REQ_GROUP_WIFI, M2M_SUCCESS, tstrHifContext::pfHifCb, tstrHifContext::pfIpCb, tstrHifContext::pfOtaCb, tstrHifContext::pfSigmaCb, tstrHifContext::pfSslCb, and tstrHifContext::pfWifiCb.
Referenced by hif_init(), m2m_ota_init(), m2m_ssl_init(), m2m_wifi_init_start(), socketDeinit(), and socketInit().
NMI_API sint8 hif_send | ( | uint8 | u8Gid, |
uint8 | u8Opcode, | ||
uint8 * | pu8CtrlBuf, | ||
uint16 | u16CtrlBufSize, | ||
uint8 * | pu8DataBuf, | ||
uint16 | u16DataSize, | ||
uint16 | u16DataOffset | ||
) |
Send packet using host interface.
[in] | u8Gid | Group ID. |
[in] | u8Opcode | Operation ID. |
[in] | pu8CtrlBuf | Pointer to the Control buffer. |
[in] | u16CtrlBufSize | Control buffer size. |
[in] | u16DataOffset | Packet Data offset. |
[in] | pu8DataBuf | Packet buffer Allocated by the caller. |
[in] | u16DataSize | Packet buffer size (including the HIF header). |
[in] | u8Gid | Group ID. |
[in] | u8Opcode | Operation ID. |
[in] | pu8CtrlBuf | Pointer to the Control buffer. |
[in] | u16CtrlBufSize | Control buffer size. |
[in] | u16DataOffset | Packet Data offset. |
[in] | pu8DataBuf | Packet buffer Allocated by the caller. |
[in] | u16DataSize | Packet buffer size (including the HIF header). |
References hif_check_code(), hif_chip_sleep(), hif_chip_sleep_sc(), hif_chip_wake(), INTERRUPT_CORTUS_1_3000D0, INTERRUPT_CORTUS_2_3000D0, ISNMC3400, M2M_DBG, M2M_ERR, M2M_ERR_MEM_ALLOC, M2M_ERR_SEND, M2M_HIF_HDR_OFFSET, M2M_HIF_MAX_PACKET_SIZE, M2M_INFO, M2M_SUCCESS, NBIT1, NBIT7, NM_BSP_B_L_16, nm_bsp_sleep(), nm_read_reg_with_ret(), nm_write_block(), nm_write_reg(), nmi_get_chipid(), NMI_STATE_REG, NULL, tstrHifHdr::u16Length, tstrHifHdr::u8Gid, tstrHifHdr::u8Opcode, WIFI_HOST_RCV_CTRL_2, WIFI_HOST_RCV_CTRL_3, and WIFI_HOST_RCV_CTRL_4.
Referenced by m2m_ota_abort(), m2m_ota_notif_check_for_update(), m2m_ota_notif_sched(), m2m_ota_notif_set_url(), m2m_ota_rollback(), m2m_ota_start_update(), m2m_ota_switch_firmware(), m2m_ssl_handshake_rsp(), m2m_ssl_send_certs_to_winc(), m2m_ssl_set_active_ciphersuites(), m2m_wifi_ble_api_send(), m2m_wifi_ble_set_gain_table(), m2m_wifi_configure_sntp(), m2m_wifi_connect_1x_mschap2(), m2m_wifi_connect_1x_tls(), m2m_wifi_connect_open(), m2m_wifi_connect_psk(), m2m_wifi_connect_wep(), m2m_wifi_default_connect(), m2m_wifi_delete_sc(), m2m_wifi_disable_ap(), m2m_wifi_disable_roaming(), m2m_wifi_disconnect(), m2m_wifi_enable_ap_ext(), m2m_wifi_enable_dhcp(), m2m_wifi_enable_firmware_logs(), m2m_wifi_enable_mac_mcast(), m2m_wifi_enable_roaming(), m2m_wifi_enable_sntp(), m2m_wifi_get_connection_info(), m2m_wifi_get_system_time(), m2m_wifi_p2p(), m2m_wifi_p2p_disconnect(), m2m_wifi_prng_get_random_bytes(), m2m_wifi_req_curr_rssi(), m2m_wifi_req_restrict_ble(), m2m_wifi_req_scan_result(), m2m_wifi_req_unrestrict_ble(), m2m_wifi_request_scan(), m2m_wifi_request_scan_passive(), m2m_wifi_request_scan_ssid_list(), m2m_wifi_request_sleep(), m2m_wifi_send_ethernet_pkt(), m2m_wifi_set_battery_voltage(), m2m_wifi_set_cust_InfoElement(), m2m_wifi_set_device_name(), m2m_wifi_set_lsn_int(), m2m_wifi_set_mac_address(), m2m_wifi_set_power_profile(), m2m_wifi_set_scan_options(), m2m_wifi_set_scan_region(), m2m_wifi_set_sleep_mode(), m2m_wifi_set_static_ip(), m2m_wifi_set_stop_scan_on_first(), m2m_wifi_set_system_time(), m2m_wifi_set_tx_power(), m2m_wifi_start_provision_mode_ext(), m2m_wifi_stop_provision_mode(), m2m_wifi_wps(), and m2m_wifi_wps_disable().
Set the sleep mode of the HIF layer.
[in] | u8Pstype | Sleep mode. |
References tstrHifContext::u8ChipMode.
Referenced by m2m_wifi_set_sleep_mode().
Yields control from interrupt event handler.
Yields control from interrupt event handler.
References tstrHifContext::u8Yield.
Referenced by m2m_wifi_yield().