#include "lwip/opt.h"
#include "lwip/pbuf.h"
#include "lwip/def.h"
#include "lwip/ip.h"
#include "lwip/ip_addr.h"
#include "lwip/ip6_addr.h"
Data Structures | |
struct | raw_pcb |
Macros | |
#define | raw_bind_ip6(pcb, ip6addr) raw_bind(pcb, ip6_2_ip(ip6addr)) |
#define | raw_connect_ip6(pcb, ip6addr) raw_connect(pcb, ip6_2_ip(ip6addr)) |
#define | raw_init() /* Compatibility define, no init needed. */ |
#define | RAW_PCB_RECV_IP6 raw_recv_ip6_fn ip6; |
#define | raw_recv_ip6(pcb, recv_ip6_fn, recv_arg) raw_recv(pcb, (raw_recv_fn)recv_ip6_fn, recv_arg) |
#define | raw_sendto_ip6(pcb, pbuf, ip6addr) raw_sendto(pcb, pbuf, ip6_2_ip(ip6addr)) |
Typedefs | |
typedef u8_t(* | raw_recv_fn )(void *arg, struct raw_pcb *pcb, struct pbuf *p, ip_addr_t *addr) |
Function prototype for raw pcb receive callback functions. More... | |
typedef u8_t(* | raw_recv_ip6_fn )(void *arg, struct raw_pcb *pcb, struct pbuf *p, ip6_addr_t *addr) |
Function prototype for raw pcb IPv6 receive callback functions. More... | |
Functions | |
err_t | raw_bind (struct raw_pcb *pcb, ip_addr_t *ipaddr) |
Bind a RAW PCB. More... | |
err_t | raw_connect (struct raw_pcb *pcb, ip_addr_t *ipaddr) |
Connect an RAW PCB. More... | |
u8_t | raw_input (struct pbuf *p, struct netif *inp) |
Determine if in incoming IP packet is covered by a RAW PCB and if so, pass it to a user-provided receive callback function. More... | |
struct raw_pcb * | raw_new (u8_t proto) |
Create a RAW PCB. More... | |
struct raw_pcb * | raw_new_ip6 (u8_t proto) |
Create a RAW PCB for IPv6. More... | |
void | raw_recv (struct raw_pcb *pcb, raw_recv_fn recv, void *recv_arg) |
Set the callback function for received packets that match the raw PCB's protocol and binding. More... | |
void | raw_remove (struct raw_pcb *pcb) |
Remove an RAW PCB. More... | |
err_t | raw_send (struct raw_pcb *pcb, struct pbuf *p) |
Send the raw IP packet to the address given by raw_connect() More... | |
err_t | raw_sendto (struct raw_pcb *pcb, struct pbuf *p, ip_addr_t *ipaddr) |
Send the raw IP packet to the given address. More... | |
#define raw_connect_ip6 | ( | pcb, | |
ip6addr | |||
) | raw_connect(pcb, ip6_2_ip(ip6addr)) |
#define raw_init | ( | ) | /* Compatibility define, no init needed. */ |
Referenced by lwip_init().
#define RAW_PCB_RECV_IP6 raw_recv_ip6_fn ip6; |
#define raw_recv_ip6 | ( | pcb, | |
recv_ip6_fn, | |||
recv_arg | |||
) | raw_recv(pcb, (raw_recv_fn)recv_ip6_fn, recv_arg) |
#define raw_sendto_ip6 | ( | pcb, | |
pbuf, | |||
ip6addr | |||
) | raw_sendto(pcb, pbuf, ip6_2_ip(ip6addr)) |
Function prototype for raw pcb receive callback functions.
arg | user supplied argument (raw_pcb.recv_arg) |
pcb | the raw_pcb which received data |
p | the packet buffer that was received |
addr | the remote IP address from which the packet was received |
Function prototype for raw pcb IPv6 receive callback functions.
arg | user supplied argument (raw_pcb.recv_arg) |
pcb | the raw_pcb which received data |
p | the packet buffer that was received |
addr | the remote IPv6 address from which the packet was received |
Bind a RAW PCB.
pcb | RAW PCB to be bound with a local address ipaddr. |
ipaddr | local IP address to bind with. Use IP_ADDR_ANY to bind to all local interfaces. |
References ERR_OK, ipX_addr_set_ipaddr, and PCB_ISIPV6.
Referenced by lwip_netconn_do_bind(), and ping_raw_init().
Connect an RAW PCB.
This function is required by upper layers of lwip. Using the raw api you could use raw_sendto() instead
This will associate the RAW PCB with the remote address.
pcb | RAW PCB to be connected with remote address ipaddr and port. |
ipaddr | remote IP address to connect with. |
References ERR_OK, ipX_addr_set_ipaddr, and PCB_ISIPV6.
Referenced by lwip_netconn_do_connect().
Determine if in incoming IP packet is covered by a RAW PCB and if so, pass it to a user-provided receive callback function.
Given an incoming IP datagram (as a chain of pbufs) this function finds a corresponding RAW PCB and calls the corresponding receive callback function.
p | pbuf to be demultiplexed to a RAW PCB. |
inp | network interface on which the datagram was received. |
References if(), raw_pcb::ip4, ip6_current_src_addr, IP6H_NEXTH, ip_addr_isbroadcast, ip_current_dest_addr, ip_current_src_addr, ip_get_option, IP_PCB_IPVER_INPUT_MATCH, IPH_PROTO, IPH_V, ipX_addr_cmp, ipX_addr_isany, ipX_current_dest_addr, LWIP_ASSERT, LWIP_IPV6, raw_pcb::next, NULL, pbuf::payload, PCB_ISIPV6, raw_pcb::protocol, raw_pcbs, raw_pcb::recv, raw_pcb::recv_arg, and SOF_BROADCAST.
Referenced by ip6_input(), and ip_input().
Create a RAW PCB.
proto | the protocol number of the IPs payload (e.g. IP_PROTO_ICMP) |
References LWIP_DBG_TRACE, LWIP_DEBUGF, memp_malloc(), raw_pcb::next, NULL, raw_pcb::protocol, RAW_DEBUG, and raw_pcbs.
Referenced by pcb_new(), ping_raw_init(), and raw_new_ip6().
Create a RAW PCB for IPv6.
proto | the protocol number (next header) of the IPv6 packet payload (e.g. IP6_NEXTH_ICMP6) |
void raw_recv | ( | struct raw_pcb * | pcb, |
raw_recv_fn | recv, | ||
void * | recv_arg | ||
) |
Set the callback function for received packets that match the raw PCB's protocol and binding.
The callback function MUST either
References raw_pcb::ip4, raw_pcb::recv, recv(), and raw_pcb::recv_arg.
Referenced by pcb_new(), and ping_raw_init().
Remove an RAW PCB.
pcb | RAW PCB to be removed. The PCB is removed from the list of RAW PCB's and the data structure is freed from memory. |
References memp_free(), raw_pcb::next, and NULL.
Referenced by lwip_netconn_do_delconn().
Send the raw IP packet to the address given by raw_connect()
pcb | the raw pcb which to send |
p | the IP payload to send |
References ipX_2_ip, and raw_sendto().
Referenced by lwip_netconn_do_send().
Send the raw IP packet to the given address.
Note that actually you cannot modify the IP headers (this is inconsistent with the receive callback where you actually get the IP headers), you can only specify the IP payload here. It requires some more changes in lwIP. (there will be a raw_send() function then.)
pcb | the raw pcb which to send |
p | the IP payload to send |
ipaddr | the destination address of the IP packet |
References raw_pcb::chksum_offset, raw_pcb::chksum_reqd, ERR_MEM, ERR_RTE, ERR_VAL, ip6_chksum_pseudo(), IP6_HLEN, ip_2_ipX, ip_addr_isbroadcast, ip_get_option, IP_HLEN, ipX_2_ip, ipX_2_ip6, ipX_addr_debug_print, ipX_addr_isany, ipX_netif_get_local_ipX, ipX_output_if, ipX_route, pbuf::len, LWIP_ASSERT, LWIP_DBG_LEVEL_SERIOUS, LWIP_DBG_LEVEL_WARNING, LWIP_DBG_TRACE, LWIP_DEBUGF, NETIF_SET_HWADDRHINT, NULL, pbuf::payload, pbuf_alloc(), pbuf_chain(), pbuf_free(), pbuf_header(), PBUF_IP, PBUF_RAM, PCB_ISIPV6, raw_pcb::protocol, RAW_DEBUG, SOF_BROADCAST, and pbuf::tot_len.
Referenced by lwip_netconn_do_send(), ping_send(), and raw_send().