This is the unit test for the IOPORT service. The IO Pin is tested by setting high and low and read back using another IO Pin by shorting the pins.
This example has been tested with the following setup(s):
See the documentation for the individual unit test functions here for detailed descriptions of the tests.
This example depends directly on the following modules:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.