Ethernet Interface Skeleton.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
err_t | ethernetif_init (struct netif *netif) |
Should be called at the beginning of the program to set up the network interface. More... | |
void | ethernetif_input (void *pv_parameters) |
This function should be called when a packet is ready to be read from the interface. More... | |
Should be called at the beginning of the program to set up the network interface.
It calls the function low_level_init() to do the actual setup of the hardware.
This function should be passed as a parameter to netif_add().
netif | the lwip network interface structure for this ethernetif. |
References ERR_OK, etharp_output(), IFNAME0, IFNAME1, netif::linkoutput, low_level_init(), low_level_output(), LWIP_ASSERT, netif::name, NET_LINK_SPEED, NETIF_INIT_SNMP, NULL, netif::output, snmp_ifType_ethernet_csmacd, and netif::state.
Referenced by ethernet_configure_interface().
This function should be called when a packet is ready to be read from the interface.
It uses the function low_level_input() that should handle the actual reception of bytes from the network interface. Then the type of the received packet is determined and the appropriate input function is called.
pv_parameters | the lwip network interface structure for this ethernetif. |
References ERR_OK, netif::input, low_level_input(), NULL, pbuf_free(), and vTaskDelay().
Referenced by low_level_init().