message_buffer.h
StreamBufferHandle_t xStreamBufferCreate( size_t xBufferSizeBytes, size_t xTriggerLevelBytes );
Creates a new stream buffer using dynamically allocated memory. See xStreamBufferCreateStatic() for a version that uses statically allocated memory (memory that is allocated at compile time).
configSUPPORT_DYNAMIC_ALLOCATION must be set to 1 or left undefined in FreeRTOSConfig.h for xStreamBufferCreate() to be available.
xBufferSizeBytes | The total number of bytes the stream buffer will be able to hold at any one time. |
xTriggerLevelBytes | The number of bytes that must be in the stream buffer before a task that is blocked on the stream buffer to wait for data is moved out of the blocked state. For example, if a task is blocked on a read of an empty stream buffer that has a trigger level of 1 then the task will be unblocked when a single byte is written to the buffer or the task's block time expires. As another example, if a task is blocked on a read of an empty stream buffer that has a trigger level of 10 then the task will not be unblocked until the stream buffer contains at least 10 bytes or the task's block time expires. If a reading task's block time expires before the trigger level is reached then the task will still receive however many bytes are actually available. Setting a trigger level of 0 will result in a trigger level of 1 being used. It is not valid to specify a trigger level that is greater than the buffer size. |
Example use:
void vAFunction( void ) { StreamBufferHandle_t xStreamBuffer; const size_t xStreamBufferSizeBytes = 100, xTriggerLevel = 10;// Create a stream buffer that can hold 100 bytes. The memory used to hold // both the stream buffer structure and the data in the stream buffer is // allocated dynamically. xStreamBuffer = xStreamBufferCreate( xStreamBufferSizeBytes, xTriggerLevel ); if( xStreamBuffer == NULL ) { // There was not enough heap memory space available to create the // stream buffer. } else { // The stream buffer was created successfully and can now be used. }}