stream_buffer.h
BaseType_t xStreamBufferReset( StreamBufferHandle_t xStreamBuffer );
Resets a stream buffer to its initial, empty, state. Any data that was in the stream buffer is discarded. A stream buffer can only be reset if there are no tasks blocked waiting to either send to or receive from the stream buffer.
xStreamBuffer | The handle of the stream buffer being reset. |