lwIP Options Configuration
Macros | |
#define | AUTOIP_DEBUG LWIP_DBG_OFF |
AUTOIP_DEBUG: Enable debugging in autoip.c. More... | |
#define | CHECKSUM_CHECK_IP 1 |
CHECKSUM_CHECK_IP==1: Check checksums in software for incoming IP packets. More... | |
#define | CHECKSUM_CHECK_TCP 1 |
CHECKSUM_CHECK_TCP==1: Check checksums in software for incoming TCP packets. More... | |
#define | CHECKSUM_CHECK_UDP 1 |
CHECKSUM_CHECK_UDP==1: Check checksums in software for incoming UDP packets. More... | |
#define | CHECKSUM_GEN_IP 1 |
CHECKSUM_GEN_IP==1: Generate checksums in software for outgoing IP packets. More... | |
#define | CHECKSUM_GEN_TCP 1 |
CHECKSUM_GEN_TCP==1: Generate checksums in software for outgoing TCP packets. More... | |
#define | CHECKSUM_GEN_UDP 1 |
CHECKSUM_GEN_UDP==1: Generate checksums in software for outgoing UDP packets. More... | |
#define | DHCP_DEBUG LWIP_DBG_OFF |
DHCP_DEBUG: Enable debugging in dhcp.c. More... | |
#define | DHCP_DOES_ARP_CHECK ((LWIP_DHCP) && (LWIP_ARP)) |
LWIP_DHCP==1: Enable DHCP module. More... | |
#define | DNS_DEBUG LWIP_DBG_OFF |
DNS_DEBUG: Enable debugging for DNS. More... | |
#define | DNS_DOES_NAME_CHECK 1 |
DNS do a name checking between the query and the response. More... | |
#define | DNS_LOCAL_HOSTLIST 0 |
DNS_LOCAL_HOSTLIST: Implements a local host-to-address list. More... | |
#define | DNS_LOCAL_HOSTLIST_IS_DYNAMIC 0 |
If this is turned on, the local host-list can be dynamically changed at runtime. More... | |
#define | DNS_MAX_NAME_LENGTH 256 |
DNS maximum host name length supported in the name table. More... | |
#define | DNS_MAX_SERVERS 2 |
The maximum of DNS servers. More... | |
#define | DNS_MSG_SIZE 512 |
DNS message max. More... | |
#define | DNS_TABLE_SIZE 4 |
DNS maximum number of entries to maintain locally. More... | |
#define | ETHARP_STATS (LWIP_ARP) |
LWIP_STATS==1: Enable statistics collection in lwip_stats. More... | |
#define | ETHARP_SUPPORT_STATIC_ENTRIES 0 |
ETH_PAD_SIZE: number of bytes added before the ethernet header to ensure alignment of payload after that header. More... | |
#define | ETHARP_SUPPORT_VLAN 0 |
ETHARP_SUPPORT_VLAN==1: support receiving ethernet packets with VLAN header. More... | |
#define | ETHARP_TRUST_IP_MAC 0 |
ARP_TABLE_SIZE: Number of active MAC-IP address pairs cached. More... | |
#define | IGMP_DEBUG LWIP_DBG_OFF |
ETHARP_DEBUG: Enable debugging in etharp.c. More... | |
#define | IGMP_STATS (LWIP_IGMP) |
ICMP_STATS==1: Enable ICMP stats. More... | |
#define | IP_DEFAULT_TTL 255 |
IP_FRAG_MAX_MTU: Assumed max MTU on any interface for IP frag buffer (requires IP_FRAG_USES_STATIC_BUF==1) More... | |
#define | IP_FRAG 1 |
IP_FRAG==1: Fragment outgoing IP packets if their size exceeds MTU. More... | |
#define | IP_FRAG_USES_STATIC_BUF 0 |
IP_FRAG_USES_STATIC_BUF==1: Use a static MTU-sized buffer for IP fragmentation. More... | |
#define | IP_OPTIONS_ALLOWED 1 |
IP_FORWARD==1: Enables the ability to forward IP packets across network interfaces. More... | |
#define | IP_REASS_MAX_PBUFS 10 |
IP_REASS_MAX_PBUFS: Total maximum amount of pbufs waiting to be reassembled. More... | |
#define | IP_REASS_MAXAGE 3 |
IP_REASS_MAXAGE: Maximum time (in multiples of IP_TMR_INTERVAL - so seconds, normally) a fragmented IP packet waits for all fragments to arrive. More... | |
#define | IP_REASSEMBLY 1 |
IP_REASSEMBLY==1: Reassemble incoming fragmented IP packets. More... | |
#define | IP_SOF_BROADCAST 0 |
IP_SOF_BROADCAST=1: Use the SOF_BROADCAST field to enable broadcast filter per pcb on udp and raw send operations. More... | |
#define | IP_SOF_BROADCAST_RECV 0 |
IP_SOF_BROADCAST_RECV (requires IP_SOF_BROADCAST=1) enable the broadcast filter on recv operations. More... | |
#define | IPFRAG_STATS (IP_REASSEMBLY || IP_FRAG) |
IP_STATS==1: Enable IP stats. More... | |
#define | LWIP_ALLOW_MEM_FREE_FROM_OTHER_CONTEXT 0 |
Set this to 1 if you want to free PBUF_RAM pbufs (or call mem_free()) from interrupt context (or another context that doesn't allow waiting for a semaphore). More... | |
#define | LWIP_ARP 1 |
PBUF_POOL_SIZE: the number of buffers in the pbuf pool. More... | |
#define | LWIP_AUTOIP 0 |
LWIP_AUTOIP==1: Enable AUTOIP module. More... | |
#define | LWIP_BROADCAST_PING 0 |
ICMP_TTL: Default value for Time-To-Live used by ICMP packets. More... | |
#define | LWIP_CALLBACK_API 1 |
#define | LWIP_CHECKSUM_ON_COPY 0 |
LWIP_CHECKSUM_ON_COPY==1: Calculate checksum when copying data from application buffers to pbufs. More... | |
#define | LWIP_COMPAT_SOCKETS 1 |
LWIP_COMPAT_SOCKETS==1: Enable BSD-style sockets functions names. More... | |
#define | LWIP_DBG_MIN_LEVEL LWIP_DBG_LEVEL_ALL |
LWIP_DBG_MIN_LEVEL: After masking, the value of the debug is compared against this value. More... | |
#define | LWIP_DBG_TYPES_ON LWIP_DBG_ON |
LWIP_DBG_TYPES_ON: A mask that can be used to globally enable/disable debug messages of certain types. More... | |
#define | LWIP_DHCP_AUTOIP_COOP 0 |
LWIP_DHCP_AUTOIP_COOP==1: Allow DHCP and AUTOIP to be both enabled on the same interface at the same time. More... | |
#define | LWIP_DHCP_AUTOIP_COOP_TRIES 9 |
LWIP_DHCP_AUTOIP_COOP_TRIES: Set to the number of DHCP DISCOVER probes that should be sent before falling back on AUTOIP. More... | |
#define | LWIP_DNS 0 |
LWIP_DNS==1: Turn on DNS module. More... | |
#define | LWIP_ETHERNET (LWIP_ARP || PPPOE_SUPPORT) |
LWIP_ETHERNET==1: enable ethernet support for PPPoE even though ARP might be disabled. More... | |
#define | LWIP_EVENT_API 0 |
LWIP_EVENT_API and LWIP_CALLBACK_API: Only one of these should be set to 1. More... | |
#define | LWIP_HAVE_LOOPIF 0 |
LWIP_HAVE_LOOPIF==1: Support loop interface (127.0.0.1) and loopif.c. More... | |
#define | LWIP_HAVE_SLIPIF 0 |
LWIP_HAVE_SLIPIF==1: Support slip interface and slipif.c. More... | |
#define | LWIP_ICMP 1 |
LWIP_ICMP==1: Enable ICMP module inside the IP stack. More... | |
#define | LWIP_IGMP 0 |
LWIP_IGMP==1: Turn on IGMP module. More... | |
#define | LWIP_LOOPBACK_MAX_PBUFS 0 |
LWIP_LOOPBACK_MAX_PBUFS: Maximum number of pbufs on queue for loopback sending for each netif (0 = disabled) More... | |
#define | LWIP_MULTICAST_PING 0 |
LWIP_MULTICAST_PING==1: respond to multicast pings (default is unicast only) More... | |
#define | LWIP_NETBUF_RECVINFO 0 |
UDP_TTL: Default Time-To-Live value. More... | |
#define | LWIP_NETCONN 1 |
LWIP_NETCONN==1: Enable Netconn API (require to use api_lib.c) More... | |
#define | LWIP_NETIF_API 0 |
LWIP_NETIF_API==1: Support netif api (in netifapi.c) More... | |
#define | LWIP_NETIF_HOSTNAME 0 |
PBUF_LINK_HLEN: the number of bytes that should be allocated for a link level header. More... | |
#define | LWIP_NETIF_HWADDRHINT 0 |
LWIP_NETIF_HWADDRHINT==1: Cache link-layer-address hints (e.g. More... | |
#define | LWIP_NETIF_LINK_CALLBACK 0 |
LWIP_NETIF_STATUS_CALLBACK==1: Support a callback function whenever an interface changes its up/down status (i.e., due to DHCP IP acquistion) More... | |
#define | LWIP_NETIF_LOOPBACK 0 |
LWIP_NETIF_LOOPBACK==1: Support sending packets with a destination IP address equal to the netif IP address, looping them back up the stack. More... | |
#define | LWIP_NETIF_LOOPBACK_MULTITHREADING (!NO_SYS) |
LWIP_NETIF_LOOPBACK_MULTITHREADING: Indicates whether threading is enabled in the system, as netifs must change how they behave depending on this setting for the LWIP_NETIF_LOOPBACK option to work. More... | |
#define | LWIP_NETIF_TX_SINGLE_PBUF 0 |
LWIP_NETIF_TX_SINGLE_PBUF: if this is set to 1, lwIP tries to put all data to be sent into one single pbuf. More... | |
#define | LWIP_POSIX_SOCKETS_IO_NAMES 1 |
LWIP_POSIX_SOCKETS_IO_NAMES==1: Enable POSIX-style sockets functions names. More... | |
#define | LWIP_RAW 1 |
LWIP_RAW==1: Enable application layer to hook into the IP layer itself. More... | |
#define | LWIP_SNMP 0 |
LWIP_SNMP==1: Turn on SNMP module. More... | |
#define | LWIP_SO_RCVBUF 0 |
LWIP_SO_RCVBUF==1: Enable SO_RCVBUF processing. More... | |
#define | LWIP_SO_RCVTIMEO 0 |
LWIP_SO_RCVTIMEO==1: Enable SO_RCVTIMEO processing. More... | |
#define | LWIP_SOCKET 1 |
LWIP_SOCKET==1: Enable Socket API (require to use sockets.c) More... | |
#define | LWIP_TCP_KEEPALIVE 0 |
LWIP_TCP_KEEPALIVE==1: Enable TCP_KEEPIDLE, TCP_KEEPINTVL and TCP_KEEPCNT options processing. More... | |
#define | LWIP_TCP_TIMESTAMPS 0 |
LWIP_TCP_TIMESTAMPS==1: support the TCP timestamp option. More... | |
#define | LWIP_TCPIP_CORE_LOCKING 0 |
TCPIP_THREAD_NAME: The name assigned to the main tcpip thread. More... | |
#define | LWIP_TCPIP_CORE_LOCKING_INPUT 0 |
LWIP_TCPIP_CORE_LOCKING_INPUT: (EXPERIMENTAL!) Don't use it if you're not an active lwIP project member. More... | |
#define | LWIP_TCPIP_TIMEOUT 1 |
LWIP_TCPIP_TIMEOUT==1: Enable tcpip_timeout/tcpip_untimeout tod create timers running in tcpip_thread from another thread. More... | |
#define | LWIP_UDPLITE 0 |
LWIP_UDP==1: Turn on UDP. More... | |
#define | MEM_LIBC_MALLOC 0 |
MEM_LIBC_MALLOC==1: Use malloc/free/realloc provided by your C-library instead of the lwip internal allocator. More... | |
#define | MEM_USE_POOLS 0 |
MEM_USE_POOLS==1: Use an alternative to malloc() by allocating from a set of memory pools of various sizes. More... | |
#define | MEM_USE_POOLS_TRY_BIGGER_POOL 0 |
MEM_USE_POOLS_TRY_BIGGER_POOL==1: if one malloc-pool is empty, try the next bigger pool - WARNING: THIS MIGHT WASTE MEMORY but it can make a system more reliable. More... | |
#define | MEMCPY(dst, src, len) memcpy(dst,src,len) |
MEMCPY: override this if you have a faster implementation at hand than the one included in your C library. More... | |
#define | MEMP_MEM_MALLOC 0 |
MEMP_MEM_MALLOC==1: Use mem_malloc/mem_free instead of the lwip pool allocator. More... | |
#define | MEMP_NUM_ARP_QUEUE 30 |
MEMP_NUM_ARP_QUEUE: the number of simulateously queued outgoing packets (pbufs) that are waiting for an ARP request (to resolve their destination address) to finish. More... | |
#define | MEMP_NUM_FRAG_PBUF 15 |
MEMP_NUM_FRAG_PBUF: the number of IP fragments simultaneously sent (fragments, not whole packets!). More... | |
#define | MEMP_NUM_IGMP_GROUP 8 |
MEMP_NUM_IGMP_GROUP: The number of multicast groups whose network interfaces can be members et the same time (one per netif - allsystems group -, plus one per netif membership). More... | |
#define | MEMP_NUM_LOCALHOSTLIST 1 |
MEMP_NUM_LOCALHOSTLIST: the number of host entries in the local host list if DNS_LOCAL_HOSTLIST_IS_DYNAMIC==1. More... | |
#define | MEMP_NUM_NETDB 1 |
MEMP_NUM_NETDB: the number of concurrently running lwip_addrinfo() calls (before freeing the corresponding memory using lwip_freeaddrinfo()). More... | |
#define | MEMP_NUM_PPPOE_INTERFACES 1 |
MEMP_NUM_PPPOE_INTERFACES: the number of concurrently active PPPoE interfaces (only used with PPPOE_SUPPORT==1) More... | |
#define | MEMP_NUM_REASSDATA 5 |
MEMP_NUM_PBUF: the number of memp struct pbufs (used for PBUF_ROM and PBUF_REF). More... | |
#define | MEMP_NUM_SNMP_NODE 50 |
MEMP_NUM_SNMP_NODE: the number of leafs in the SNMP tree. More... | |
#define | MEMP_NUM_SNMP_ROOTNODE 30 |
MEMP_NUM_SNMP_ROOTNODE: the number of branches in the SNMP tree. More... | |
#define | MEMP_NUM_SNMP_VALUE 3 |
MEMP_NUM_SNMP_VALUE: the number of OID or values concurrently used (does not have to be changed normally) - 3 of these are used per request (1 for the value read and 2 for OIDs - input and output) More... | |
#define | MEMP_NUM_SNMP_VARBIND 2 |
MEMP_NUM_SNMP_VARBIND: the number of concurrent requests (does not have to be changed normally) - 2 of these are used per request (1 for input, 1 for output) More... | |
#define | MEMP_NUM_TCPIP_MSG_API 8 |
MEMP_NUM_SYS_TIMEOUT: the number of simulateously active timeouts. More... | |
#define | MEMP_NUM_TCPIP_MSG_INPKT 8 |
MEMP_NUM_TCPIP_MSG_INPKT: the number of struct tcpip_msg, which are used for incoming packets. More... | |
#define | MEMP_OVERFLOW_CHECK 0 |
MEMP_OVERFLOW_CHECK: memp overflow protection reserves a configurable amount of bytes before and after each memp element in every pool and fills it with a prominent default value. More... | |
#define | MEMP_SANITY_CHECK 0 |
MEMP_SANITY_CHECK==1: run a sanity check after each memp_free() to make sure that there are no cycles in the linked lists. More... | |
#define | MEMP_SEPARATE_POOLS 0 |
MEM_ALIGNMENT: should be set to the alignment of the CPU 4 byte alignment -> #define MEM_ALIGNMENT 4 2 byte alignment -> #define MEM_ALIGNMENT 2. More... | |
#define | MEMP_USE_CUSTOM_POOLS 0 |
MEMP_USE_CUSTOM_POOLS==1: whether to include a user file lwippools.h that defines additional pools beyond the "standard" ones required by lwIP. More... | |
#define | NO_SYS 0 |
SYS_LIGHTWEIGHT_PROT==1: if you want inter-task protection for certain critical regions during buffer allocation, deallocation and memory allocation and deallocation. More... | |
#define | NO_SYS_NO_TIMERS 0 |
NO_SYS_NO_TIMERS==1: Drop support for sys_timeout when NO_SYS==1 Mainly for compatibility to old versions. More... | |
#define | PPP_DEBUG LWIP_DBG_OFF |
TCP_DEBUG: Enable debugging for TCP. More... | |
#define | PPP_SUPPORT 0 |
UDP_STATS==1: Enable UDP stats. More... | |
#define | PPPOE_SUPPORT 0 |
PPPOE_SUPPORT==1: Enable PPP Over Ethernet. More... | |
#define | PPPOS_SUPPORT PPP_SUPPORT |
PPPOS_SUPPORT==1: Enable PPP Over Serial. More... | |
#define | RAW_TTL (IP_DEFAULT_TTL) |
LWIP_RAW==1: Enable application layer to hook into the IP layer itself. More... | |
#define | RECV_BUFSIZE_DEFAULT INT_MAX |
If LWIP_SO_RCVBUF is used, this is the default value for recv_bufsize. More... | |
#define | SLIP_DEBUG LWIP_DBG_OFF |
SLIP_DEBUG: Enable debugging in slipif.c. More... | |
#define | SMEMCPY(dst, src, len) memcpy(dst,src,len) |
SMEMCPY: override this with care! Some compilers (e.g. More... | |
#define | SNMP_CONCURRENT_REQUESTS 1 |
SNMP_CONCURRENT_REQUESTS: Number of concurrent requests the module will allow. More... | |
#define | SNMP_MAX_OCTET_STRING_LEN 127 |
The maximum length of strings used. More... | |
#define | SNMP_MAX_TREE_DEPTH 15 |
The maximum depth of the SNMP tree. More... | |
#define | SNMP_MAX_VALUE_SIZE LWIP_MAX((SNMP_MAX_OCTET_STRING_LEN)+1, sizeof(s32_t)*(SNMP_MAX_TREE_DEPTH)) |
The size of the MEMP_SNMP_VALUE elements, normally calculated from SNMP_MAX_OCTET_STRING_LEN and SNMP_MAX_TREE_DEPTH. More... | |
#define | SNMP_MIB_DEBUG LWIP_DBG_OFF |
SNMP_MIB_DEBUG: Enable debugging for SNMP MIBs. More... | |
#define | SNMP_MSG_DEBUG LWIP_DBG_OFF |
SNMP_MSG_DEBUG: Enable debugging for SNMP messages. More... | |
#define | SNMP_PRIVATE_MIB 0 |
SNMP_PRIVATE_MIB: When using a private MIB, you have to create a file 'private_mib.h' that contains a 'struct mib_array_node mib_private' which contains your MIB. More... | |
#define | SNMP_SAFE_REQUESTS 1 |
Only allow SNMP write actions that are 'safe' (e.g. More... | |
#define | SNMP_TRAP_DESTINATIONS 1 |
SNMP_TRAP_DESTINATIONS: Number of trap destinations. More... | |
#define | SO_REUSE 0 |
SO_REUSE==1: Enable SO_REUSEADDR option. More... | |
#define | SO_REUSE_RXTOALL 0 |
SO_REUSE_RXTOALL==1: Pass a copy of incoming broadcast/multicast packets to all local matches if SO_REUSEADDR is turned on. More... | |
#define | TCP_CALCULATE_EFF_SEND_MSS 1 |
LWIP_TCP==1: Turn on TCP. More... | |
#define | TCP_DEFAULT_LISTEN_BACKLOG 0xff |
The maximum allowed backlog for TCP listen netconns. More... | |
#define | TCP_LISTEN_BACKLOG 0 |
TCP_LISTEN_BACKLOG: Enable the backlog option for tcp listen pcb. More... | |
#define | TCP_OVERSIZE TCP_MSS |
TCP_OVERSIZE: The maximum number of bytes that tcp_write may allocate ahead of time in an attempt to create shorter pbuf chains for transmission. More... | |
#define | TCP_SNDLOWAT ((TCP_SND_BUF)/2) |
TCP_SND_BUF: TCP sender buffer space (bytes). More... | |
#define | TCP_SNDQUEUELOWAT ((TCP_SND_QUEUELEN)/2) |
TCP_SNDQUEUELOWAT: TCP writable bufs (pbuf count). More... | |
#define | TCP_WND_UPDATE_THRESHOLD (TCP_WND / 4) |
TCP_WND_UPDATE_THRESHOLD: difference in window to trigger an explicit window update. More... | |
#define | TIMERS_DEBUG LWIP_DBG_OFF |
INET_DEBUG: Enable debugging in inet.c. More... | |
#define AUTOIP_DEBUG LWIP_DBG_OFF |
AUTOIP_DEBUG: Enable debugging in autoip.c.
#define CHECKSUM_CHECK_IP 1 |
CHECKSUM_CHECK_IP==1: Check checksums in software for incoming IP packets.
#define CHECKSUM_CHECK_TCP 1 |
CHECKSUM_CHECK_TCP==1: Check checksums in software for incoming TCP packets.
#define CHECKSUM_CHECK_UDP 1 |
CHECKSUM_CHECK_UDP==1: Check checksums in software for incoming UDP packets.
#define CHECKSUM_GEN_IP 1 |
CHECKSUM_GEN_IP==1: Generate checksums in software for outgoing IP packets.
#define CHECKSUM_GEN_TCP 1 |
CHECKSUM_GEN_TCP==1: Generate checksums in software for outgoing TCP packets.
Referenced by tcp_keepalive().
#define CHECKSUM_GEN_UDP 1 |
CHECKSUM_GEN_UDP==1: Generate checksums in software for outgoing UDP packets.
#define DHCP_DEBUG LWIP_DBG_OFF |
DHCP_DEBUG: Enable debugging in dhcp.c.
Referenced by dhcp_arp_reply(), dhcp_bind(), dhcp_check(), dhcp_coarse_tmr(), dhcp_create_msg(), dhcp_decline(), dhcp_discover(), dhcp_fine_tmr(), dhcp_handle_nak(), dhcp_handle_offer(), dhcp_inform(), dhcp_parse_reply(), dhcp_rebind(), dhcp_reboot(), dhcp_recv(), dhcp_release(), dhcp_renew(), dhcp_select(), dhcp_start(), dhcp_stop(), dhcp_t1_timeout(), dhcp_t2_timeout(), and dhcp_timeout().
LWIP_DHCP==1: Enable DHCP module.
DHCP_DOES_ARP_CHECK==1: Do an ARP check on the offered address.
#define DNS_DEBUG LWIP_DBG_OFF |
DNS_DEBUG: Enable debugging for DNS.
#define DNS_DOES_NAME_CHECK 1 |
DNS do a name checking between the query and the response.
#define DNS_LOCAL_HOSTLIST 0 |
DNS_LOCAL_HOSTLIST: Implements a local host-to-address list.
If enabled, you have to define #define DNS_LOCAL_HOSTLIST_INIT {{"host1", 0x123}, {"host2", 0x234}} (an array of structs name/address, where address is an u32_t in network byte order).
Instead, you can also use an external function: #define DNS_LOOKUP_LOCAL_EXTERN(x) extern u32_t my_lookup_function(const char *name) that returns the IP address or INADDR_NONE if not found.
#define DNS_LOCAL_HOSTLIST_IS_DYNAMIC 0 |
If this is turned on, the local host-list can be dynamically changed at runtime.
#define DNS_MAX_NAME_LENGTH 256 |
DNS maximum host name length supported in the name table.
#define DNS_MAX_SERVERS 2 |
The maximum of DNS servers.
Referenced by dhcp_handle_ack(), and dhcp_parse_reply().
#define DNS_MSG_SIZE 512 |
DNS message max.
size. Default value is RFC compliant.
#define DNS_TABLE_SIZE 4 |
DNS maximum number of entries to maintain locally.
#define ETHARP_STATS (LWIP_ARP) |
LWIP_STATS==1: Enable statistics collection in lwip_stats.
LWIP_STATS_DISPLAY==1: Compile in the statistics output functions. LINK_STATS==1: Enable link stats. ETHARP_STATS==1: Enable etharp stats.
#define ETHARP_SUPPORT_STATIC_ENTRIES 0 |
ETH_PAD_SIZE: number of bytes added before the ethernet header to ensure alignment of payload after that header.
Since the header is 14 bytes long, without this padding e.g. addresses in the IP header will not be aligned on a 32-bit boundary, so setting this to 2 can speed up 32-bit-platforms. ETHARP_SUPPORT_STATIC_ENTRIES==1: enable code to support static ARP table entries (using etharp_add_static_entry/etharp_remove_static_entry).
Referenced by etharp_tmr().
#define ETHARP_SUPPORT_VLAN 0 |
ETHARP_SUPPORT_VLAN==1: support receiving ethernet packets with VLAN header.
Additionally, you can define ETHARP_VLAN_CHECK to an u16_t VLAN ID to check. If ETHARP_VLAN_CHECK is defined, only VLAN-traffic for this VLAN is accepted. If ETHARP_VLAN_CHECK is not defined, all traffic is accepted.
#define ETHARP_TRUST_IP_MAC 0 |
ARP_TABLE_SIZE: Number of active MAC-IP address pairs cached.
ARP_QUEUEING==1: Multiple outgoing packets are queued during hardware address resolution. By default, only the most recent packet is queued per IP address. This is sufficient for most protocols and mainly reduces TCP connection startup time. Set this to 1 if you know your application sends more than one packet in a row to an IP address that is not in the ARP cache. ETHARP_TRUST_IP_MAC==1: Incoming IP packets cause the ARP table to be updated with the source MAC and IP addresses supplied in the packet. You may want to disable this if you do not trust LAN peers to have the correct addresses, or as a limited approach to attempt to handle spoofing. If disabled, lwIP will need to make a new ARP request if the peer is not already in the ARP table, adding a little latency. The peer is in the ARP table if it requested our address before. Also notice that this slows down input processing of every IP packet!
#define IGMP_DEBUG LWIP_DBG_OFF |
ETHARP_DEBUG: Enable debugging in etharp.c.
NETIF_DEBUG: Enable debugging in netif.c. PBUF_DEBUG: Enable debugging in pbuf.c. API_LIB_DEBUG: Enable debugging in api_lib.c. API_MSG_DEBUG: Enable debugging in api_msg.c. SOCKETS_DEBUG: Enable debugging in sockets.c. ICMP_DEBUG: Enable debugging in icmp.c. IGMP_DEBUG: Enable debugging in igmp.c.
#define IGMP_STATS (LWIP_IGMP) |
ICMP_STATS==1: Enable ICMP stats.
IGMP_STATS==1: Enable IGMP stats.
#define IP_DEFAULT_TTL 255 |
IP_FRAG_MAX_MTU: Assumed max MTU on any interface for IP frag buffer (requires IP_FRAG_USES_STATIC_BUF==1)
IP_DEFAULT_TTL: Default value for Time-To-Live used by transport layers.
#define IP_FRAG 1 |
IP_FRAG==1: Fragment outgoing IP packets if their size exceeds MTU.
Note that this option does not affect incoming packet sizes, which can be controlled via IP_REASSEMBLY.
#define IP_FRAG_USES_STATIC_BUF 0 |
IP_FRAG_USES_STATIC_BUF==1: Use a static MTU-sized buffer for IP fragmentation.
Otherwise pbufs are allocated and reference the original packet data to be fragmented (or with LWIP_NETIF_TX_SINGLE_PBUF==1, new PBUF_RAM pbufs are used for fragments). ATTENTION: IP_FRAG_USES_STATIC_BUF==1 may not be used for DMA-enabled MACs!
#define IP_OPTIONS_ALLOWED 1 |
IP_FORWARD==1: Enables the ability to forward IP packets across network interfaces.
If you are going to run lwIP on a device with only one network interface, define this to 0. IP_OPTIONS_ALLOWED: Defines the behavior for IP options. IP_OPTIONS_ALLOWED==0: All packets with IP options are dropped. IP_OPTIONS_ALLOWED==1: IP options are allowed (but not parsed).
#define IP_REASS_MAX_PBUFS 10 |
IP_REASS_MAX_PBUFS: Total maximum amount of pbufs waiting to be reassembled.
Since the received pbufs are enqueued, be sure to configure PBUF_POOL_SIZE > IP_REASS_MAX_PBUFS so that the stack is still able to receive packets even if the maximum amount of fragments is enqueued for reassembly!
Referenced by ip_reass().
#define IP_REASS_MAXAGE 3 |
IP_REASS_MAXAGE: Maximum time (in multiples of IP_TMR_INTERVAL - so seconds, normally) a fragmented IP packet waits for all fragments to arrive.
If not all fragments arrived in this time, the whole packet is discarded.
Referenced by ip_reass_enqueue_new_datagram().
#define IP_REASSEMBLY 1 |
IP_REASSEMBLY==1: Reassemble incoming fragmented IP packets.
Note that this option does not affect outgoing packet sizes, which can be controlled via IP_FRAG.
#define IP_SOF_BROADCAST 0 |
IP_SOF_BROADCAST=1: Use the SOF_BROADCAST field to enable broadcast filter per pcb on udp and raw send operations.
To enable broadcast filter on recv operations, you also have to set IP_SOF_BROADCAST_RECV=1.
#define IP_SOF_BROADCAST_RECV 0 |
IP_SOF_BROADCAST_RECV (requires IP_SOF_BROADCAST=1) enable the broadcast filter on recv operations.
Referenced by udp_input().
#define IPFRAG_STATS (IP_REASSEMBLY || IP_FRAG) |
IP_STATS==1: Enable IP stats.
IPFRAG_STATS==1: Enable IP fragmentation stats. Default is on if using either frag or reass.
#define LWIP_ALLOW_MEM_FREE_FROM_OTHER_CONTEXT 0 |
Set this to 1 if you want to free PBUF_RAM pbufs (or call mem_free()) from interrupt context (or another context that doesn't allow waiting for a semaphore).
If set to 1, mem_malloc will be protected by a semaphore and SYS_ARCH_PROTECT, while mem_free will only use SYS_ARCH_PROTECT. mem_malloc SYS_ARCH_UNPROTECTs with each loop so that mem_free can run.
ATTENTION: As you can see from the above description, this leads to dis-/ enabling interrupts often, which can be slow! Also, on low memory, mem_malloc can need longer.
If you don't want that, at least for NO_SYS=0, you can still use the following functions to enqueue a deallocation call which then runs in the tcpip_thread context:
#define LWIP_ARP 1 |
PBUF_POOL_SIZE: the number of buffers in the pbuf pool.
LWIP_ARP==1: Enable ARP functionality.
#define LWIP_AUTOIP 0 |
LWIP_AUTOIP==1: Enable AUTOIP module.
Referenced by netif_set_ipaddr().
#define LWIP_BROADCAST_PING 0 |
ICMP_TTL: Default value for Time-To-Live used by ICMP packets.
LWIP_BROADCAST_PING==1: respond to broadcast pings (default is unicast only)
#define LWIP_CALLBACK_API 1 |
#define LWIP_CHECKSUM_ON_COPY 0 |
LWIP_CHECKSUM_ON_COPY==1: Calculate checksum when copying data from application buffers to pbufs.
#define LWIP_COMPAT_SOCKETS 1 |
LWIP_COMPAT_SOCKETS==1: Enable BSD-style sockets functions names.
(only used if you use sockets.c)
#define LWIP_DBG_MIN_LEVEL LWIP_DBG_LEVEL_ALL |
LWIP_DBG_MIN_LEVEL: After masking, the value of the debug is compared against this value.
If it is smaller, then debugging messages are written.
#define LWIP_DBG_TYPES_ON LWIP_DBG_ON |
LWIP_DBG_TYPES_ON: A mask that can be used to globally enable/disable debug messages of certain types.
#define LWIP_DHCP_AUTOIP_COOP 0 |
LWIP_DHCP_AUTOIP_COOP==1: Allow DHCP and AUTOIP to be both enabled on the same interface at the same time.
#define LWIP_DHCP_AUTOIP_COOP_TRIES 9 |
LWIP_DHCP_AUTOIP_COOP_TRIES: Set to the number of DHCP DISCOVER probes that should be sent before falling back on AUTOIP.
This can be set as low as 1 to get an AutoIP address very quickly, but you should be prepared to handle a changing IP address when DHCP overrides AutoIP.
Referenced by dhcp_discover().
#define LWIP_DNS 0 |
LWIP_DNS==1: Turn on DNS module.
UDP must be available for DNS transport.
#define LWIP_ETHERNET (LWIP_ARP || PPPOE_SUPPORT) |
LWIP_ETHERNET==1: enable ethernet support for PPPoE even though ARP might be disabled.
#define LWIP_EVENT_API 0 |
LWIP_EVENT_API and LWIP_CALLBACK_API: Only one of these should be set to 1.
LWIP_EVENT_API==1: The user defines lwip_tcp_event() to receive all events (accept, sent, etc) that happen in the system. LWIP_CALLBACK_API==1: The PCB callback function is called directly for the event.
#define LWIP_HAVE_LOOPIF 0 |
LWIP_HAVE_LOOPIF==1: Support loop interface (127.0.0.1) and loopif.c.
#define LWIP_HAVE_SLIPIF 0 |
LWIP_HAVE_SLIPIF==1: Support slip interface and slipif.c.
#define LWIP_ICMP 1 |
LWIP_ICMP==1: Enable ICMP module inside the IP stack.
Be careful, disable that make your product non-compliant to RFC1122
#define LWIP_IGMP 0 |
LWIP_IGMP==1: Turn on IGMP module.
Referenced by udp_input().
#define LWIP_LOOPBACK_MAX_PBUFS 0 |
LWIP_LOOPBACK_MAX_PBUFS: Maximum number of pbufs on queue for loopback sending for each netif (0 = disabled)
#define LWIP_MULTICAST_PING 0 |
LWIP_MULTICAST_PING==1: respond to multicast pings (default is unicast only)
#define LWIP_NETBUF_RECVINFO 0 |
UDP_TTL: Default Time-To-Live value.
LWIP_NETBUF_RECVINFO==1: append destination addr and port to every netbuf.
#define LWIP_NETCONN 1 |
LWIP_NETCONN==1: Enable Netconn API (require to use api_lib.c)
#define LWIP_NETIF_API 0 |
LWIP_NETIF_API==1: Support netif api (in netifapi.c)
#define LWIP_NETIF_HOSTNAME 0 |
PBUF_LINK_HLEN: the number of bytes that should be allocated for a link level header.
The default is 14, the standard value for Ethernet. PBUF_POOL_BUFSIZE: the size of each pbuf in the pbuf pool. The default is designed to accomodate single full size TCP frame in one pbuf, including TCP_MSS, IP header, and link header. LWIP_NETIF_HOSTNAME==1: use DHCP_OPTION_HOSTNAME with netif's hostname field.
#define LWIP_NETIF_HWADDRHINT 0 |
LWIP_NETIF_HWADDRHINT==1: Cache link-layer-address hints (e.g.
table indices) in struct netif. TCP and UDP can make use of this to prevent scanning the ARP table for every sent packet. While this is faster for big ARP tables or many concurrent connections, it might be counterproductive if you have a tiny ARP table or if there never are concurrent connections.
#define LWIP_NETIF_LINK_CALLBACK 0 |
LWIP_NETIF_STATUS_CALLBACK==1: Support a callback function whenever an interface changes its up/down status (i.e., due to DHCP IP acquistion)
LWIP_NETIF_LINK_CALLBACK==1: Support a callback function from an interface whenever the link changes (i.e., link down)
#define LWIP_NETIF_LOOPBACK 0 |
LWIP_NETIF_LOOPBACK==1: Support sending packets with a destination IP address equal to the netif IP address, looping them back up the stack.
#define LWIP_NETIF_LOOPBACK_MULTITHREADING (!NO_SYS) |
LWIP_NETIF_LOOPBACK_MULTITHREADING: Indicates whether threading is enabled in the system, as netifs must change how they behave depending on this setting for the LWIP_NETIF_LOOPBACK option to work.
Setting this is needed to avoid reentering non-reentrant functions like tcp_input(). LWIP_NETIF_LOOPBACK_MULTITHREADING==1: Indicates that the user is using a multithreaded environment like tcpip.c. In this case, netif->input() is called directly. LWIP_NETIF_LOOPBACK_MULTITHREADING==0: Indicates a polling (or NO_SYS) setup. The packets are put on a list and netif_poll() must be called in the main application loop.
#define LWIP_NETIF_TX_SINGLE_PBUF 0 |
LWIP_NETIF_TX_SINGLE_PBUF: if this is set to 1, lwIP tries to put all data to be sent into one single pbuf.
This is for compatibility with DMA-enabled MACs that do not support scatter-gather. Beware that this might involve CPU-memcpy before transmitting that would not be needed without this flag! Use this only if you need to!
#define LWIP_POSIX_SOCKETS_IO_NAMES 1 |
LWIP_POSIX_SOCKETS_IO_NAMES==1: Enable POSIX-style sockets functions names.
Disable this option if you use a POSIX operating system that uses the same names (read, write & close). (only used if you use sockets.c)
#define LWIP_RAW 1 |
LWIP_RAW==1: Enable application layer to hook into the IP layer itself.
#define LWIP_SNMP 0 |
LWIP_SNMP==1: Turn on SNMP module.
UDP must be available for SNMP transport.
#define LWIP_SO_RCVBUF 0 |
LWIP_SO_RCVBUF==1: Enable SO_RCVBUF processing.
#define LWIP_SO_RCVTIMEO 0 |
LWIP_SO_RCVTIMEO==1: Enable SO_RCVTIMEO processing.
#define LWIP_SOCKET 1 |
LWIP_SOCKET==1: Enable Socket API (require to use sockets.c)
#define LWIP_TCP_KEEPALIVE 0 |
#define LWIP_TCP_TIMESTAMPS 0 |
LWIP_TCP_TIMESTAMPS==1: support the TCP timestamp option.
#define LWIP_TCPIP_CORE_LOCKING 0 |
TCPIP_THREAD_NAME: The name assigned to the main tcpip thread.
TCPIP_THREAD_STACKSIZE: The stack size used by the main tcpip thread. The stack size value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created. TCPIP_THREAD_PRIO: The priority assigned to the main tcpip thread. The priority value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created. TCPIP_MBOX_SIZE: The mailbox size for the tcpip thread messages The queue size value itself is platform-dependent, but is passed to sys_mbox_new() when tcpip_init is called. SLIPIF_THREAD_NAME: The name assigned to the slipif_loop thread. SLIP_THREAD_STACKSIZE: The stack size used by the slipif_loop thread. The stack size value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created. SLIPIF_THREAD_PRIO: The priority assigned to the slipif_loop thread. The priority value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created. PPP_THREAD_NAME: The name assigned to the pppInputThread. PPP_THREAD_STACKSIZE: The stack size used by the pppInputThread. The stack size value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created. PPP_THREAD_PRIO: The priority assigned to the pppInputThread. The priority value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created. DEFAULT_THREAD_NAME: The name assigned to any other lwIP thread. DEFAULT_THREAD_STACKSIZE: The stack size used by any other lwIP thread. The stack size value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created. DEFAULT_THREAD_PRIO: The priority assigned to any other lwIP thread. The priority value itself is platform-dependent, but is passed to sys_thread_new() when the thread is created. DEFAULT_RAW_RECVMBOX_SIZE: The mailbox size for the incoming packets on a NETCONN_RAW. The queue size value itself is platform-dependent, but is passed to sys_mbox_new() when the recvmbox is created. DEFAULT_UDP_RECVMBOX_SIZE: The mailbox size for the incoming packets on a NETCONN_UDP. The queue size value itself is platform-dependent, but is passed to sys_mbox_new() when the recvmbox is created. DEFAULT_TCP_RECVMBOX_SIZE: The mailbox size for the incoming packets on a NETCONN_TCP. The queue size value itself is platform-dependent, but is passed to sys_mbox_new() when the recvmbox is created. DEFAULT_ACCEPTMBOX_SIZE: The mailbox size for the incoming connections. The queue size value itself is platform-dependent, but is passed to sys_mbox_new() when the acceptmbox is created. LWIP_TCPIP_CORE_LOCKING: (EXPERIMENTAL!) Don't use it if you're not an active lwIP project member
#define LWIP_TCPIP_CORE_LOCKING_INPUT 0 |
LWIP_TCPIP_CORE_LOCKING_INPUT: (EXPERIMENTAL!) Don't use it if you're not an active lwIP project member.
#define LWIP_TCPIP_TIMEOUT 1 |
LWIP_TCPIP_TIMEOUT==1: Enable tcpip_timeout/tcpip_untimeout tod create timers running in tcpip_thread from another thread.
#define LWIP_UDPLITE 0 |
LWIP_UDP==1: Turn on UDP.
LWIP_UDPLITE==1: Turn on UDP-Lite. (Requires LWIP_UDP)
#define MEM_LIBC_MALLOC 0 |
MEM_LIBC_MALLOC==1: Use malloc/free/realloc provided by your C-library instead of the lwip internal allocator.
Can save code size if you already use it.
#define MEM_USE_POOLS 0 |
MEM_USE_POOLS==1: Use an alternative to malloc() by allocating from a set of memory pools of various sizes.
When mem_malloc is called, an element of the smallest pool that can provide the length needed is returned. To use this, MEMP_USE_CUSTOM_POOLS also has to be enabled.
#define MEM_USE_POOLS_TRY_BIGGER_POOL 0 |
MEM_USE_POOLS_TRY_BIGGER_POOL==1: if one malloc-pool is empty, try the next bigger pool - WARNING: THIS MIGHT WASTE MEMORY but it can make a system more reliable.
#define MEMCPY | ( | dst, | |
src, | |||
len | |||
) | memcpy(dst,src,len) |
MEMCPY: override this if you have a faster implementation at hand than the one included in your C library.
Referenced by lwip_accept(), lwip_getaddrname(), lwip_recvfrom(), lwip_sendto(), pbuf_copy(), pbuf_copy_partial(), and pbuf_take().
#define MEMP_MEM_MALLOC 0 |
MEMP_MEM_MALLOC==1: Use mem_malloc/mem_free instead of the lwip pool allocator.
Especially useful with MEM_LIBC_MALLOC but handle with care regarding execution speed and usage from interrupts!
#define MEMP_NUM_ARP_QUEUE 30 |
MEMP_NUM_ARP_QUEUE: the number of simulateously queued outgoing packets (pbufs) that are waiting for an ARP request (to resolve their destination address) to finish.
(requires the ARP_QUEUEING option)
#define MEMP_NUM_FRAG_PBUF 15 |
MEMP_NUM_FRAG_PBUF: the number of IP fragments simultaneously sent (fragments, not whole packets!).
This is only used with IP_FRAG_USES_STATIC_BUF==0 and LWIP_NETIF_TX_SINGLE_PBUF==0 and only has to be > 1 with DMA-enabled MACs where the packet is not yet sent when netif->output returns.
#define MEMP_NUM_IGMP_GROUP 8 |
MEMP_NUM_IGMP_GROUP: The number of multicast groups whose network interfaces can be members et the same time (one per netif - allsystems group -, plus one per netif membership).
(requires the LWIP_IGMP option)
#define MEMP_NUM_LOCALHOSTLIST 1 |
MEMP_NUM_LOCALHOSTLIST: the number of host entries in the local host list if DNS_LOCAL_HOSTLIST_IS_DYNAMIC==1.
#define MEMP_NUM_NETDB 1 |
MEMP_NUM_NETDB: the number of concurrently running lwip_addrinfo() calls (before freeing the corresponding memory using lwip_freeaddrinfo()).
#define MEMP_NUM_PPPOE_INTERFACES 1 |
MEMP_NUM_PPPOE_INTERFACES: the number of concurrently active PPPoE interfaces (only used with PPPOE_SUPPORT==1)
#define MEMP_NUM_REASSDATA 5 |
MEMP_NUM_PBUF: the number of memp struct pbufs (used for PBUF_ROM and PBUF_REF).
If the application sends a lot of data out of ROM (or other static memory), this should be set high. MEMP_NUM_RAW_PCB: Number of raw connection PCBs (requires the LWIP_RAW option) MEMP_NUM_UDP_PCB: the number of UDP protocol control blocks. One per active UDP "connection". (requires the LWIP_UDP option) MEMP_NUM_TCP_PCB: the number of simulatenously active TCP connections. (requires the LWIP_TCP option) MEMP_NUM_TCP_PCB_LISTEN: the number of listening TCP connections. (requires the LWIP_TCP option) MEMP_NUM_TCP_SEG: the number of simultaneously queued TCP segments. (requires the LWIP_TCP option) MEMP_NUM_REASSDATA: the number of IP packets simultaneously queued for reassembly (whole packets, not fragments!)
#define MEMP_NUM_SNMP_NODE 50 |
MEMP_NUM_SNMP_NODE: the number of leafs in the SNMP tree.
#define MEMP_NUM_SNMP_ROOTNODE 30 |
MEMP_NUM_SNMP_ROOTNODE: the number of branches in the SNMP tree.
Every branch has one leaf (MEMP_NUM_SNMP_NODE) at least!
#define MEMP_NUM_SNMP_VALUE 3 |
MEMP_NUM_SNMP_VALUE: the number of OID or values concurrently used (does not have to be changed normally) - 3 of these are used per request (1 for the value read and 2 for OIDs - input and output)
#define MEMP_NUM_SNMP_VARBIND 2 |
MEMP_NUM_SNMP_VARBIND: the number of concurrent requests (does not have to be changed normally) - 2 of these are used per request (1 for input, 1 for output)
#define MEMP_NUM_TCPIP_MSG_API 8 |
MEMP_NUM_SYS_TIMEOUT: the number of simulateously active timeouts.
(requires NO_SYS==0) MEMP_NUM_NETBUF: the number of struct netbufs. (only needed if you use the sequential API, like api_lib.c) MEMP_NUM_NETCONN: the number of struct netconns. (only needed if you use the sequential API, like api_lib.c) MEMP_NUM_TCPIP_MSG_API: the number of struct tcpip_msg, which are used for callback/timeout API communication. (only needed if you use tcpip.c)
#define MEMP_NUM_TCPIP_MSG_INPKT 8 |
#define MEMP_OVERFLOW_CHECK 0 |
MEMP_OVERFLOW_CHECK: memp overflow protection reserves a configurable amount of bytes before and after each memp element in every pool and fills it with a prominent default value.
MEMP_OVERFLOW_CHECK == 0 no checking MEMP_OVERFLOW_CHECK == 1 checks each element when it is freed MEMP_OVERFLOW_CHECK >= 2 checks each element in every pool every time memp_malloc() or memp_free() is called (useful but slow!)
Referenced by memp_init().
#define MEMP_SANITY_CHECK 0 |
MEMP_SANITY_CHECK==1: run a sanity check after each memp_free() to make sure that there are no cycles in the linked lists.
#define MEMP_SEPARATE_POOLS 0 |
MEM_ALIGNMENT: should be set to the alignment of the CPU 4 byte alignment -> #define MEM_ALIGNMENT 4 2 byte alignment -> #define MEM_ALIGNMENT 2.
MEM_SIZE: the size of the heap memory. If the application will send a lot of data that needs to be copied, this should be set high. MEMP_SEPARATE_POOLS: if defined to 1, each pool is placed in its own array. This can be used to individually change the location of each pool. Default is one big array for all pools
#define MEMP_USE_CUSTOM_POOLS 0 |
MEMP_USE_CUSTOM_POOLS==1: whether to include a user file lwippools.h that defines additional pools beyond the "standard" ones required by lwIP.
If you set this to 1, you must have lwippools.h in your inlude path somewhere.
#define NO_SYS 0 |
SYS_LIGHTWEIGHT_PROT==1: if you want inter-task protection for certain critical regions during buffer allocation, deallocation and memory allocation and deallocation.
NO_SYS==1: Provides VERY minimal functionality. Otherwise, use lwIP facilities.
#define NO_SYS_NO_TIMERS 0 |
NO_SYS_NO_TIMERS==1: Drop support for sys_timeout when NO_SYS==1 Mainly for compatibility to old versions.
#define PPP_DEBUG LWIP_DBG_OFF |
TCP_DEBUG: Enable debugging for TCP.
TCP_INPUT_DEBUG: Enable debugging in tcp_in.c for incoming debug. TCP_FR_DEBUG: Enable debugging in tcp_in.c for fast retransmit. TCP_RTO_DEBUG: Enable debugging in TCP for retransmit timeout. TCP_CWND_DEBUG: Enable debugging for TCP congestion window. TCP_WND_DEBUG: Enable debugging in tcp_in.c for window updating. TCP_OUTPUT_DEBUG: Enable debugging in tcp_out.c output functions. TCP_RST_DEBUG: Enable debugging for TCP with the RST message. TCP_QLEN_DEBUG: Enable debugging for TCP queue lengths. UDP_DEBUG: Enable debugging in UDP. TCPIP_DEBUG: Enable debugging in tcpip.c. PPP_DEBUG: Enable debugging for PPP.
#define PPP_SUPPORT 0 |
UDP_STATS==1: Enable UDP stats.
Default is on if UDP enabled, otherwise off. TCP_STATS==1: Enable TCP stats. Default is on if TCP enabled, otherwise off. MEM_STATS==1: Enable mem.c stats. MEMP_STATS==1: Enable memp.c pool stats. SYS_STATS==1: Enable system stats (sem and mbox counts, etc). PPP_SUPPORT==1: Enable PPP.
#define PPPOE_SUPPORT 0 |
PPPOE_SUPPORT==1: Enable PPP Over Ethernet.
#define PPPOS_SUPPORT PPP_SUPPORT |
PPPOS_SUPPORT==1: Enable PPP Over Serial.
#define RAW_TTL (IP_DEFAULT_TTL) |
LWIP_RAW==1: Enable application layer to hook into the IP layer itself.
Referenced by raw_new().
#define RECV_BUFSIZE_DEFAULT INT_MAX |
If LWIP_SO_RCVBUF is used, this is the default value for recv_bufsize.
Referenced by netconn_alloc().
#define SLIP_DEBUG LWIP_DBG_OFF |
SLIP_DEBUG: Enable debugging in slipif.c.
#define SMEMCPY | ( | dst, | |
src, | |||
len | |||
) | memcpy(dst,src,len) |
SMEMCPY: override this with care! Some compilers (e.g.
gcc) can inline a call to memcpy() if the length is known at compile time and is small.
Referenced by icmp_send_response(), ip_frag(), ip_reass(), ip_reass_enqueue_new_datagram(), ip_reass_free_complete_datagram(), and tcp_seg_copy().
#define SNMP_CONCURRENT_REQUESTS 1 |
SNMP_CONCURRENT_REQUESTS: Number of concurrent requests the module will allow.
At least one request buffer is required. Does not have to be changed unless external MIBs answer request asynchronously
#define SNMP_MAX_OCTET_STRING_LEN 127 |
The maximum length of strings used.
This affects the size of MEMP_SNMP_VALUE elements.
#define SNMP_MAX_TREE_DEPTH 15 |
The maximum depth of the SNMP tree.
With private MIBs enabled, this depends on your MIB! This affects the size of MEMP_SNMP_VALUE elements.
#define SNMP_MAX_VALUE_SIZE LWIP_MAX((SNMP_MAX_OCTET_STRING_LEN)+1, sizeof(s32_t)*(SNMP_MAX_TREE_DEPTH)) |
The size of the MEMP_SNMP_VALUE elements, normally calculated from SNMP_MAX_OCTET_STRING_LEN and SNMP_MAX_TREE_DEPTH.
#define SNMP_MIB_DEBUG LWIP_DBG_OFF |
SNMP_MIB_DEBUG: Enable debugging for SNMP MIBs.
#define SNMP_MSG_DEBUG LWIP_DBG_OFF |
SNMP_MSG_DEBUG: Enable debugging for SNMP messages.
#define SNMP_PRIVATE_MIB 0 |
SNMP_PRIVATE_MIB: When using a private MIB, you have to create a file 'private_mib.h' that contains a 'struct mib_array_node mib_private' which contains your MIB.
#define SNMP_SAFE_REQUESTS 1 |
Only allow SNMP write actions that are 'safe' (e.g.
disabeling netifs is not a safe action and disabled when SNMP_SAFE_REQUESTS = 1). Unsafe requests are disabled by default!
#define SNMP_TRAP_DESTINATIONS 1 |
SNMP_TRAP_DESTINATIONS: Number of trap destinations.
At least one trap destination is required
#define SO_REUSE 0 |
SO_REUSE==1: Enable SO_REUSEADDR option.
#define SO_REUSE_RXTOALL 0 |
SO_REUSE_RXTOALL==1: Pass a copy of incoming broadcast/multicast packets to all local matches if SO_REUSEADDR is turned on.
WARNING: Adds a memcpy for every packet if passing to more than one pcb!
#define TCP_CALCULATE_EFF_SEND_MSS 1 |
LWIP_TCP==1: Turn on TCP.
TCP_TTL: Default Time-To-Live value. TCP_WND: The size of a TCP window. This must be at least (2 * TCP_MSS) for things to work well TCP_MAXRTX: Maximum number of retransmissions of data segments. TCP_SYNMAXRTX: Maximum number of retransmissions of SYN segments. TCP_QUEUE_OOSEQ==1: TCP will queue segments that arrive out of order. Define to 0 if your device is low on memory. TCP_MSS: TCP Maximum segment size. (default is 536, a conservative default, you might want to increase this.) For the receive side, this MSS is advertised to the remote side when opening a connection. For the transmit size, this MSS sets an upper limit on the MSS advertised by the remote host. TCP_CALCULATE_EFF_SEND_MSS: "The maximum size of a segment that TCP really sends, the 'effective send MSS,' MUST be the smaller of the send MSS (which reflects the available reassembly buffer size at the remote host) and the largest size permitted by the IP layer" (RFC 1122) Setting this to 1 enables code that checks TCP_MSS against the MTU of the netif used for a connection and limits the MSS if it would be too big otherwise.
#define TCP_DEFAULT_LISTEN_BACKLOG 0xff |
The maximum allowed backlog for TCP listen netconns.
This backlog is used unless another is explicitly specified. 0xff is the maximum (u8_t).
#define TCP_LISTEN_BACKLOG 0 |
TCP_LISTEN_BACKLOG: Enable the backlog option for tcp listen pcb.
#define TCP_OVERSIZE TCP_MSS |
TCP_OVERSIZE: The maximum number of bytes that tcp_write may allocate ahead of time in an attempt to create shorter pbuf chains for transmission.
The meaningful range is 0 to TCP_MSS. Some suggested values are:
0: Disable oversized allocation. Each tcp_write() allocates a new pbuf (old behaviour). 1: Allocate size-aligned pbufs with minimal excess. Use this if your scatter-gather DMA requires aligned fragments. 128: Limit the pbuf/memory overhead to 20%. TCP_MSS: Try to create unfragmented TCP packets. TCP_MSS/4: Try to create 4 fragments or less per TCP packet.
Referenced by tcp_pbuf_prealloc().
#define TCP_SNDLOWAT ((TCP_SND_BUF)/2) |
TCP_SND_BUF: TCP sender buffer space (bytes).
TCP_SND_QUEUELEN: TCP sender buffer space (pbufs). This must be at least as much as (2 * TCP_SND_BUF/TCP_MSS) for things to work. TCP_SNDLOWAT: TCP writable space (bytes). This must be less than TCP_SND_BUF. It is the amount of space which must be available in the TCP snd_buf for select to return writable (combined with TCP_SNDQUEUELOWAT).
Referenced by do_writemore(), poll_tcp(), and sent_tcp().
#define TCP_SNDQUEUELOWAT ((TCP_SND_QUEUELEN)/2) |
TCP_SNDQUEUELOWAT: TCP writable bufs (pbuf count).
This must be grater than TCP_SND_QUEUELEN. If the number of pbufs queued on a pcb drops below this number, select returns writable (combined with TCP_SNDLOWAT).
Referenced by do_writemore(), poll_tcp(), and sent_tcp().
#define TCP_WND_UPDATE_THRESHOLD (TCP_WND / 4) |
TCP_WND_UPDATE_THRESHOLD: difference in window to trigger an explicit window update.
Referenced by tcp_recved().
#define TIMERS_DEBUG LWIP_DBG_OFF |
INET_DEBUG: Enable debugging in inet.c.
IP_DEBUG: Enable debugging for IP. IP_REASS_DEBUG: Enable debugging in ip_frag.c for both frag & reass. RAW_DEBUG: Enable debugging in raw.c. MEM_DEBUG: Enable debugging in mem.c. MEMP_DEBUG: Enable debugging in memp.c. SYS_DEBUG: Enable debugging in sys.c. TIMERS_DEBUG: Enable debugging in timers.c.
Referenced by arp_timer(), dhcp_timer_coarse(), dhcp_timer_fine(), and ip_reass_timer().