Microchip® Advanced Software Framework

conf_usb_host.h File Reference

USB host configuration file.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"
#include "uhi_aoa.h"
#include "ui.h"

Macros

#define USB_HOST_UHI   UHI_AOA
 USB Host Configuration. More...
 
#define USB_HOST_POWER_MAX   500
 Maximum current allowed on Vbus (mA) More...
 
#define UHC_MODE_CHANGE(b_host_mode)   ui_usb_mode_change(b_host_mode)
 Authorize the USB HUB support. More...
 
#define UHC_VBUS_CHANGE(b_present)   ui_usb_vbus_change(b_present)
 To notify that the Vbus level has changed. More...
 
#define UHC_VBUS_ERROR()   ui_usb_vbus_error()
 To notify that a Vbus error has occurred. More...
 
#define UHC_CONNECTION_EVENT(dev, b_present)   ui_usb_connection_event(dev, b_present)
 To notify that a device has been connected or disconnected. More...
 
#define UHC_WAKEUP_EVENT()   ui_usb_wakeup_event()
 Called when a USB device or the host have wake up the USB line. More...
 
#define UHC_SOF_EVENT()   ui_usb_sof_event()
 Called for each received SOF each 1 ms. More...
 
#define UHC_ENUM_EVENT(dev, b_status)   ui_usb_enum_event(dev, b_status)
 Called when a USB device configuration must be chosen Thus, the application can choose either a configuration number for this device or a configuration number 0 to reject it. More...
 
#define UHI_AOA_CHANGE(dev, b_plug)   ui_uhi_aoa_change(dev, b_plug)
 USB Interface Configuration. More...
 

#define UHC_CONNECTION_EVENT (   dev,
  b_present 
)    ui_usb_connection_event(dev, b_present)

To notify that a device has been connected or disconnected.

Referenced by uhc_connection_tree().

#define UHC_ENUM_EVENT (   dev,
  b_status 
)    ui_usb_enum_event(dev, b_status)

Called when a USB device configuration must be chosen Thus, the application can choose either a configuration number for this device or a configuration number 0 to reject it.

If callback not defined the configuration 1 is chosen Called when a USB device enumeration is completed

Referenced by uhc_enumeration_error(), uhc_enumeration_step13(), uhc_enumeration_step14(), and uhc_enumeration_step15().

#define UHC_MODE_CHANGE (   b_host_mode)    ui_usb_mode_change(b_host_mode)

Authorize the USB HUB support.

USB Host callbacksTo notify that the USB mode are switched automatically This is possible only when ID pin is available

Referenced by ISR(), and otg_dual_enable().

#define UHC_SOF_EVENT ( )    ui_usb_sof_event()

Called for each received SOF each 1 ms.

Note: Available in High and Full speed mode

Referenced by uhd_sof_interrupt().

#define UHC_VBUS_CHANGE (   b_present)    ui_usb_vbus_change(b_present)

To notify that the Vbus level has changed.

Available only in USB hardware with Vbus monitoring

Referenced by uhd_interrupt().

#define UHC_VBUS_ERROR ( )    ui_usb_vbus_error()

To notify that a Vbus error has occurred.

Available only in USB hardware with Vbus monitoring

Referenced by uhd_interrupt().

#define UHC_WAKEUP_EVENT ( )    ui_usb_wakeup_event()

Called when a USB device or the host have wake up the USB line.

Referenced by uhc_notify_resume().

#define UHI_AOA_CHANGE (   dev,
  b_plug 
)    ui_uhi_aoa_change(dev, b_plug)

USB Interface Configuration.

Configuration of AOA Interface

Referenced by uhi_aoa_enable_success(), and uhi_aoa_uninstall().

#define USB_HOST_POWER_MAX   500

Maximum current allowed on Vbus (mA)

Referenced by uhc_enumeration_step13().

#define USB_HOST_UHI   UHI_AOA

USB Host Configuration.

Array of UHI APIs Define the list of UHI supported by USB host