Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
USB Device Interface (UDI) for Human Interface Device (HID) Mouse Class

Common APIs used by high level application to use this USB class.

See Quick start guide for USB device mouse module (UDI mouse).

Modules

 Interface with USB Device Core (UDC)
 Structures and functions required by UDC.
 
 Implementation of UDI HID Mouse
 Class internal implementation.
 
 USB device descriptors for a single interface
 The following structures provide the USB device descriptors required for USB Device with a single interface HID mouse.
 
 USB interface descriptors
 The following structures provide predefined USB interface descriptors.
 

Interfaces for mouse events

bool udi_hid_mouse_moveScroll (int8_t pos)
 Move the scroll wheel. More...
 
bool udi_hid_mouse_moveY (int8_t pos_y)
 Move the mouse pointer on Y axe. More...
 
bool udi_hid_mouse_moveX (int8_t pos_x)
 Move the mouse pointer on X axe. More...
 

Interfaces for buttons events

bool udi_hid_mouse_btnmiddle (bool b_state)
 Changes middle button state. More...
 
bool udi_hid_mouse_btnright (bool b_state)
 Changes right button state. More...
 
bool udi_hid_mouse_btnleft (bool b_state)
 Changes left button state. More...
 
#define HID_MOUSE_BTN_DOWN   true
 Value to signal a button down (pressed) More...
 
#define HID_MOUSE_BTN_UP   false
 Value to signal a button up (released) More...
 

#define HID_MOUSE_BTN_DOWN   true

Value to signal a button down (pressed)

Referenced by udi_hid_mouse_btn().

#define HID_MOUSE_BTN_UP   false

Value to signal a button up (released)

bool udi_hid_mouse_btnleft ( bool  b_state)

Changes left button state.

Parameters
b_stateNew button state
Returns
1 if function was successfully done, otherwise 0.

References udi_hid_mouse_btn().

bool udi_hid_mouse_btnmiddle ( bool  b_state)

Changes middle button state.

Parameters
b_stateNew button state
Returns
1 if function was successfully done, otherwise 0.

References udi_hid_mouse_btn().

bool udi_hid_mouse_btnright ( bool  b_state)

Changes right button state.

Parameters
b_stateNew button state
Returns
1 if function was successfully done, otherwise 0.

References udi_hid_mouse_btn().

bool udi_hid_mouse_moveScroll ( int8_t  pos)

Move the scroll wheel.

Parameters
posSigned value to move
Returns
1 if function was successfully done, otherwise 0.

References udi_hid_mouse_move().

bool udi_hid_mouse_moveX ( int8_t  pos_x)

Move the mouse pointer on X axe.

Parameters
pos_xSigned value to move
Returns
1 if function was successfully done, otherwise 0.

References udi_hid_mouse_move().

bool udi_hid_mouse_moveY ( int8_t  pos_y)

Move the mouse pointer on Y axe.

Parameters
pos_ySigned value to move
Returns
1 if function was successfully done, otherwise 0.

References udi_hid_mouse_move().

Referenced by ui_process().