Human interface on SAM4S-EK:
Introduction
This example shows how to implement a USB Device HID Multi-touch on Atmel MCU with USB module.
Startup
The example uses the buttons or sensors available on the board to simulate a standard multi-touch. After loading firmware, connect the board (EVKxx,Xplain,...) to the USB Host. When connected to a USB host system this application provides a HID multi-touch with two points application in the Windows 7 operating systems. This example uses the native HID driver for these operating systems.
- Led 0 (D2) blinks when USB host has checked and enabled HID generic interface
- Push button 0 (SW0) is used to draw line in paint application on Windows O.S
- Run the application and connect usb to he PC first.
- Open paint and push button 0 continuously, then two lines painted.
About example
The example uses the following module groups:
- Basic modules: Startup, board, clock, interrupt, power management
- USB Device stack and HID modules:
services/usb/
services/usb/udc/
services/usb/class/hid/
services/usb/class/hid/mtouch/
- Specific implementation:
- main.c,
initializes clock
initializes interrupt
manages UI
- specific implementation for each target "./examples/product_board/":
- conf_foo.h configuration of each module
- ui.c implement of user's interface (buttons, leds)