User Interface.
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_multitouch_down (void) |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void | ui_wakeup_disable (void) |
Disables the asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enables the asynchronous interrupts of the user interface. More... | |
Variables | |
static uint8_t | ui_hid_report [UDI_HID_REPORT_IN_SIZE] = {0} |
static uint8_t | ui_step = 0 |
void ui_init | ( | void | ) |
Initializes the user interface.
References LED0_GPIO, LED_On, and pmc_enable_periph_clk().
Referenced by main().
void ui_multitouch_down | ( | void | ) |
References udi_hid_multi_touch_send_report_in(), UDI_HID_REPORT_ID_MTOUCH, ui_hid_report, and ui_step.
Referenced by ui_process().
void ui_powerdown | ( | void | ) |
Enters the user interface in power down mode.
References LED0_GPIO, and LED_Off.
Referenced by main(), and main_suspend_action().
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
References gpio_pin_is_high, GPIO_PUSH_BUTTON_0, LED0_GPIO, LED_Off, LED_On, ui_multitouch_down(), and ui_step.
Referenced by main(), and main_sof_action().
void ui_wakeup | ( | void | ) |
Exits the user interface of power down mode.
References LED0_GPIO, and LED_On.
Referenced by main_resume_action().
void ui_wakeup_disable | ( | void | ) |
Disables the asynchronous interrupts of the user interface.
Referenced by main_remotewakeup_disable().
void ui_wakeup_enable | ( | void | ) |
Enables the asynchronous interrupts of the user interface.
Referenced by main_remotewakeup_enable().
|
static |
Referenced by ui_multitouch_down().
|
static |
Referenced by ui_multitouch_down(), and ui_process().