Microchip® Advanced Software Framework

main.h File Reference

Declaration of main function used by HID multi-touch example.

Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.

Functions

void main_multitouch_disable (void)
 Called by HID interface Callback running when USB Host disable multi-touch interface. More...
 
bool main_multitouch_enable (void)
 Called by HID interface Callback running when USB Host enable multi-touch interface. More...
 
void main_remotewakeup_disable (void)
 Called by UDC when USB Host request to disable remote wakeup. More...
 
void main_remotewakeup_enable (void)
 Called by UDC when USB Host request to enable remote wakeup. More...
 
void main_resume_action (void)
 Called by UDD when the USB line exit of suspend state. More...
 
void main_sof_action (void)
 Called when a start of frame is received on USB line. More...
 
void main_suspend_action (void)
 Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More...
 

void main_multitouch_disable ( void  )

Called by HID interface Callback running when USB Host disable multi-touch interface.

References main_b_mtouch_enable.

bool main_multitouch_enable ( void  )

Called by HID interface Callback running when USB Host enable multi-touch interface.

Return values
trueif multi-touch startup is ok

References main_b_mtouch_enable.

void main_remotewakeup_disable ( void  )

Called by UDC when USB Host request to disable remote wakeup.

References ui_wakeup_disable().

void main_remotewakeup_enable ( void  )

Called by UDC when USB Host request to enable remote wakeup.

References ui_wakeup_enable().

void main_resume_action ( void  )

Called by UDD when the USB line exit of suspend state.

References ui_wakeup().

void main_sof_action ( void  )

Called when a start of frame is received on USB line.

References main_b_mtouch_enable, udd_get_frame_number(), and ui_process().

void main_suspend_action ( void  )

Enters the application in low power mode Callback called when USB host sets USB line in suspend state.

References ui_powerdown().