This example will create a simple touch-enabled GUI on the display of the mXT143E Xplained, using the Widget Toolkit.
The widget library API can be found here, while the graphics service API can be found here. The maXTouch API can be found here.
This example has been tested with the mXT143E Xplained on the following kits:
On startup the example application will create a plot widget, a slider, and a button. Pressing the button will add the current slider value as a new plot point in the plot widget, and force a display refresh to plot the new value.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.