This module describes all MAC Confirmation Callback's.
|
void | usr_mcps_data_conf (uint8_t msduHandle, uint8_t status, uint32_t Timestamp) |
| Callback function that must be implemented by application (NHLE) for MAC service MCPS-DATA.confirm. More...
|
|
void | usr_mcps_purge_conf (uint8_t msduHandle, uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MCPS-PURGE.confirm. More...
|
|
void | usr_mlme_associate_conf (uint16_t AssocShortAddress, uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-ASSOCIATE.confirm. More...
|
|
void | usr_mlme_disassociate_conf (uint8_t status, wpan_addr_spec_t *DeviceAddrSpec) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.confirm. More...
|
|
void | usr_mlme_get_conf (uint8_t status, uint8_t PIBAttribute, void *PIBAttributeValue) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-GET.confirm. More...
|
|
void | usr_mlme_poll_conf (uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-POLL.confirm. More...
|
|
void | usr_mlme_reset_conf (uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-RESET.confirm. More...
|
|
void | usr_mlme_rx_enable_conf (uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-RX-ENABLE.confirm. More...
|
|
void | usr_mlme_scan_conf (uint8_t status, uint8_t ScanType, uint8_t ChannelPage, uint32_t UnscannedChannels, uint8_t ResultListSize, void *ResultList) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-SCAN.confirm. More...
|
|
void | usr_mlme_set_conf (uint8_t status, uint8_t PIBAttribute) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-SET.confirm. More...
|
|
void | usr_mlme_start_conf (uint8_t status) |
| Callback function that must be implemented by application (NHLE) for MAC service MLME-START.confirm. More...
|
|
void usr_mcps_data_conf |
( |
uint8_t |
msduHandle, |
|
|
uint8_t |
status, |
|
|
uint32_t |
Timestamp |
|
) |
| |
Callback function that must be implemented by application (NHLE) for MAC service MCPS-DATA.confirm.
- Parameters
-
msduHandle | Handle of MSDU handed over to MAC earlier. |
status | Result for requested data transmission request. |
Timestamp | The time, in symbols, at which the data were transmitted; this parameter is only available if timestamping is enabled via compile switch ENABLE_TSTAMP. |
- Returns
- void
References Dispaly_Result_Frame, EOT, get_next_tx_buffer(), LED_DATA, LED_Off, MAC_CHANNEL_ACCESS_FAILURE, MAC_NO_ACK, MAC_PID, MAC_PID_LEN, MAC_SUCCESS, MAC_TRANSACTION_EXPIRED, MAC_TRANSACTION_OVERFLOW, MCPS_DATA_CON_LEN, MCPS_DATA_CONFIRM, and status.
Referenced by mcps_data_conf().
void usr_mlme_set_conf |
( |
uint8_t |
status, |
|
|
uint8_t |
PIBAttribute |
|
) |
| |
Callback function that must be implemented by application (NHLE) for MAC service MLME-SET.confirm.
- Parameters
-
status | Result of requested PIB attribute set operation. |
PIBAttribute | Updated PIB attribute. |
PIBAttributeIndex | Index of updated PIB attribute. |
- Returns
- void
References wpan_addr_spec_tag::Addr, APP_IDLE, app_state, beacon_payload, BEACON_PAYLOAD_LEN, COORD_STARTING, coord_state, current_channel, current_channel_page, EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MAC_SUCCESS, macAssociationPermit, macBeaconPayload, macBeaconPayloadLength, macCoordShortAddress, macPANId, macRxOnWhenIdle, macShortAddress, MLME_SCAN_TYPE_ACTIVE, MLME_SET_CONF_LEN, MLME_SET_CONFIRM, SCAN_CHANNEL, SCAN_DURATION_COORDINATOR, status, wpan_mlme_reset_req(), wpan_mlme_scan_req(), wpan_mlme_set_req(), and wpan_mlme_sync_req().
Referenced by mlme_set_conf().