Includes Stack Definitions.
#define EXTRA_RTB_BUFFER (0) |
The following macros hold the size of a large buffer.
Additional octets for the length of the frame, the LQI and the ED value are required.
#define NUMBER_OF_RTB_TIMERS (0) |
#define NUMBER_OF_SMALL_STACK_BUFS (0) |
#define NUMBER_OF_TOTAL_STACK_TIMERS |
Value:
#define NUMBER_OF_RTB_TIMERS
Definition: wireless/avr2025_mac/include/stack_config.h:281
#define NUMBER_OF_TAL_TIMERS
Definition: atmel_rf4ce/lib/inc/tal_config.h:68
#define NUMBER_OF_MAC_TIMERS
Definition: wireless/avr2025_mac/source/mac/inc/mac_config.h:112