Honeywell HMC5883L 3-axis magnetometer.
This file contains functions for initializing and reading data from a Honeywell HMC5883L 3-axis magnetometer.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | angle_t |
struct | cal_data_t |
Sensor calibration data. More... | |
struct | hmc588l_axis_t |
HMC 5883l axis data format. More... | |
Macros | |
#define | CAL_OFFSETS_ADDR (0) |
#define | CAL_SENSITIVITY_ADDR (0 + sizeof(vector3_t)) |
#define | DATA_OUTPUT_OVERFLOW ((int16_t)0xf000) |
#define | READ_DELAY_MSEC (100) /* delay in msec between consecutive */ |
#define | SELF_TEST_DELAY_MSEC (250) /* delay in msec during self test */ |
Enumerations | |
enum | { index_90uT, index_130uT, index_190uT, index_250uT, index_400uT, index_470uT, index_560uT, index_810uT } |
enum | { index_1hz, index_2hz, index_3hz, index_8hz, index_15hz, index_30hz, index_75hz } |
Functions | |
static void | hmc5883l_apply_offset (vector3_t *input) |
Apply stored offset values to sensor reading. More... | |
static void | hmc5883l_apply_sensitivity (vector3_t *input) |
Apply stored sensitivity scaling factors to sensor reading. More... | |
static bool | hmc5883l_calibrate (sensor_t *sensor, sensor_calibration_t calib_type, int step, void *info) |
Calibrate magnetometer. More... | |
static bool | hmc5883l_device_id (sensor_hal_t *hal, sensor_data_t *data) |
Read magnetometer device ID. More... | |
static bool | hmc5883l_get_data (sensor_hal_t *hal, vector3_t *data) |
Read magnetometer vector data. More... | |
static bool | hmc5883l_get_field (sensor_hal_t *hal, sensor_data_t *data) |
Read magnetometer vector (3-axis) data. More... | |
static bool | hmc5883l_get_heading (sensor_hal_t *hal, sensor_data_t *data) |
Read magnetometer heading/direction data. More... | |
bool | hmc5883l_init (sensor_t *sensor, int resvd) |
Honeywell HMC5883L magnetometer driver initialization. More... | |
static bool | hmc5883l_ioctl (sensor_t *sensor, sensor_command_t cmd, void *arg) |
HMC5883L ioctl control entry point. More... | |
static bool | hmc5883l_read (sensor_t *sensor, sensor_read_t type, sensor_data_t *data) |
Read sensor data. More... | |
static bool | hmc5883l_selftest (sensor_t *sensor, int *test_code, void *arg) |
Perform self-test function. More... | |
static bool | hmc5883l_set_bandwidth (sensor_hal_t *hal, int16_t bw) |
Set the sample bandwidth for the magnetometer. More... | |
static bool | hmc5883l_set_range (sensor_hal_t *hal, int16_t range) |
Set the range for the magnetometer. More... | |
Variables | |
static const sensor_map_t | band_table [] |
Honeywell HMC5883L Bandwidth Table (hertz, register value) More... | |
static cal_data_t | cal_data |
static int | dev_range |
Current range index for device. More... | |
static const sensor_map_t | range_table [] |
Honeywell HMC5883L Range Table (microtesla, register value) More... | |
static const int | scale_table [] |
Honeywell HMC5883L Data Scaling Table (counts per milligauss) More... | |
#define CAL_OFFSETS_ADDR (0) |
Referenced by hmc5883l_calibrate().
#define CAL_SENSITIVITY_ADDR (0 + sizeof(vector3_t)) |
Referenced by hmc5883l_calibrate().
#define DATA_OUTPUT_OVERFLOW ((int16_t)0xf000) |
Referenced by hmc5883l_get_data().
#define READ_DELAY_MSEC (100) /* delay in msec between consecutive */ |
Referenced by hmc5883l_calibrate().
#define SELF_TEST_DELAY_MSEC (250) /* delay in msec during self test */ |
Referenced by hmc5883l_selftest().
anonymous enum |
|
static |
Apply stored offset values to sensor reading.
This function applies stored calibration offsets to the "input" vector of magnetometer values (the magnetic field vector) and returns the modified values. The offsets are calculated based on sensitivity-adjusted readings, so this function should be used after the values that have been adjusted using hmc5883l_apply_sensitivity().
input | Contains the measured magnetic field values, adjusted for sensitivity. The offset-adjusted values will replace the contents. |
true | successfully adjusted sensor readings |
false | Failed to adjust sensor readings |
References cal_data_t::offsets.
Referenced by hmc5883l_get_field(), and hmc5883l_get_heading().
|
static |
Apply stored sensitivity scaling factors to sensor reading.
This function applies stored sensitivity scaling to the "input" vector of magnetometer values (the magnetic field vector) and returns the modified values.
input | Contains the measured magnetic field values. The sensitivty-adjusted values will replace the contents. |
true | successfully adjusted sensor readings |
false | Failed to adjust sensor readings |
References cal_data_t::sensitivity.
Referenced by hmc5883l_calibrate(), hmc5883l_get_field(), and hmc5883l_get_heading().
|
static |
Calibrate magnetometer.
This function measures the magnetometer output if 3 different device orientations, calculates average offset values, and stores these offsets in non-volatile memory. The offsets will later be used during normal measurements, to compensate for fixed magnetic effects.
This routine must be called 3 times total, with the "step" parameter indicating what stage of the calibration is being performed. This multi-step mechanism allows the application to prompt for physical placement of the sensor device before this routine is called.
sensor | Address of an initialized sensor descriptor. |
data | The address of a vector storing sensor axis data. |
step | The calibration stage number (1 to 3). |
info | Unimplemented (ignored) parameter. |
References CAL_OFFSETS_ADDR, CAL_SENSITIVITY_ADDR, delay_ms, hmc5883l_apply_sensitivity(), hmc5883l_get_data(), hmc5883l_selftest(), HMC5883L_TEST_X_NORM, HMC5883L_TEST_Y_NORM, HMC5883L_TEST_Z_NORM, cal_data_t::offsets, READ_DELAY_MSEC, and cal_data_t::sensitivity.
Referenced by hmc5883l_init().
|
static |
Read magnetometer device ID.
This function reads the magnetometer hardware identification registers and returns these values to the addresses specified in the function parameters.
hal | Address of an initialized sensor hardware descriptor. |
data | Address of sensor_data_t structure to return values. |
References count, and HMC5883L_ID_REG_A.
Referenced by hmc5883l_init(), and hmc5883l_read().
|
static |
Read magnetometer vector data.
This function obtains magnetometer data for all three axes of the Honeywell device. The data is read from six device registers using a multi-byte bus transfer. The 13-bit raw results are then assembled from the two register values for each axis, including extending the sign bit, to form a signed 16-bit value.
hal | Address of an initialized sensor hardware descriptor. |
data | The address of a vector storing sensor axis data. |
References count, DATA_OUTPUT_OVERFLOW, gpio_pin_is_low, HMC5883L_MAG_X_HI, HMC5883L_MODE_REG, hmc588l_axis_t::lsb, MODE_SINGLE, and orient.
Referenced by hmc5883l_calibrate(), hmc5883l_get_field(), hmc5883l_get_heading(), and hmc5883l_selftest().
|
static |
Read magnetometer vector (3-axis) data.
This function obtains magnetometer data for all three axes of the Honeywell device. The data is read from six device registers using a multi-byte bus transfer. The 10-bit raw results are then assembled from the two register values for each axis, including extending the sign bit, to form a signed 32-bit value.
Along with the actual sensor data, the LSB byte contains a "new" flag indicating if the data for this axis has been updated since the last time the axis data was read. Reading either LSB or MSB data will clear this flag.
hal | Address of an initialized sensor device descriptor. |
data | The address of a vector storing sensor axis data. |
References dev_range, hmc5883l_apply_offset(), hmc5883l_apply_sensitivity(), hmc5883l_get_data(), and scale_table.
Referenced by hmc5883l_read().
|
static |
Read magnetometer heading/direction data.
This function obtains magnetometer data for all three axes of the Honeywell device. The data is read from six device registers using a multi-byte bus transfer. The 10-bit raw results are then assembled from the two register values for each axis, including extending the sign bit, to form a signed 32-bit value.
Along with the actual sensor data, the LSB byte contains a "new" flag indicating if the data for this axis has been updated since the last time the axis data was read. Reading either LSB or MSB data will clear this flag.
hal | Address of an initialized sensor device descriptor. |
data | The address of a vector storing sensor axis data. |
References dev_range, hmc5883l_apply_offset(), hmc5883l_apply_sensitivity(), hmc5883l_get_data(), and scale_table.
Referenced by hmc5883l_read().
bool hmc5883l_init | ( | sensor_t * | sensor, |
int | resvd | ||
) |
Honeywell HMC5883L magnetometer driver initialization.
This is the main initialization function for the HMC5883L device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
References band_table, data, DATA_RATE_15HZ, hmc5883l_calibrate(), HMC5883L_CONFIG_REG_A, HMC5883L_DATA_RESOLUTION, HMC5883L_DEV_ID, hmc5883l_device_id(), hmc5883l_ioctl(), HMC5883L_MODE_REG, hmc5883l_read(), hmc5883l_selftest(), hmc5883l_set_bandwidth(), hmc5883l_set_range(), index_130uT, index_15hz, MEAS_MODE_NORM, MODE_CONTIN, cal_data_t::offsets, range_table, status, and STATUS_OK.
|
static |
HMC5883L ioctl control entry point.
sensor | Address of an initialized sensor descriptor. |
cmd | Command to execute |
arg | Argument for command (varies) |
References hmc5883l_set_bandwidth(), hmc5883l_set_range(), and status.
Referenced by hmc5883l_init().
|
static |
Read sensor data.
This routine calls the appropriate internal data function to obtain the specified type of data from the sensor device.
sensor | Address of an initialized sensor device descriptor. |
type | Type of sensor data to read. |
data | The address where data values are returned. |
References hmc5883l_device_id(), hmc5883l_get_field(), and hmc5883l_get_heading().
Referenced by hmc5883l_init().
|
static |
Perform self-test function.
This function sets up and executes an built-in self test function within the HMC5883L device.
sensor | Address of an initialized sensor descriptor. |
test_code | Address of a numeric code of which test to perform This location will contain the specific test result code when the function returns. |
References count, data, DATA_RATE_15HZ, delay_ms, HMC5883L_CONFIG_REG_A, HMC5883L_CONFIG_REG_B, hmc5883l_get_data(), HMC5883L_MODE_REG, HMC5883L_TEST_GAIN, HMC5883L_TEST_X_MAX, HMC5883L_TEST_X_MIN, HMC5883L_TEST_Y_MAX, HMC5883L_TEST_Y_MIN, HMC5883L_TEST_Z_MAX, HMC5883L_TEST_Z_MIN, MEAS_AVG_1, MEAS_MODE_NEG, MEAS_MODE_POS, MODE_SINGLE, NULL, SELF_TEST_DELAY_MSEC, and status.
Referenced by hmc5883l_calibrate(), and hmc5883l_init().
|
static |
Set the sample bandwidth for the magnetometer.
hal | Address of an initialized sensor hardware descriptor. |
band | The index of a driver-specific bandwidth table entry. |
References band_table, DATA_RATE, and HMC5883L_CONFIG_REG_A.
Referenced by hmc5883l_init(), and hmc5883l_ioctl().
|
static |
Set the range for the magnetometer.
hal | Address of an initialized sensor hardware descriptor. |
range | The index of a driver-specific range table entry. |
References dev_range, HMC5883L_CONFIG_REG_B, and range_table.
Referenced by hmc5883l_init(), and hmc5883l_ioctl().
|
static |
Honeywell HMC5883L Bandwidth Table (hertz, register value)
Referenced by hmc5883l_init(), and hmc5883l_set_bandwidth().
|
static |
|
static |
Current range index for device.
Referenced by hmc5883l_get_field(), hmc5883l_get_heading(), and hmc5883l_set_range().
|
static |
Honeywell HMC5883L Range Table (microtesla, register value)
Referenced by hmc5883l_init(), and hmc5883l_set_range().
|
static |
Honeywell HMC5883L Data Scaling Table (counts per milligauss)
Referenced by hmc5883l_get_field(), and hmc5883l_get_heading().