These are application-specific resources which are used in the example application of the coordinator in addition to the underlaying stack.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include "nwk_config.h"
#include "rf4ce.h"
Macros | |
#define | NWKC_MAX_PAIRING_TABLE_ENTRIES (5) |
#define | NWKC_NODE_CAPABILITIES |
#define NWKC_MAX_PAIRING_TABLE_ENTRIES (5) |
#define NWKC_NODE_CAPABILITIES |