Microchip® Advanced Software Framework

COG_parameters_t Struct Reference

Define the COG driver's parameters.

#include <EPD_COG_process.h>

Data Fields

uint8_t channel_select [8]
 the SPI register data of Channel Select More...
 
uint8_t data_line_size
 Data + Scan + Dummy bytes. More...
 
uint16_t frame_time_offset
 the rest of frame time in a stage More...
 
uint16_t horizontal_size
 the bytes of width of EPD More...
 
uint16_t stage_time
 defined stage time More...
 
uint16_t vertical_size
 the bytes of height of EPD More...
 
uint8_t voltage_level
 the SPI register data of Voltage Level More...
 

uint8_t COG_parameters_t::channel_select[8]

the SPI register data of Channel Select

uint8_t COG_parameters_t::data_line_size

Data + Scan + Dummy bytes.

uint16_t COG_parameters_t::frame_time_offset

the rest of frame time in a stage

uint16_t COG_parameters_t::horizontal_size

the bytes of width of EPD

uint16_t COG_parameters_t::stage_time

defined stage time

uint16_t COG_parameters_t::vertical_size

the bytes of height of EPD

uint8_t COG_parameters_t::voltage_level

the SPI register data of Voltage Level