Elements of the NodeDesc type as defined by 094945r00ZB_RF4CE-Specification.pdf.
#include <rf4ce.h>
Data Fields | |
uint8_t | AppCapabilities |
The application capabilities of the responding node. More... | |
uint8_t | DevTypeList [3] |
The list of device types supported by the responding node. More... | |
uint8_t | DiscReqLQI |
The LQI of the discovery request command frame reported by the responding device. More... | |
uint64_t | IEEEAddr |
The IEEE address of the responding device. More... | |
uint8_t | LogicalChannel |
The logical channel of the responding device. More... | |
uint8_t | NodeCapabilities |
The capabilities of the responding node. More... | |
uint16_t | PANId |
The PAN identifier of the responding device. More... | |
uint8_t | ProfileIdList [7] |
The list of profile identifiers supported by the responding node. More... | |
nwk_enum_t | Status |
The status of the discovery request as reported by the responding device. More... | |
uint8_t | UserString [15] |
The user defined identification string of the responding node. More... | |
uint16_t | VendorId |
The vendor identifier of the responding node. More... | |
uint8_t | VendorString [7] |
The vendor string of the responding node. More... | |
uint8_t NodeDesc_tag::AppCapabilities |
The application capabilities of the responding node.
Referenced by nlme_discovery_confirm().
uint8_t NodeDesc_tag::DevTypeList |
The list of device types supported by the responding node.
Referenced by nlme_discovery_confirm().
uint8_t NodeDesc_tag::DiscReqLQI |
The LQI of the discovery request command frame reported by the responding device.
Referenced by nlme_discovery_confirm().
uint64_t NodeDesc_tag::IEEEAddr |
The IEEE address of the responding device.
uint8_t NodeDesc_tag::LogicalChannel |
The logical channel of the responding device.
Referenced by nlme_discovery_confirm().
uint8_t NodeDesc_tag::NodeCapabilities |
The capabilities of the responding node.
Referenced by nlme_discovery_confirm().
uint16_t NodeDesc_tag::PANId |
The PAN identifier of the responding device.
uint8_t NodeDesc_tag::ProfileIdList |
The list of profile identifiers supported by the responding node.
Referenced by nlme_discovery_confirm().
nwk_enum_t NodeDesc_tag::Status |
The status of the discovery request as reported by the responding device.
NWK_SUCCESS or NO_REC_CAPACITY
Referenced by nlme_discovery_confirm().
uint8_t NodeDesc_tag::UserString |
The user defined identification string of the responding node.
This field is present only if the user string specified subfield of the AppCapabilities field is set to one.
Referenced by nlme_discovery_confirm().
uint16_t NodeDesc_tag::VendorId |
The vendor identifier of the responding node.
uint8_t NodeDesc_tag::VendorString |
The vendor string of the responding node.
Referenced by nlme_discovery_confirm().