Structure implementing the pairing table entry as defined by 094945r00ZB_RF4CE-Specification.pdf.
#include <rf4ce.h>
Data Fields | |
uint64_t | DestinationIEEEaddress |
The IEEE address of the destination device. More... | |
uint8_t | DestinationLogicalChannel |
The expected channel of the destination device. More... | |
uint16_t | DestinationNetworkAddress |
The network address of the destination device. More... | |
uint16_t | DestinationPANidentifier |
The PAN identifier of the destination device. More... | |
uint8_t | RecipientCapabilities |
The node capabilities of the recipient node. More... | |
uint32_t | RecipientFrameCounter |
The frame counter last received from the recipient node. More... | |
uint8_t | SecurityLinkKey [16] |
The link key to be used to secure this pairing link. More... | |
uint16_t | SourceNetworkAddress |
The network address to be assumed by the source device. More... | |
uint64_t pairing_table_tag::DestinationIEEEaddress |
The IEEE address of the destination device.
Referenced by print_pairing_table().
uint8_t pairing_table_tag::DestinationLogicalChannel |
The expected channel of the destination device.
Referenced by print_pairing_table().
uint16_t pairing_table_tag::DestinationNetworkAddress |
The network address of the destination device.
Referenced by print_pairing_table().
uint16_t pairing_table_tag::DestinationPANidentifier |
The PAN identifier of the destination device.
Referenced by print_pairing_table().
uint8_t pairing_table_tag::RecipientCapabilities |
The node capabilities of the recipient node.
Referenced by print_pairing_table().
uint32_t pairing_table_tag::RecipientFrameCounter |
The frame counter last received from the recipient node.
Referenced by print_pairing_table().
uint8_t pairing_table_tag::SecurityLinkKey |
The link key to be used to secure this pairing link.
Referenced by print_pairing_table().
uint16_t pairing_table_tag::SourceNetworkAddress |
The network address to be assumed by the source device.
Referenced by print_pairing_table().