See Quickstart guide for SAM CAN module..
The CAN controller provides all the features required to implement the serial communication protocol CAN defined by Robert Bosch GmbH, the CAN specification. This is a driver for configuration, enabling, disabling and use of the CAN peripheral.
Functions | |
void | can_disable (Can *p_can) |
Disable CAN Controller. More... | |
void | can_disable_autobaud_listen_mode (Can *p_can) |
Disable CAN Controller autobaud/listen mode. More... | |
void | can_disable_interrupt (Can *p_can, uint32_t dw_mask) |
Disable CAN interrupt. More... | |
void | can_disable_low_power_mode (Can *p_can) |
Disable CAN Controller low power mode. More... | |
void | can_disable_overload_frame (Can *p_can) |
CAN Controller won't generate overload frame. More... | |
void | can_disable_time_triggered_mode (Can *p_can) |
Disable CAN Controller time triggered mode. More... | |
void | can_disable_timer_freeze (Can *p_can) |
Disable CAN Controller timer freeze. More... | |
void | can_disable_tx_repeat (Can *p_can) |
Disable CAN Controller transmit repeat function. More... | |
void | can_enable (Can *p_can) |
Enable CAN Controller. More... | |
void | can_enable_autobaud_listen_mode (Can *p_can) |
Enable CAN Controller autobaud/listen mode. More... | |
void | can_enable_interrupt (Can *p_can, uint32_t dw_mask) |
Enable CAN interrupt. More... | |
void | can_enable_low_power_mode (Can *p_can) |
Enable CAN Controller low power mode. More... | |
void | can_enable_overload_frame (Can *p_can) |
CAN Controller will generate an overload frame after each successful reception for mailboxes configured in Receive mode, Producer and Consumer. More... | |
void | can_enable_time_triggered_mode (Can *p_can) |
Enable CAN Controller time triggered mode. More... | |
void | can_enable_timer_freeze (Can *p_can) |
Enable CAN Controller timer freeze. More... | |
void | can_enable_tx_repeat (Can *p_can) |
Enable CAN Controller transmit repeat function. More... | |
uint32_t | can_get_internal_timer_value (Can *p_can) |
Get the 16-bit free-running internal timer count. More... | |
uint32_t | can_get_interrupt_mask (Can *p_can) |
Get CAN Interrupt Mask. More... | |
uint8_t | can_get_rx_error_cnt (Can *p_can) |
Get CAN receive error counter. More... | |
uint32_t | can_get_status (Can *p_can) |
Get CAN status. More... | |
uint32_t | can_get_timestamp_value (Can *p_can) |
Get CAN timestamp register value. More... | |
uint8_t | can_get_tx_error_cnt (Can *p_can) |
Get CAN transmit error counter. More... | |
void | can_global_send_abort_cmd (Can *p_can, uint8_t uc_mask) |
Send global abort request. More... | |
void | can_global_send_transfer_cmd (Can *p_can, uint8_t uc_mask) |
Send global transfer request. More... | |
uint32_t | can_init (Can *p_can, uint32_t ul_mck, uint32_t ul_baudrate) |
Initialize CAN controller. More... | |
uint32_t | can_mailbox_get_status (Can *p_can, uint8_t uc_index) |
Get status of the mailbox. More... | |
void | can_mailbox_init (Can *p_can, can_mb_conf_t *p_mailbox) |
Initialize the mailbox in different mode and set up related configuration. More... | |
uint32_t | can_mailbox_read (Can *p_can, can_mb_conf_t *p_mailbox) |
Read receive information for the mailbox. More... | |
void | can_mailbox_send_abort_cmd (Can *p_can, can_mb_conf_t *p_mailbox) |
Send single mailbox abort request. More... | |
void | can_mailbox_send_transfer_cmd (Can *p_can, can_mb_conf_t *p_mailbox) |
Send single mailbox transfer request. More... | |
void | can_mailbox_set_timemark (Can *p_can, uint8_t uc_index, uint16_t us_cnt) |
Configure the timemark for the mailbox. More... | |
uint32_t | can_mailbox_tx_remote_frame (Can *p_can, can_mb_conf_t *p_mailbox) |
Require to send out a remote frame. More... | |
uint32_t | can_mailbox_write (Can *p_can, can_mb_conf_t *p_mailbox) |
Prepare transmit information and write them into the mailbox. More... | |
void | can_reset_all_mailbox (Can *p_can) |
Reset the eight mailboxes. More... | |
void | can_reset_internal_timer (Can *p_can) |
Reset the internal free-running 16-bit timer. More... | |
void | can_set_rx_sync_stage (Can *p_can, uint32_t ul_stage) |
void | can_set_timestamp_capture_point (Can *p_can, uint32_t ul_flag) |
Configure the timestamp capture point, at the start or the end of frame. More... | |
void can_disable | ( | Can * | p_can | ) |
Disable CAN Controller.
p_can | Pointer to a CAN peripheral instance. |
Referenced by can_set_baudrate(), and run_can_test().
void can_disable_autobaud_listen_mode | ( | Can * | p_can | ) |
Disable CAN Controller autobaud/listen mode.
p_can | Pointer to a CAN peripheral instance. |
void can_disable_interrupt | ( | Can * | p_can, |
uint32_t | dw_mask | ||
) |
Disable CAN interrupt.
p_can | Pointer to a CAN peripheral instance. |
dw_mask | Interrupt to be disabled. |
Referenced by run_can_test().
void can_disable_low_power_mode | ( | Can * | p_can | ) |
Disable CAN Controller low power mode.
p_can | Pointer to a CAN peripheral instance. |
void can_disable_overload_frame | ( | Can * | p_can | ) |
CAN Controller won't generate overload frame.
p_can | Pointer to a CAN peripheral instance. |
void can_disable_time_triggered_mode | ( | Can * | p_can | ) |
Disable CAN Controller time triggered mode.
p_can | Pointer to a CAN peripheral instance. |
void can_disable_timer_freeze | ( | Can * | p_can | ) |
Disable CAN Controller timer freeze.
p_can | Pointer to a CAN peripheral instance. |
void can_disable_tx_repeat | ( | Can * | p_can | ) |
Disable CAN Controller transmit repeat function.
p_can | Pointer to a CAN peripheral instance. |
void can_enable | ( | Can * | p_can | ) |
Enable CAN Controller.
p_can | Pointer to a CAN peripheral instance. |
Referenced by can_init().
void can_enable_autobaud_listen_mode | ( | Can * | p_can | ) |
Enable CAN Controller autobaud/listen mode.
p_can | Pointer to a CAN peripheral instance. |
void can_enable_interrupt | ( | Can * | p_can, |
uint32_t | dw_mask | ||
) |
Enable CAN interrupt.
p_can | Pointer to a CAN peripheral instance. |
dw_mask | Interrupt to be enabled. |
Referenced by run_can_test().
void can_enable_low_power_mode | ( | Can * | p_can | ) |
Enable CAN Controller low power mode.
p_can | Pointer to a CAN peripheral instance. |
void can_enable_overload_frame | ( | Can * | p_can | ) |
CAN Controller will generate an overload frame after each successful reception for mailboxes configured in Receive mode, Producer and Consumer.
p_can | Pointer to a CAN peripheral instance. |
void can_enable_time_triggered_mode | ( | Can * | p_can | ) |
Enable CAN Controller time triggered mode.
p_can | Pointer to a CAN peripheral instance. |
void can_enable_timer_freeze | ( | Can * | p_can | ) |
Enable CAN Controller timer freeze.
p_can | Pointer to a CAN peripheral instance. |
void can_enable_tx_repeat | ( | Can * | p_can | ) |
Enable CAN Controller transmit repeat function.
p_can | Pointer to a CAN peripheral instance. |
uint32_t can_get_internal_timer_value | ( | Can * | p_can | ) |
Get the 16-bit free-running internal timer count.
p_can | Pointer to a CAN peripheral instance. |
The | internal CAN free-running timer counter. |
uint32_t can_get_interrupt_mask | ( | Can * | p_can | ) |
Get CAN Interrupt Mask.
p_can | Pointer to a CAN peripheral instance. |
CAN | interrupt mask. |
uint8_t can_get_rx_error_cnt | ( | Can * | p_can | ) |
Get CAN receive error counter.
p_can | Pointer to a CAN peripheral instance. |
Receive | error counter. |
uint32_t can_get_status | ( | Can * | p_can | ) |
Get CAN status.
p_can | Pointer to a CAN peripheral instance. |
CAN | status. |
Referenced by CAN0_Handler(), and can_init().
uint32_t can_get_timestamp_value | ( | Can * | p_can | ) |
Get CAN timestamp register value.
p_can | Pointer to a CAN peripheral instance. |
The | timestamp value. |
uint8_t can_get_tx_error_cnt | ( | Can * | p_can | ) |
Get CAN transmit error counter.
p_can | Pointer to a CAN peripheral instance. |
Transmit | error counter. |
void can_global_send_abort_cmd | ( | Can * | p_can, |
uint8_t | uc_mask | ||
) |
Send global abort request.
p_can | Pointer to a CAN peripheral instance. |
uc_mask | Mask for mailboxes that are requested to abort. |
References GLOBAL_MAILBOX_MASK.
void can_global_send_transfer_cmd | ( | Can * | p_can, |
uint8_t | uc_mask | ||
) |
Send global transfer request.
p_can | Pointer to a CAN peripheral instance. |
uc_mask | Mask for mailboxes that are requested to transfer. |
References GLOBAL_MAILBOX_MASK.
Referenced by can_mailbox_tx_remote_frame(), and run_can_test().
uint32_t can_init | ( | Can * | p_can, |
uint32_t | ul_mck, | ||
uint32_t | ul_baudrate | ||
) |
Initialize CAN controller.
p_can | Pointer to a CAN peripheral instance. |
ul_mck | CAN module input clock. |
ul_baudrate | CAN communication baudrate in kbs. |
0 | If failed to initialize the CAN module; otherwise successful. |
References can_enable(), can_get_status(), can_reset_all_mailbox(), can_set_baudrate(), and CAN_TIMEOUT.
Referenced by run_can_test().
uint32_t can_mailbox_get_status | ( | Can * | p_can, |
uint8_t | uc_index | ||
) |
Get status of the mailbox.
p_can | Pointer to a CAN peripheral instance. |
uc_index | Indicate which mailbox is to be read. |
The | mailbox status. |
Referenced by CAN0_Handler(), and can_mailbox_write().
void can_mailbox_init | ( | Can * | p_can, |
can_mb_conf_t * | p_mailbox | ||
) |
Initialize the mailbox in different mode and set up related configuration.
p_can | Pointer to a CAN peripheral instance. |
p_mailbox | Pointer to a CAN mailbox instance. |
References can_mb_conf_t::uc_id_ver, can_mb_conf_t::uc_obj_type, can_mb_conf_t::uc_tx_prio, can_mb_conf_t::ul_id, can_mb_conf_t::ul_id_msk, and can_mb_conf_t::ul_mb_idx.
Referenced by can_reset_all_mailbox(), and run_can_test().
uint32_t can_mailbox_read | ( | Can * | p_can, |
can_mb_conf_t * | p_mailbox | ||
) |
Read receive information for the mailbox.
p_can | Pointer to a CAN peripheral instance. |
p_mailbox | Pointer to a CAN mailbox instance. |
Different | CAN mailbox transfer status. |
References CAN_MAILBOX_RX_NEED_RD_AGAIN, CAN_MAILBOX_RX_OVER, can_mailbox_send_transfer_cmd(), CAN_MAILBOX_TRANSFER_OK, can_mb_conf_t::uc_length, can_mb_conf_t::ul_datah, can_mb_conf_t::ul_datal, can_mb_conf_t::ul_fid, can_mb_conf_t::ul_mb_idx, and can_mb_conf_t::ul_status.
Referenced by CAN0_Handler().
void can_mailbox_send_abort_cmd | ( | Can * | p_can, |
can_mb_conf_t * | p_mailbox | ||
) |
Send single mailbox abort request.
p_can | Pointer to a CAN peripheral instance. |
p_mailbox | Pointer to a CAN mailbox instance. |
References can_mb_conf_t::uc_length, and can_mb_conf_t::ul_mb_idx.
void can_mailbox_send_transfer_cmd | ( | Can * | p_can, |
can_mb_conf_t * | p_mailbox | ||
) |
Send single mailbox transfer request.
p_can | Pointer to a CAN peripheral instance. |
p_mailbox | Pointer to a CAN mailbox instance. |
References can_mb_conf_t::uc_length, and can_mb_conf_t::ul_mb_idx.
Referenced by can_mailbox_read().
void can_mailbox_set_timemark | ( | Can * | p_can, |
uint8_t | uc_index, | ||
uint16_t | us_cnt | ||
) |
Configure the timemark for the mailbox.
p_can | Pointer to a CAN peripheral instance. |
uc_index | Indicate which mailbox is to be configured. |
us_cnt | The timemark to be set. |
References TIMEMARK_MASK.
uint32_t can_mailbox_tx_remote_frame | ( | Can * | p_can, |
can_mb_conf_t * | p_mailbox | ||
) |
Require to send out a remote frame.
p_can | Pointer to a CAN peripheral instance. |
p_mailbox | Pointer to a CAN mailbox instance. |
CAN_MAILBOX_NOT_READY,: | Failed because mailbox isn't ready for transmitting message. CAN_MAILBOX_TRANSFER_OK: Successfully send out a remote frame. |
References can_global_send_transfer_cmd(), CAN_MAILBOX_NOT_READY, CAN_MAILBOX_TRANSFER_OK, can_mb_conf_t::uc_id_ver, can_mb_conf_t::uc_length, can_mb_conf_t::ul_id, can_mb_conf_t::ul_mb_idx, and can_mb_conf_t::ul_status.
Referenced by run_can_test().
uint32_t can_mailbox_write | ( | Can * | p_can, |
can_mb_conf_t * | p_mailbox | ||
) |
Prepare transmit information and write them into the mailbox.
p_can | Pointer to a CAN peripheral instance. |
p_mailbox | Pointer to a CAN mailbox instance. |
CAN_MAILBOX_NOT_READY,: | Failed because mailbox isn't ready. CAN_MAILBOX_TRANSFER_OK: Successfully write message into mailbox. |
References can_mailbox_get_status(), CAN_MAILBOX_NOT_READY, CAN_MAILBOX_TRANSFER_OK, can_mb_conf_t::uc_id_ver, can_mb_conf_t::uc_length, can_mb_conf_t::ul_datah, can_mb_conf_t::ul_datal, can_mb_conf_t::ul_id, can_mb_conf_t::ul_mb_idx, and can_mb_conf_t::ul_status.
Referenced by run_can_test().
void can_reset_all_mailbox | ( | Can * | p_can | ) |
Reset the eight mailboxes.
p_can | Pointer to a CAN peripheral instance. |
References can_mailbox_init(), CAN_MB_DISABLE_MODE, can_mb_conf_t::uc_obj_type, and can_mb_conf_t::ul_mb_idx.
Referenced by can_init(), and run_can_test().
void can_reset_internal_timer | ( | Can * | p_can | ) |
Reset the internal free-running 16-bit timer.
p_can | Pointer to a CAN peripheral instance. |
void can_set_rx_sync_stage | ( | Can * | p_can, |
uint32_t | ul_stage | ||
) |
void can_set_timestamp_capture_point | ( | Can * | p_can, |
uint32_t | ul_flag | ||
) |
Configure the timestamp capture point, at the start or the end of frame.
p_can | Pointer to a CAN peripheral instance. |
ul_flag | 0: Timestamp is captured at each start of frame; 1: Timestamp is captured at each end of frame. |