Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Generic Clock Management

Generic clocks are configurable clocks which run outside the system clock domain.

They are often connected to peripherals which have an asynchronous component running independently of the bus clock, e.g. USB controllers, low-power timers and RTCs, etc.

Note that not all platforms have support for generic clocks; on such platforms, this API will not be available.

Data Structures

struct  genclk_config
 Hardware representation of a set of generic clock parameters. More...
 

Enumerations

enum  genclk_source {
  GENCLK_SRC_RCSYS = 0,
  GENCLK_SRC_OSC32K = 1,
  GENCLK_SRC_DFLL = 2,
  GENCLK_SRC_OSC0 = 3,
  GENCLK_SRC_RC80M = 4,
  GENCLK_SRC_RCFAST = 5,
  GENCLK_SRC_RC1M = 6,
  GENCLK_SRC_CLK_CPU = 7,
  GENCLK_SRC_CLK_HSB = 8,
  GENCLK_SRC_CLK_PBA = 9,
  GENCLK_SRC_CLK_PBB = 10,
  GENCLK_SRC_CLK_PBC = 11,
  GENCLK_SRC_CLK_PBD = 12,
  GENCLK_SRC_RC32K = 13,
  GENCLK_SRC_CLK_1K = 15,
  GENCLK_SRC_PLL0 = 16,
  GENCLK_SRC_HRPCLK = 17,
  GENCLK_SRC_FPCLK = 18,
  GENCLK_SRC_GCLKIN0 = 19,
  GENCLK_SRC_GCLKIN1 = 20,
  GENCLK_SRC_GCLK11 = 21
}
 Generic clock source ID. More...
 

Functions

static void genclk_config_defaults (struct genclk_config *cfg, uint32_t id)
 
static void genclk_config_read (struct genclk_config *cfg, uint32_t id)
 
static void genclk_config_set_divider (struct genclk_config *cfg, uint32_t divider)
 
static void genclk_config_write (const struct genclk_config *cfg, uint32_t id)
 
static void genclk_disable (uint32_t id)
 
static void genclk_enable (const struct genclk_config *cfg, uint32_t id)
 
static void genclk_enable_config (unsigned int id, enum genclk_source src, unsigned int divider)
 Enable the configuration defined by src and divider for the generic clock identified by id. More...
 

Generic clock configuration

static void genclk_config_set_source (struct genclk_config *cfg, enum genclk_source src)
 Select a new source clock src in configuration cfg. More...
 
static void genclk_enable_source (enum genclk_source src)
 Enable the source clock src used by a generic clock. More...
 

Chip-specific generic clock definitions

#define GENCLK_DIV_MAX   256
 Maximum divider supported by the generic clock implementation. More...
 

#define GENCLK_DIV_MAX   256

Maximum divider supported by the generic clock implementation.

Referenced by genclk_config_set_divider().

Generic clock source ID.

Each generic clock may be generated from a different clock source. These are the available alternatives provided by the chip.

Enumerator
GENCLK_SRC_RCSYS 

System RC oscillator.

GENCLK_SRC_OSC32K 

32 kHz oscillator

GENCLK_SRC_DFLL 

DFLL.

GENCLK_SRC_OSC0 

Oscillator 0.

GENCLK_SRC_RC80M 

80 MHz RC oscillator

GENCLK_SRC_RCFAST 

4-8-12 MHz RC oscillator

GENCLK_SRC_RC1M 

1 MHz RC oscillator

GENCLK_SRC_CLK_CPU 

CPU clock.

GENCLK_SRC_CLK_HSB 

High Speed Bus clock.

GENCLK_SRC_CLK_PBA 

Peripheral Bus A clock.

GENCLK_SRC_CLK_PBB 

Peripheral Bus B clock.

GENCLK_SRC_CLK_PBC 

Peripheral Bus C clock.

GENCLK_SRC_CLK_PBD 

Peripheral Bus D clock.

GENCLK_SRC_RC32K 

32 kHz RC oscillator

GENCLK_SRC_CLK_1K 

1 kHz output from OSC32K

GENCLK_SRC_PLL0 

PLL0.

GENCLK_SRC_HRPCLK 

High resolution prescaler.

GENCLK_SRC_FPCLK 

Fractional prescaler.

GENCLK_SRC_GCLKIN0 

GCLKIN0.

GENCLK_SRC_GCLKIN1 

GCLKIN1.

GENCLK_SRC_GCLK11 

GCLK11.

static void genclk_config_defaults ( struct genclk_config cfg,
uint32_t  id 
)
inlinestatic
static void genclk_config_read ( struct genclk_config cfg,
uint32_t  id 
)
inlinestatic

References genclk_config::ctrl.

static void genclk_config_set_divider ( struct genclk_config cfg,
uint32_t  divider 
)
inlinestatic
void genclk_config_set_source ( struct genclk_config cfg,
enum genclk_source  src 
)
inlinestatic

Select a new source clock src in configuration cfg.

References genclk_config::ctrl.

Referenced by genclk_enable_config(), and run_iis_test().

static void genclk_config_write ( const struct genclk_config cfg,
uint32_t  id 
)
inlinestatic

References genclk_config::ctrl.

static void genclk_disable ( uint32_t  id)
inlinestatic
static void genclk_enable ( const struct genclk_config cfg,
uint32_t  id 
)
inlinestatic
static void genclk_enable_config ( unsigned int  id,
enum genclk_source  src,
unsigned int  divider 
)
inlinestatic

Enable the configuration defined by src and divider for the generic clock identified by id.

Parameters
idThe ID of the generic clock.
srcThe source clock of the generic clock.
dividerThe divider used to generate the generic clock.

References genclk_config_defaults(), genclk_config_set_divider(), genclk_config_set_source(), genclk_enable(), and genclk_enable_source().

Referenced by sysclk_enable_usb().