Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
PLL Management

This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs.

A PLL will take an input signal (the source), optionally divide the frequency by a configurable divider, and then multiply the frequency by a configurable multiplier.

Some devices don't support input dividers; specifying any other divisor than 1 on these devices will result in an assertion failure. Other devices may have various restrictions to the frequency range of the input and output signals.

Example: Setting up PLL0 with default parameters

The following example shows how to configure and enable PLL0 using the default parameters specified using the configuration symbols listed above.

To configure, enable PLL0 using the default parameters and to disable a specific feature like Wide Bandwidth Mode (a UC3A3-specific PLL option.), you can use this initialization process.

struct pll_config pllcfg;
if (pll_is_locked(pll_id)) {
return; // Pll already running
}
pll_config_defaults(&pllcfg, 0);
pll_enable(&pllcfg, 0);

When the last function call returns, PLL0 is ready to be used as the main system clock source.

Configuration Symbols

Each PLL has a set of default parameters determined by the following configuration symbols in the application's configuration file:

These configuration symbols determine the result of calling pll_config_defaults() and pll_get_default_rate().

Data Structures

struct  pll_config
 Hardware-specific representation of PLL configuration. More...
 

Macros

#define PLL_TIMEOUT_MS   div_ceil(1000 * (PLL_MAX_STARTUP_CYCLES * 2), OSC_RCSYS_MIN_HZ)
 Number of milliseconds to wait for PLL lock. More...
 

Enumerations

enum  pll_source {
  PLL_SRC_OSC0 = 0,
  PLL_SRC_GCLK9 = 1,
  PLL_NR_SOURCES
}
 PLL clock source. More...
 

Functions

static void pll_config_clear_option (struct pll_config *cfg, uint32_t option)
 
static void pll_config_init (struct pll_config *cfg, enum pll_source src, uint32_t divide, uint32_t mul)
 The PLL options PLL_OPT_VCO_RANGE_HIGH and PLL_OPT_OUTPUT_DIV will be set automatically based on the calculated target frequency. More...
 
static void pll_config_read (struct pll_config *cfg, uint32_t pll_id)
 
static void pll_config_set_option (struct pll_config *cfg, uint32_t option)
 
void pll_config_write (const struct pll_config *cfg, uint32_t pll_id)
 
void pll_disable (uint32_t pll_id)
 
void pll_enable (const struct pll_config *cfg, uint32_t pll_id)
 
static void pll_enable_config_defaults (uint32_t pll_id)
 
static bool pll_is_locked (uint32_t pll_id)
 

Chip-specific PLL characteristics

#define PLL_MAX_STARTUP_CYCLES   (SCIF_PLL_PLLCOUNT_Msk >> SCIF_PLL_PLLCOUNT_Pos)
 Maximum PLL startup time in number of slow clock cycles. More...
 
#define NR_PLLS   1
 Number of on-chip PLLs. More...
 
#define PLL_MIN_HZ   40000000
 Minimum frequency that the PLL can generate. More...
 
#define PLL_MAX_HZ   240000000
 Maximum frequency that the PLL can generate. More...
 

PLL configuration

#define pll_config_defaults(cfg, pll_id)
 Initialize PLL configuration using default parameters. More...
 
#define pll_get_default_rate(pll_id)
 Get the default rate in Hz of pll_id. More...
 

Interaction with the PLL hardware

static int pll_wait_for_lock (unsigned int pll_id)
 Wait for PLL pll_id to become locked. More...
 
static void pll_enable_source (enum pll_source src)
 Enable the source of the pll. More...
 

Chip-specific PLL options

#define PLL_NR_OPTIONS   3
 Number of PLL option bits. More...
 
#define PLL_OPT_VCO_RANGE_HIGH   0
 VCO frequency range is 160-240 MHz (80-180 MHz if unset). More...
 
#define PLL_OPT_OUTPUT_DIV   1
 Divide output frequency by two. More...
 
#define PLL_OPT_WBM_DISABLE   2
 Disable wide-bandwidth mode. More...
 
#define PLL_VCO_LOW_THRESHOLD
 The threshold above which to set the PLL_OPT_VCO_RANGE_HIGH option. More...
 

#define NR_PLLS   1
#define pll_config_defaults (   cfg,
  pll_id 
)
Value:
CONFIG_PLL ## pll_id ## _SOURCE, \
CONFIG_PLL ## pll_id ## _DIV, \
CONFIG_PLL ## pll_id ## _MUL)
static void pll_config_init(struct pll_config *cfg, enum pll_source src, uint32_t divide, uint32_t mul)
The PLL options PLL_OPT_VCO_RANGE_HIGH and PLL_OPT_OUTPUT_DIV will be set automatically based on the ...
Definition: sam4l/pll.h:124

Initialize PLL configuration using default parameters.

After this function returns, cfg will contain a configuration which will make the PLL run at (CONFIG_PLLx_MUL / CONFIG_PLLx_DIV) times the frequency of CONFIG_PLLx_SOURCE.

Parameters
cfgThe PLL configuration to be initialized.
pll_idUse defaults for this PLL.
#define pll_get_default_rate (   pll_id)
Value:
((osc_get_rate(CONFIG_PLL ## pll_id ## _SOURCE) \
* CONFIG_PLL ## pll_id ## _MUL) \
/ CONFIG_PLL ## pll_id ## _DIV)
static uint32_t osc_get_rate(uint8_t id)
Return the frequency of oscillator id in Hz.
Definition: sam4l/osc.h:447

Get the default rate in Hz of pll_id.

Referenced by sysclk_get_main_hz().

#define PLL_MAX_HZ   240000000

Maximum frequency that the PLL can generate.

Referenced by pll_config_init().

#define PLL_MAX_STARTUP_CYCLES   (SCIF_PLL_PLLCOUNT_Msk >> SCIF_PLL_PLLCOUNT_Pos)

Maximum PLL startup time in number of slow clock cycles.

Referenced by pll_config_init().

#define PLL_MIN_HZ   40000000

Minimum frequency that the PLL can generate.

Note
The PLL must run at twice this frequency internally, but the output frequency may be divided by two by setting the PLLOPT[1] bit.

Referenced by pll_config_init().

#define PLL_NR_OPTIONS   3

Number of PLL option bits.

Number of PLL options.

Referenced by pll_config_clear_option(), and pll_config_set_option().

#define PLL_OPT_OUTPUT_DIV   1

Divide output frequency by two.

Referenced by pll_config_init().

#define PLL_OPT_VCO_RANGE_HIGH   0

VCO frequency range is 160-240 MHz (80-180 MHz if unset).

Referenced by pll_config_init().

#define PLL_OPT_WBM_DISABLE   2

Disable wide-bandwidth mode.

#define PLL_TIMEOUT_MS   div_ceil(1000 * (PLL_MAX_STARTUP_CYCLES * 2), OSC_RCSYS_MIN_HZ)

Number of milliseconds to wait for PLL lock.

#define PLL_VCO_LOW_THRESHOLD
Value:
#define SCIF_PLL0_VCO_RANGE1_MIN_FREQ
Definition: sam4l/pll.h:44
#define SCIF_PLL0_VCO_RANGE0_MAX_FREQ
Definition: sam4l/pll.h:45

The threshold above which to set the PLL_OPT_VCO_RANGE_HIGH option.

Referenced by pll_config_init().

enum pll_source

PLL clock source.

Enumerator
PLL_SRC_OSC0 

Oscillator 0.

PLL_SRC_GCLK9 

Generic Clock 9.

PLL_NR_SOURCES 

Number of PLL sources.

static void pll_config_clear_option ( struct pll_config cfg,
uint32_t  option 
)
inlinestatic
static void pll_config_init ( struct pll_config cfg,
enum pll_source  src,
uint32_t  divide,
uint32_t  mul 
)
inlinestatic
static void pll_config_read ( struct pll_config cfg,
uint32_t  pll_id 
)
inlinestatic

References Assert, pll_config::ctrl, and NR_PLLS.

static void pll_config_set_option ( struct pll_config cfg,
uint32_t  option 
)
inlinestatic

References Assert, pll_config::ctrl, and PLL_NR_OPTIONS.

Referenced by pll_config_init().

void pll_config_write ( const struct pll_config cfg,
uint32_t  pll_id 
)
void pll_disable ( uint32_t  pll_id)
void pll_enable ( const struct pll_config cfg,
uint32_t  pll_id 
)
static void pll_enable_config_defaults ( uint32_t  pll_id)
inlinestatic
void pll_enable_source ( enum pll_source  src)
inlinestatic

Enable the source of the pll.

The source is enabled, if the source is not already running.

Parameters
srcThe ID of the PLL source to enable.

References Assert, osc_enable(), OSC_ID_OSC0, osc_is_ready(), osc_wait_ready(), PLL_SRC_GCLK9, and PLL_SRC_OSC0.

Referenced by pll_enable_config_defaults().

static bool pll_is_locked ( uint32_t  pll_id)
inlinestatic

References Assert, and NR_PLLS.

Referenced by pll_enable_config_defaults(), and pll_wait_for_lock().

static int pll_wait_for_lock ( unsigned int  pll_id)
inlinestatic

Wait for PLL pll_id to become locked.

Todo:
Use a timeout to avoid waiting forever and hanging the system
Parameters
pll_idThe ID of the PLL to wait for.
Return values
STATUS_OKThe PLL is now locked.
ERR_TIMEOUTTimed out waiting for PLL to become locked.

References Assert, NR_PLLS, and pll_is_locked().

Referenced by run_iis_test().