This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Liquid Crystal Display Controller functionality.
The LCD controller is intended for monochrome passive Liquid Crystal Displays (LCDs) with up to four common terminals and up to 40 segment terminals.
Devices from the following series can use this module:
The outline of this documentation is as follows:
There are no prerequisites for this module.
An LCD is made up of several segments (or complete symbols), which can be visible or invisible. Any single segment has two electrodes, with liquid crystal between them. These electrodes are connected to the common terminal (COM) and the segment terminal (SEG) on the display. When a voltage above a threshold voltage is applied across the liquid crystal, the segment becomes visible. The voltage must alternate, to avoid an electrophoresis effect in the liquid crystal, which degrades the display.
The LCD Controller is intended for use with monochrome passive Liquid Crystal Displays (LCDs) with up to four common terminals and up to 40 segment terminals.
The LCDCA display memory stores the values of all segments to display and should be filled before the next frame starts.
The start of a new frame triggers the update of the shadow display memory. The content of the display memory is copied into the shadow display memory. A display memory refresh is possible without affecting data that is sent to the panel.
When any bit in the display memory is written to a one, the corresponding LCD segment will be energized and opaque. If the same bit has zero written to it, then the corresponding LCD segment is de-energized and thus transparent.
The LCDCA pins (SEGx and COMy) are multiplexed with other peripherals. The user application must first configure the I/O Controller, to give control of the requisite pins to the LCDCA.
This module can control the LCD display while CLK_LCDCA is disabled, but stops functioning when CLK_LCD (32kHz) is disabled.
The power consumption of LCDCA itself can be minimized by:
The clock for this module (CLK_LCDCA) is generated by the Power Manager. It can be enabled or disabled, either manually (via the Power Manager) or automatically when the system enters a sleep mode that disables the clocks to the peripheral bus modules.
The 32kHz clock (CLK_LCD) must be enabled before use.
The LCDCA interrupt request line is connected to the Nested Vectored Interrupt Controller (NVIC). Use of the LCDCA interrupt requires the interrupt controller to be configured first.
The LCD Controller's wake-up signal is connected to the Power Manager Controller (PMC). Use of the wake-up mechanism requires the PMC to enable the corresponding asynchronous wake-up source first. Also, the LCDCA interrupt must be enabled first.
When an external debugger forces the CPU into debug mode, the LCDCA continues normal operation.
For extra information, see Extra Information for Liquid Crystal Display Controller Driver. This includes:
For a list of examples related to this driver, see Examples for Liquid Crystal Display Controller.
Data Structures | |
struct | lcdca_automated_char_config |
Automated character display configuration structure. More... | |
struct | lcdca_blink_config |
Blink configuration structure. More... | |
struct | lcdca_circular_shift_config |
Circular shift configuration structure. More... | |
struct | lcdca_config |
LCDCA controller configuration structure. More... | |
Macros | |
#define | LCDCA_AUTOMATED_CHAR_DMA_CH 3 |
LCDCA automated character DMA Channel (sequential or scrolling) More... | |
Typedefs | |
typedef struct lcdca_automated_char_config | lcdca_automated_char_config_t |
Automated character display configuration structure. More... | |
typedef struct lcdca_blink_config | lcdca_blink_config_t |
Blink configuration structure. More... | |
typedef void(* | lcdca_callback_t )(void) |
LCDCA interrupt callback type. More... | |
typedef struct lcdca_circular_shift_config | lcdca_circular_shift_config_t |
Circular shift configuration structure. More... | |
typedef struct lcdca_config | lcdca_config_t |
LCDCA controller configuration structure. More... | |
Functions | |
void | lcdca_automated_char_reload (const uint8_t *data, size_t width) |
LCDCA automated display reload. More... | |
void | lcdca_automated_char_set_config (struct lcdca_automated_char_config *ac_cfg) |
Configure the LCDCA automated display. More... | |
void | lcdca_automated_char_start (const uint8_t *data, size_t width) |
Start the LCDCA automated display. More... | |
static void | lcdca_automated_char_stop (void) |
Stop the LCDCA automated display mode. More... | |
static void | lcdca_blink_disable (void) |
Disable the LCDCA blink mode. More... | |
static void | lcdca_blink_enable (void) |
Enable the LCDCA blink mode. More... | |
void | lcdca_blink_set_config (struct lcdca_blink_config *blink_cfg) |
Set the LCDCA blink configuration. More... | |
static void | lcdca_circular_shift_disable (void) |
Disable the LCDCA circular shift mode. More... | |
static void | lcdca_circular_shift_enable (void) |
Enable the LCDCA circular shift mode. More... | |
void | lcdca_circular_shift_set_config (struct lcdca_circular_shift_config *cs_cfg) |
Set the LCDCA circular shift configuration. More... | |
void | lcdca_clear_blink_all_pixel (void) |
Stop all LCDCA pixels/segments from blinking. More... | |
void | lcdca_clear_blink_pixel (uint8_t pix_com, uint8_t pix_seg) |
Stop a specified LCDCA pixel/segment from blinking. More... | |
static void | lcdca_clear_display_memory (void) |
Clear all the LCDCA display memory. More... | |
void | lcdca_clear_pixel (uint8_t pix_com, uint8_t pix_seg) |
Disable the specified pixel/segment in the LCDCA display memory. More... | |
static void | lcdca_clear_status (void) |
Clear the LCDCA beginning of frame interrupt status. More... | |
void | lcdca_clk_init (void) |
LCDCA clock initialization. More... | |
void | lcdca_disable (void) |
Disable the LCDCA module. More... | |
static void | lcdca_disable_interrupt (void) |
Disable the LCDCA beginning of frame interrupt. More... | |
void | lcdca_disable_timer (uint8_t lcd_timer) |
Disable the specified LCDCA timer. More... | |
static void | lcdca_disable_wakeup (void) |
Disable the LCDCA wake-up. More... | |
void | lcdca_enable (void) |
Enable the LCDCA module. More... | |
static void | lcdca_enable_interrupt (void) |
Enable the LCDCA beginning of frame interrupt. More... | |
void | lcdca_enable_timer (uint8_t lcd_timer) |
Enable the specified LCDCA timer, and wait until it is running. More... | |
static void | lcdca_enable_wakeup (void) |
Enable the LCDCA wake-up. More... | |
bool | lcdca_get_pixel (uint8_t pix_com, uint8_t pix_seg) |
Get the specified pixel/segment state from the LCDCA display memory. More... | |
static uint32_t | lcdca_get_status (void) |
Get the LCDCA status register. More... | |
static void | lcdca_lock_shadow_dislay (void) |
Lock the LCDCA shadow display memory. More... | |
void | lcdca_set_blink_pixel (uint8_t pix_com, uint8_t pix_seg) |
Start an LCDCA pixel/segment blinking. More... | |
void | lcdca_set_callback (lcdca_callback_t callback, uint8_t irq_line, uint8_t irq_level) |
Set the callback for the LCDCA 'beginning of frame' interrupt. More... | |
void | lcdca_set_config (struct lcdca_config *lcdca_cfg) |
Configure the LCDCA controller. More... | |
void | lcdca_set_contrast (int8_t contrast) |
Set the LCDCA fine contrast. More... | |
void | lcdca_set_display_memory (void) |
Set all bits in the LCDCA display memory high. More... | |
void | lcdca_set_pixel (uint8_t pix_com, uint8_t pix_seg) |
Enable the specified pixel/segment in the LCDCA display memory. More... | |
void | lcdca_toggle_pixel (uint8_t pix_com, uint8_t pix_seg) |
Toggle the specified pixel/segment in the LCDCA display memory. More... | |
static void | lcdca_unlock_shadow_dislay (void) |
Unlock the LCDCA shadow display memory. More... | |
void | lcdca_write_packet (uint8_t lcd_tdg, uint8_t first_seg, const uint8_t *data, size_t width, uint8_t dir) |
Send a sequence of ASCII bytes to the LCDCA via the digit decoder. More... | |
LCDCA Address Limits | |
#define | LCDCA_MAX_NR_OF_COM 4 |
Maximum number of common lines. More... | |
#define | LCDCA_MAX_NBR_OF_SEG 40 |
Maximum number of segment lines. More... | |
LCDCA Display Digit | |
#define | LCDCA_TDG_7SEG3COM 0 |
7-segment display with three common terminals More... | |
#define | LCDCA_TDG_7SEG4COM 1 |
7-segment display with four common terminals More... | |
#define | LCDCA_TDG_14SEG4COM 2 |
14-segment display with four common terminals More... | |
#define | LCDCA_TDG_16SEG3COM 3 |
16-segment display with three common terminals More... | |
LCDCA Timer Resource | |
#define | LCDCA_TIMER_FC0 0 |
Timer FC0 resource. More... | |
#define | LCDCA_TIMER_FC1 1 |
Timer FC1 resource. More... | |
#define | LCDCA_TIMER_FC2 2 |
Timer FC2 resource. More... | |
LCDCA CMCFG Digit Reverse Mode | |
#define | LCDCA_CMCFG_DREV_LEFT 1 |
Decrement the segment index. More... | |
#define | LCDCA_CMCFG_DREV_RIGHT 0 |
Increment the segment index. More... | |
LCDCA Duty Selection. | |
#define | LCDCA_DUTY_1_4 0 |
Duty=1/4, Bias=1/3, COM0:3. More... | |
#define | LCDCA_DUTY_STATIC 1 |
Duty=Static, Bias=Static, COM0. More... | |
#define | LCDCA_DUTY_1_2 2 |
Duty=1/2, Bias=1/3, COM0:1. More... | |
#define | LCDCA_DUTY_1_3 3 |
Duty=1/3, Bias=1/3, COM0:2. More... | |
LCDCA Blink Mode | |
#define | LCDCA_BLINK_FULL 0 |
All LCD segments will blink. More... | |
#define | LCDCA_BLINK_SELECTED LCDCA_BCFG_MODE |
Only the selected segment will blink. More... | |
LCDCA Shift Register Direction | |
#define | LCDCA_CSR_RIGHT LCDCA_CSRCFG_DIR |
Right direction. More... | |
#define | LCDCA_CSR_LEFT 0 |
Left direction. More... | |
LCDCA Automated Mode. | |
#define | LCDCA_AUTOMATED_MODE_SEQUENTIAL 0 |
Sequential character string display mode. More... | |
#define | LCDCA_AUTOMATED_MODE_SCROLLING 1 |
Scrolling character string display mode. More... | |
LCDCA Automated Direction. | |
#define | LCDCA_AUTOMATED_DIR_REVERSE 1 |
Digit direction is reversed. More... | |
#define | LCDCA_AUTOMATED_DIR_NOT_REVERSE 0 |
Digit direction is not reversed. More... | |
#define LCDCA_AUTOMATED_CHAR_DMA_CH 3 |
LCDCA automated character DMA Channel (sequential or scrolling)
Referenced by lcdca_automated_char_reload(), lcdca_automated_char_start(), and lcdca_automated_char_stop().
#define LCDCA_AUTOMATED_DIR_NOT_REVERSE 0 |
Digit direction is not reversed.
#define LCDCA_AUTOMATED_DIR_REVERSE 1 |
Digit direction is reversed.
Referenced by run_lcdca_automated_scrolling_test(), and run_lcdca_automated_sequential_test().
#define LCDCA_AUTOMATED_MODE_SCROLLING 1 |
Scrolling character string display mode.
Referenced by run_lcdca_automated_scrolling_test().
#define LCDCA_AUTOMATED_MODE_SEQUENTIAL 0 |
Sequential character string display mode.
Referenced by run_lcdca_automated_sequential_test().
#define LCDCA_BLINK_FULL 0 |
All LCD segments will blink.
#define LCDCA_BLINK_SELECTED LCDCA_BCFG_MODE |
Only the selected segment will blink.
Referenced by run_lcdca_blink_test().
#define LCDCA_CMCFG_DREV_LEFT 1 |
Decrement the segment index.
Referenced by lcdca_write_packet().
#define LCDCA_CMCFG_DREV_RIGHT 0 |
Increment the segment index.
Referenced by lcdca_write_packet().
#define LCDCA_CSR_LEFT 0 |
Left direction.
#define LCDCA_CSR_RIGHT LCDCA_CSRCFG_DIR |
Right direction.
Referenced by run_lcdca_autonomous_test().
#define LCDCA_DUTY_1_2 2 |
Duty=1/2, Bias=1/3, COM0:1.
#define LCDCA_DUTY_1_3 3 |
Duty=1/3, Bias=1/3, COM0:2.
#define LCDCA_DUTY_1_4 0 |
Duty=1/4, Bias=1/3, COM0:3.
#define LCDCA_DUTY_STATIC 1 |
Duty=Static, Bias=Static, COM0.
#define LCDCA_MAX_NBR_OF_SEG 40 |
Maximum number of segment lines.
Referenced by lcdca_clear_pixel(), lcdca_set_pixel(), and lcdca_toggle_pixel().
#define LCDCA_MAX_NR_OF_COM 4 |
Maximum number of common lines.
Referenced by lcdca_clear_blink_all_pixel(), lcdca_clear_pixel(), lcdca_set_pixel(), and lcdca_toggle_pixel().
#define LCDCA_TDG_14SEG4COM 2 |
14-segment display with four common terminals
Referenced by run_lcdca_automated_scrolling_test(), and run_lcdca_automated_sequential_test().
#define LCDCA_TDG_16SEG3COM 3 |
16-segment display with three common terminals
#define LCDCA_TDG_7SEG3COM 0 |
7-segment display with three common terminals
#define LCDCA_TDG_7SEG4COM 1 |
7-segment display with four common terminals
#define LCDCA_TIMER_FC0 0 |
Timer FC0 resource.
Referenced by lcdca_disable_timer(), lcdca_enable_timer(), and run_lcdca_init_test().
#define LCDCA_TIMER_FC1 1 |
Timer FC1 resource.
Referenced by lcdca_disable_timer(), lcdca_enable_timer(), run_lcdca_automated_scrolling_test(), run_lcdca_automated_sequential_test(), and run_lcdca_init_test().
#define LCDCA_TIMER_FC2 2 |
Timer FC2 resource.
Referenced by lcdca_disable_timer(), lcdca_enable_timer(), run_lcdca_autonomous_test(), run_lcdca_blink_test(), and run_lcdca_init_test().
typedef struct lcdca_automated_char_config lcdca_automated_char_config_t |
Automated character display configuration structure.
typedef struct lcdca_blink_config lcdca_blink_config_t |
Blink configuration structure.
typedef void(* lcdca_callback_t)(void) |
LCDCA interrupt callback type.
typedef struct lcdca_circular_shift_config lcdca_circular_shift_config_t |
Circular shift configuration structure.
typedef struct lcdca_config lcdca_config_t |
LCDCA controller configuration structure.
void lcdca_automated_char_reload | ( | const uint8_t * | data, |
size_t | width | ||
) |
LCDCA automated display reload.
[in] | data | Data string buffer pointer |
[in] | width | Data string length |
References LCDCA_AUTOMATED_CHAR_DMA_CH, and pdca_channel_write_reload().
void lcdca_automated_char_set_config | ( | struct lcdca_automated_char_config * | ac_cfg | ) |
Configure the LCDCA automated display.
[in] | ac_cfg | Pointer to an automated display configuration structure |
References Assert, lcdca_automated_char_config::automated_mode, lcdca_automated_char_config::automated_timer, lcdca_automated_char_config::dign, lcdca_automated_char_config::dir_reverse, lcdca_automated_char_config::lcd_tdg, lcdca_automated_char_config::steps, and lcdca_automated_char_config::stseg.
Referenced by run_lcdca_automated_scrolling_test(), and run_lcdca_automated_sequential_test().
void lcdca_automated_char_start | ( | const uint8_t * | data, |
size_t | width | ||
) |
Start the LCDCA automated display.
[in] | data | Data string buffer pointer |
[in] | width | Data string length |
References pdca_channel_config_t::addr, Assert, pdca_channel_config_t::etrig, LCDCA_AUTOMATED_CHAR_DMA_CH, pdca_channel_enable(), pdca_channel_set_config(), pdca_enable(), pdca_channel_config_t::pid, pdca_channel_config_t::r_addr, pdca_channel_config_t::r_size, pdca_channel_config_t::ring, pdca_channel_config_t::size, and pdca_channel_config_t::transfer_size.
Referenced by run_lcdca_automated_scrolling_test(), and run_lcdca_automated_sequential_test().
|
inlinestatic |
Stop the LCDCA automated display mode.
References LCDCA_AUTOMATED_CHAR_DMA_CH, and pdca_channel_disable().
Referenced by lcdca_disable(), run_lcdca_automated_scrolling_test(), and run_lcdca_automated_sequential_test().
|
inlinestatic |
Disable the LCDCA blink mode.
Referenced by lcdca_disable(), and run_lcdca_blink_test().
|
inlinestatic |
Enable the LCDCA blink mode.
Referenced by run_lcdca_blink_test().
void lcdca_blink_set_config | ( | struct lcdca_blink_config * | blink_cfg | ) |
Set the LCDCA blink configuration.
[in] | blink_cfg | Pointer to the LCD blink configuration structure |
References Assert, lcdca_blink_config::lcd_blink_mode, and lcdca_blink_config::lcd_blink_timer.
Referenced by run_lcdca_blink_test().
|
inlinestatic |
Disable the LCDCA circular shift mode.
Referenced by lcdca_disable(), and run_lcdca_autonomous_test().
|
inlinestatic |
Enable the LCDCA circular shift mode.
Referenced by run_lcdca_autonomous_test().
void lcdca_circular_shift_set_config | ( | struct lcdca_circular_shift_config * | cs_cfg | ) |
Set the LCDCA circular shift configuration.
[in] | cs_cfg | Pointer to a circular shift configuration structure |
References lcdca_circular_shift_config::data, lcdca_circular_shift_config::lcd_csr_dir, lcdca_circular_shift_config::lcd_csr_timer, and lcdca_circular_shift_config::size.
Referenced by run_lcdca_autonomous_test().
void lcdca_clear_blink_all_pixel | ( | void | ) |
Stop all LCDCA pixels/segments from blinking.
References lcdca_clear_blink_pixel(), and LCDCA_MAX_NR_OF_COM.
void lcdca_clear_blink_pixel | ( | uint8_t | pix_com, |
uint8_t | pix_seg | ||
) |
Stop a specified LCDCA pixel/segment from blinking.
[in] | pix_com | Pixel/segment COMx coordinate |
[in] | pix_seg | Pixel/segment SEGy coordinate (range 0 to 1 inclusive) |
References Assert.
Referenced by lcdca_clear_blink_all_pixel().
|
inlinestatic |
Clear all the LCDCA display memory.
void lcdca_clear_pixel | ( | uint8_t | pix_com, |
uint8_t | pix_seg | ||
) |
Disable the specified pixel/segment in the LCDCA display memory.
[in] | pix_com | Pixel/segment COMx coordinate |
[in] | pix_seg | Pixel/segment SEGy coordinate |
References lcdca_get_pixel_register(), LCDCA_MAX_NBR_OF_SEG, and LCDCA_MAX_NR_OF_COM.
Referenced by lcdca_toggle_pixel(), and run_lcdca_blink_test().
|
inlinestatic |
Clear the LCDCA beginning of frame interrupt status.
Referenced by LCDCA_Handler().
void lcdca_clk_init | ( | void | ) |
LCDCA clock initialization.
References BPM_CLK32_SOURCE_OSC32K, BPM_CLK32_SOURCE_RC32K, bpm_set_clk32_source(), osc_enable(), OSC_ID_OSC32, OSC_ID_RC32K, osc_is_ready(), osc_wait_ready(), and sysclk_enable_peripheral_clock().
Referenced by run_lcdca_init_test().
void lcdca_disable | ( | void | ) |
Disable the LCDCA module.
References lcdca_automated_char_stop(), lcdca_blink_disable(), lcdca_circular_shift_disable(), SLEEPMGR_RET, and sleepmgr_unlock_mode().
Referenced by run_lcdca_end_test().
|
inlinestatic |
Disable the LCDCA beginning of frame interrupt.
void lcdca_disable_timer | ( | uint8_t | lcd_timer | ) |
Disable the specified LCDCA timer.
[in] | lcd_timer | Timer number to be disabled |
References LCDCA_TIMER_FC0, LCDCA_TIMER_FC1, and LCDCA_TIMER_FC2.
|
inlinestatic |
Disable the LCDCA wake-up.
void lcdca_enable | ( | void | ) |
Enable the LCDCA module.
References sleepmgr_lock_mode(), and SLEEPMGR_RET.
Referenced by run_lcdca_init_test().
|
inlinestatic |
Enable the LCDCA beginning of frame interrupt.
Referenced by lcdca_set_callback().
void lcdca_enable_timer | ( | uint8_t | lcd_timer | ) |
Enable the specified LCDCA timer, and wait until it is running.
[in] | lcd_timer | Timer number to be enabled |
References LCDCA_TIMER_FC0, LCDCA_TIMER_FC1, and LCDCA_TIMER_FC2.
Referenced by run_lcdca_init_test().
|
inlinestatic |
Enable the LCDCA wake-up.
bool lcdca_get_pixel | ( | uint8_t | pix_com, |
uint8_t | pix_seg | ||
) |
Get the specified pixel/segment state from the LCDCA display memory.
[in] | pix_com | Pixel/segment COMx coordinate |
[in] | pix_seg | Pixel/segment SEGy coordinate |
References lcdca_get_pixel_register().
|
inlinestatic |
Get the LCDCA status register.
Referenced by run_lcdca_autonomous_test(), run_lcdca_blink_test(), and run_lcdca_init_test().
|
inlinestatic |
Lock the LCDCA shadow display memory.
void lcdca_set_blink_pixel | ( | uint8_t | pix_com, |
uint8_t | pix_seg | ||
) |
Start an LCDCA pixel/segment blinking.
[in] | pix_com | Pixel/segment COMx coordinate |
[in] | pix_seg | Pixel/segment SEGy coordinate (range 0 to 1 inclusive) |
References Assert.
Referenced by run_lcdca_blink_test().
void lcdca_set_callback | ( | lcdca_callback_t | callback, |
uint8_t | irq_line, | ||
uint8_t | irq_level | ||
) |
Set the callback for the LCDCA 'beginning of frame' interrupt.
[in] | callback | Pointer to an interrupt callback function |
[in] | irq_line | Interrupt line |
[in] | irq_level | Interrupt priority level |
References lcdca_callback_pointer, and lcdca_enable_interrupt().
void lcdca_set_config | ( | struct lcdca_config * | lcdca_cfg | ) |
Configure the LCDCA controller.
[in] | lcdca_cfg | Pointer to an LCDCA configuration structure |
References Assert, lcdca_config::contrast, lcdca_config::duty_type, lcdca_config::fc0, lcdca_config::fc1, lcdca_config::fc2, lcdca_config::lcd_clkdiv, lcdca_config::lcd_pres, lcdca_set_contrast(), lcdca_config::lp_wave, lcdca_config::port_mask, and lcdca_config::x_bias.
Referenced by run_lcdca_init_test().
void lcdca_set_contrast | ( | int8_t | contrast | ) |
Set the LCDCA fine contrast.
Transfer function: VLCD = 3.0V + (fcont[5:0] * 0.016V)
[in] | contrast | Contrast value (range -32 to 31 inclusive) |
Referenced by lcdca_set_config(), and run_lcdca_contrast_change_test().
void lcdca_set_display_memory | ( | void | ) |
Set all bits in the LCDCA display memory high.
void lcdca_set_pixel | ( | uint8_t | pix_com, |
uint8_t | pix_seg | ||
) |
Enable the specified pixel/segment in the LCDCA display memory.
[in] | pix_com | Pixel/segment COMx coordinate |
[in] | pix_seg | Pixel/segment SEGy coordinate |
References lcdca_get_pixel_register(), LCDCA_MAX_NBR_OF_SEG, and LCDCA_MAX_NR_OF_COM.
Referenced by lcdca_toggle_pixel(), and run_lcdca_blink_test().
void lcdca_toggle_pixel | ( | uint8_t | pix_com, |
uint8_t | pix_seg | ||
) |
Toggle the specified pixel/segment in the LCDCA display memory.
[in] | pix_com | Pixel/segment COMx coordinate |
[in] | pix_seg | Pixel/segment SEGy coordinate |
References lcdca_clear_pixel(), lcdca_get_pixel_register(), LCDCA_MAX_NBR_OF_SEG, LCDCA_MAX_NR_OF_COM, and lcdca_set_pixel().
|
inlinestatic |
Unlock the LCDCA shadow display memory.
void lcdca_write_packet | ( | uint8_t | lcd_tdg, |
uint8_t | first_seg, | ||
const uint8_t * | data, | ||
size_t | width, | ||
uint8_t | dir | ||
) |
Send a sequence of ASCII bytes to the LCDCA via the digit decoder.
[in] | lcd_tdg | Type of digit decoder |
[in] | first_seg | First SEG where the data will be written |
[in] | data | ASCII data buffer pointer |
[in] | width | Maximum number of data bytes |
[in] | dir | Direction (0 for left to right, otherwise right to left) |
References LCDCA_CMCFG_DREV_LEFT, and LCDCA_CMCFG_DREV_RIGHT.