Template of a user-defined protocol support for PLC USI service.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include <compiler.h>
#include <asf.h>
#include "conf_example.h"
Variables | |
static bool | b_led_swap = false |
Response buffer | |
enum | serial_if_user_def_cmd_t { SERIAL_IF_USER_DEF_GET_CMD, SERIAL_IF_USER_DEF_GET_CMD_RSP, SERIAL_IF_USER_DEF_SET_CMD, SERIAL_IF_USER_DEF_SET_CMD_RSP, SERIAL_IF_USER_DEF_INVALID } |
static uint8_t | uc_serial_rsp_buf [5] |
static x_usi_serial_cmd_params_t | x_phy_serial_msg |
uint8_t | serial_if_user_def_api_parser (uint8_t *puc_rx_msg, uint16_t us_len) |
Task to manage the serialization of the user defined protocol. More... | |
static void | prvSetupHardware (void) |
Configure the hardware. More... | |
int | main (void) |
Main code entry point. More... | |
int main | ( | void | ) |
Main code entry point.
References b_led_swap, LED_Toggle, PROTOCOL_USER_DEFINED, prvSetupHardware(), x_usi_serial_cmd_params_t::uc_protocol_type, usi_init(), and usi_process().
|
static |
|
static |
Referenced by serial_if_user_def_api_parser().
|
static |