This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Configurable Custom Logic functionality.
Support and FAQ: visit Microchip Support
The following peripheral is used by this module:
The following devices can use this module:
The outline of this documentation is as follows:
There are no prerequisites for this module.
The Temperature Sensor (TSENS) can be used to accurately measure the operating temperature of the device. TSENS accurately measures the operating temperature of the device by comparing the difference in two temperature dependent frequencies to a known frequency. The frequency of the temperature dependent oscillator (TOSC) is measured twice: first with the min configuration and next with the maximum configuration. The resulting signed value is proportional to the temperature and is corrected for offset by the contents of the OFFSET register.
Accurately measures a temperature:
The number of periods of GCLK_TSENS used for the measurement is defined by the GAIN register. The width of the resulting pulse is measured using a counter clocked by GCLK_TSENS in the up direction for the 1st phase and in the down 2nd phase. Register GAIN and OFFSET is loaded from NVM, or can also be fixed by user.
\[ VALUE = OFFSET + (\frac{f_{TOSCMIN} - f_{TOSCMAX}}{f_{GCLK}}) \times GAIN \]
Resolution (#/°C) | GAIN@48MHz | GAIN@40MHz |
---|---|---|
×1 (1°C) | 960 | 800 |
×10 (0.1°C) | 9600 | 8000 |
×100 (0.01°C) | 96000 | 80000 |
The TSENS module window monitor function can be used to automatically compare the conversion result against a predefined pair of upper and lower threshold values.
Event generation and event actions are configurable in the TSENS.
The TSENS has one actions that can be triggered upon event reception:
The TSENS can generate the following output event:
If the event actions are enabled in the configuration, any incoming event will trigger the action.
If the window monitor event is enabled, an event will be generated when the configured window condition is detected.
There are no special considerations for this module.
For extra information, see Extra Information for TSENS Driver. This includes:
For a list of examples related to this driver, see Examples for TSENS Driver.
Data Structures | |
struct | tsens_calibration |
Calibration configuration structure. More... | |
struct | tsens_config |
TSENS configuration structure. More... | |
struct | tsens_events |
TSENS event enable/disable structure. More... | |
struct | tsens_module |
TSENS software device instance structure. More... | |
struct | tsens_window_config |
Window monitor configuration structure. More... | |
Macros | |
#define | ERRATA_14476 true |
The magnitude of the temperature measurement value decreases with increasing temperature, i.e. More... | |
Typedefs | |
typedef void(* | tsens_callback_t )(enum tsens_callback) |
Type of the callback functions. More... | |
Enumerations | |
enum | tsens_callback { TSENS_CALLBACK_RESULT_READY, TSENS_CALLBACK_OVERRUN, TSENS_CALLBACK_WINDOW, TSENS_CALLBACK_OVF } |
TSENS Callback Types. More... | |
enum | tsens_event_action { TSENS_EVENT_ACTION_DISABLED = 0, TSENS_EVENT_ACTION_START_CONV = TSENS_EVCTRL_STARTEI } |
TSENS event action enum. More... | |
enum | tsens_window_mode { TSENS_WINDOW_MODE_DISABLE = TSENS_CTRLC_WINMODE_DISABLE, TSENS_WINDOW_MODE_ABOVE = TSENS_CTRLC_WINMODE_ABOVE, TSENS_WINDOW_MODE_BELOW = TSENS_CTRLC_WINMODE_BELOW, TSENS_WINDOW_MODE_INSIDE = TSENS_CTRLC_WINMODE_INSIDE, TSENS_WINDOW_MODE_OUTSIDE = TSENS_CTRLC_WINMODE_OUTSIDE, TSENS_WINDOW_MODE_HYST_ABOVE = TSENS_CTRLC_WINMODE_HYST_ABOVE, TSENS_WINDOW_MODE_HYST_BELOW = TSENS_CTRLC_WINMODE_HYST_BELOW } |
TSENS window monitor mode enum. More... | |
Module Status Flags | |
TSENS status flags, returned by tsens_get_status() and cleared by tsens_clear_status(). | |
#define | TSENS_STATUS_RESULT_READY (1UL << 0) |
TSENS result ready. More... | |
#define | TSENS_STATUS_OVERRUN (1UL << 1) |
TSENS result overwritten before read. More... | |
#define | TSENS_STATUS_WINDOW (1UL << 2) |
Window monitor match. More... | |
#define | TSENS_STATUS_OVERFLOW (1UL << 3) |
TSENS result overflows. More... | |
Driver Initialization and Configuration | |
enum status_code | tsens_init (struct tsens_config *config) |
Initializes the TSENS. More... | |
void | tsens_get_config_defaults (struct tsens_config *const config) |
Initializes an TSENS configuration structure to defaults. More... | |
Status Management | |
static uint32_t | tsens_get_status (void) |
Retrieves the current module status. More... | |
static void | tsens_clear_status (const uint32_t status_flags) |
Clears a module status flag. More... | |
Enable, Disable, and Reset TSENS Module, Start Conversion and Read Result | |
static bool | tsens_is_syncing (void) |
Determines if the hardware module is currently synchronizing to the bus. More... | |
static void | tsens_enable (void) |
Enables the TSENS module. More... | |
static void | tsens_disable (void) |
Disables the TSENS module. More... | |
static void | tsens_reset (void) |
Resets the TSENS module. More... | |
static void | tsens_enable_events (struct tsens_events *const events) |
Enables an TSENS event output. More... | |
static void | tsens_disable_events (struct tsens_events *const events) |
Disables an TSENS event output. More... | |
static void | tsens_start_conversion (void) |
Start a TSENS conversion. More... | |
enum status_code | tsens_read (int32_t *result) |
Reads the TSENS result. More... | |
Callback Management | |
enum status_code | tsens_register_callback (struct tsens_module *const module, tsens_callback_t callback_func, enum tsens_callback callback_type) |
Registers a callback. More... | |
enum status_code | tsens_unregister_callback (struct tsens_module *const module, enum tsens_callback callback_type) |
Unregisters a callback. More... | |
static void | tsens_enable_callback (enum tsens_callback callback_type) |
Enables callback. More... | |
static void | tsens_disable_callback (enum tsens_callback callback_type) |
Disables callback. More... | |
void | tsens_read_job (struct tsens_module *const module_inst, int32_t *result) |
Read result from TSENS. More... | |
#define ERRATA_14476 true |
The magnitude of the temperature measurement value decreases with increasing temperature, i.e.
it has a negative temperature coefficient. Errata reference: 14476.
#define TSENS_STATUS_OVERFLOW (1UL << 3) |
TSENS result overflows.
Referenced by tsens_clear_status(), and tsens_get_status().
#define TSENS_STATUS_OVERRUN (1UL << 1) |
TSENS result overwritten before read.
Referenced by tsens_clear_status(), tsens_get_status(), and tsens_read().
#define TSENS_STATUS_RESULT_READY (1UL << 0) |
TSENS result ready.
Referenced by tsens_clear_status(), tsens_get_status(), and tsens_read().
#define TSENS_STATUS_WINDOW (1UL << 2) |
Window monitor match.
Referenced by tsens_clear_status(), and tsens_get_status().
typedef void(* tsens_callback_t)(enum tsens_callback) |
Type of the callback functions.
enum tsens_callback |
TSENS Callback Types.
Callback types for TSENS callback driver.
enum tsens_event_action |
enum tsens_window_mode |
TSENS window monitor mode enum.
Enum for the possible window monitor modes for the TSENS.
|
inlinestatic |
Clears a module status flag.
Clears the given status flag of the module.
[in] | module_inst | Pointer to the TSENS software instance struct |
[in] | status_flags | Bitmask of TSENS_STATUS_* flags to clear |
References TSENS_STATUS_OVERFLOW, TSENS_STATUS_OVERRUN, TSENS_STATUS_RESULT_READY, and TSENS_STATUS_WINDOW.
Referenced by tsens_read().
|
inlinestatic |
Disables the TSENS module.
Disables an TSENS module that was previously enabled.
References tsens_is_syncing().
Referenced by tsens_reset().
|
inlinestatic |
Disables callback.
Disables the callback function registered by the tsens_register_callback.
[in] | callback_type | Callback type given by an enum |
References TSENS_CALLBACK_OVERRUN, TSENS_CALLBACK_OVF, TSENS_CALLBACK_RESULT_READY, and TSENS_CALLBACK_WINDOW.
|
inlinestatic |
Disables an TSENS event output.
Disables one or more output events to or from the TSENS module. See tsens_events for a list of events this module supports.
[in] | events | Struct containing flags of events to disable |
References Assert, and tsens_events::generate_event_on_window_monitor.
|
inlinestatic |
Enables the TSENS module.
Enables an TSENS module that has previously been configured.
References tsens_is_syncing().
|
inlinestatic |
Enables callback.
Enables the callback function registered by tsens_register_callback. The callback function will be called from the interrupt handler when the conditions for the callback type are met.
[in] | callback_type | Callback type given by an enum |
References TSENS_CALLBACK_OVERRUN, TSENS_CALLBACK_OVF, TSENS_CALLBACK_RESULT_READY, and TSENS_CALLBACK_WINDOW.
|
inlinestatic |
Enables an TSENS event output.
Enables one or more input or output events to or from the TSENS module. See tsens_events for a list of events this module supports.
[in] | events | Struct containing flags of events to enable |
References Assert, and tsens_events::generate_event_on_window_monitor.
void tsens_get_config_defaults | ( | struct tsens_config *const | config | ) |
Initializes an TSENS configuration structure to defaults.
Initializes a given TSENS configuration struct to a set of known default values. This function should be called on any new instance of the configuration struct before being modified by the user application.
The default configuration is as follows:
[out] | config | Pointer to configuration struct to initialize to default values |
References Assert, tsens_config::calibration, tsens_config::clock_source, tsens_config::event_action, tsens_config::free_running, tsens_calibration::gain, GAIN_1_OFFSET, GCLK_GENERATOR_0, tsens_calibration::offset, tsens_config::run_in_standby, TSENS_EVENT_ACTION_DISABLED, TSENS_WINDOW_MODE_DISABLE, tsens_config::window, tsens_window_config::window_lower_value, tsens_window_config::window_mode, and tsens_window_config::window_upper_value.
|
inlinestatic |
Retrieves the current module status.
Retrieves the status of the module, giving overall state information.
TSENS_STATUS_RESULT_READY | TSENS result is ready to be read |
TSENS_STATUS_OVERRUN | TSENS result overwritten before read |
TSENS_STATUS_WINDOW | TSENS has detected a value inside the set window range |
TSENS_STATUS_OVERFLOW | TSENS result overflows |
References TSENS_STATUS_OVERFLOW, TSENS_STATUS_OVERRUN, TSENS_STATUS_RESULT_READY, and TSENS_STATUS_WINDOW.
Referenced by tsens_read().
enum status_code tsens_init | ( | struct tsens_config * | config | ) |
Initializes the TSENS.
Initializes the TSENS device struct and the hardware module based on the given configuration struct values.
[in] | config | Pointer to the configuration struct |
STATUS_OK | The initialization was successful |
STATUS_ERR_INVALID_ARG | Invalid argument(s) were provided |
STATUS_BUSY | The module is busy with a reset operation |
STATUS_ERR_DENIED | The module is enabled |
References _tsens_set_config(), Assert, STATUS_BUSY, STATUS_ERR_DENIED, system_apb_clock_set_mask(), and SYSTEM_CLOCK_APB_APBA.
|
inlinestatic |
Determines if the hardware module is currently synchronizing to the bus.
Checks to see if the underlying hardware peripheral module(s) are currently synchronizing across multiple clock domains to the hardware bus. This function can be used to delay further operations on a module until such time that it is ready, to prevent blocking delays for synchronization in the user application.
true | If the module synchronization is ongoing |
false | If the module has completed synchronization |
Referenced by tsens_disable(), tsens_enable(), tsens_reset(), and tsens_start_conversion().
enum status_code tsens_read | ( | int32_t * | result | ) |
Reads the TSENS result.
Reads the result from a TSENS conversion that was previously started.
[out] | result | Pointer to store the result value in |
STATUS_OK | The result was retrieved successfully |
STATUS_BUSY | A conversion result was not ready |
STATUS_ERR_OVERFLOW | The result register has been overwritten by the TSENS module before the result was read by the software |
References Assert, STATUS_BUSY, STATUS_ERR_BAD_DATA, STATUS_ERR_OVERFLOW, STATUS_OK, tsens_clear_status(), tsens_get_status(), TSENS_STATUS_OVERRUN, and TSENS_STATUS_RESULT_READY.
void tsens_read_job | ( | struct tsens_module *const | module_inst, |
int32_t * | result | ||
) |
Read result from TSENS.
[in] | module_inst | Pointer to the TSENS software instance struct |
[out] | result | Pointer to store the TSENS result |
References Assert, and tsens_start_conversion().
enum status_code tsens_register_callback | ( | struct tsens_module *const | module, |
tsens_callback_t | callback_func, | ||
enum tsens_callback | callback_type | ||
) |
Registers a callback.
Registers a callback function which is implemented by the user.
[in] | module | Pointer to TSENS software instance struct |
[in] | callback_func | Pointer to callback function |
[in] | callback_type | Callback type given by an enum |
References Assert, STATUS_ERR_INVALID_ARG, and STATUS_OK.
|
inlinestatic |
Resets the TSENS module.
Resets an TSENS module, clearing all module state and registers to their default values.
References tsens_disable(), and tsens_is_syncing().
|
inlinestatic |
Start a TSENS conversion.
Start a new TSENS conversion.
References tsens_is_syncing().
Referenced by tsens_read_job().
enum status_code tsens_unregister_callback | ( | struct tsens_module *const | module, |
enum tsens_callback | callback_type | ||
) |
Unregisters a callback.
Unregisters a callback function which is implemented by the user.
[in] | module | Pointer to TSENS software instance struct |
[in] | callback_type | Callback type given by an enum |
References Assert, STATUS_ERR_INVALID_ARG, and STATUS_OK.