Copyright (c) 2013-2018 Microchip Technology Inc.
and its subsidiaries.
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
#include <stdlib.h>
#include "pal.h"
#include "return_val.h"
#include "tal.h"
#include "ieee_const.h"
#include "tal_pib.h"
#include "tal_irq_handler.h"
#include "at86rf232.h"
#include "stack_config.h"
#include "bmm.h"
#include "qmm.h"
#include "tal_rx.h"
#include "tal_tx.h"
#include "tal_constants.h"
#include "tal_internal.h"
#include "tal_slotted_csma.h"
#include "mac_build_config.h"
Macros | |
#define | PLL_LOCK_ATTEMPTS (3) |
Functions | |
tal_trx_status_t | set_trx_state (trx_cmd_t trx_cmd) |
Sets transceiver state. More... | |
static void | switch_pll_on (void) |
Switches the PLL on. More... | |
void | tal_task (void) |
TAL task handling. More... | |
Variables | |
uint8_t | last_frame_length |
frame_info_t * | mac_frame_ptr |
Frame pointer for the frame structure provided by the MCL. More... | |
volatile bool | tal_awake_end_flag |
csma_state_t | tal_csma_state |
CSMA state machine variable. More... | |
uint8_t * | tal_frame_to_tx |
Pointer to the 15.4 frame created by the TAL to be handed over to the transceiver. More... | |
queue_t | tal_incoming_frame_queue |
Queue that contains all frames that are uploaded from the trx, but have not be processed by the MCL yet. More... | |
tal_pib_t | tal_pib |
buffer_t * | tal_rx_buffer = NULL |
Pointer to receive buffer that can be used to upload a frame from the trx. More... | |
bool | tal_rx_on_required |
Indicates if the transceiver needs to switch on its receiver by tal_task(), because it could not be switched on due to buffer shortage. More... | |
tal_state_t | tal_state |
Current state of the TAL state machine. More... | |
uint32_t | tal_timestamp |
Timestamp The timestamping is only required for beaconing networks or if timestamping is explicitly enabled. More... | |
tal_trx_status_t | tal_trx_status |
Current state of the transceiver. More... | |
#define PLL_LOCK_ATTEMPTS (3) |
|
static |
Switches the PLL on.
References Assert, CMD_PLL_ON, PLL_LOCK_DURATION_MAX_US, RG_IRQ_MASK, RG_IRQ_STATUS, RG_PLL_CF, RG_TRX_STATE, SR_TRX_STATUS, start_time, TRX_IRQ_0_PLL_LOCK, and TRX_OFF.
Referenced by set_trx_state().
void tal_task | ( | void | ) |
TAL task handling.
This function
References Assert, CMD_RX_AACK_ON, CMD_RX_ON, NULL, process_incoming_frame(), set_trx_state(), slotted_csma_state_handling(), TAL_IDLE, tal_incoming_frame_queue, tal_pib, tal_rx_buffer, tal_rx_on_required, TAL_SLOTTED_CSMA, tal_state, TAL_TX_AUTO, TAL_TX_DONE, and tx_done_handling().
uint8_t last_frame_length |
frame_info_t* mac_frame_ptr |
Frame pointer for the frame structure provided by the MCL.
volatile bool tal_awake_end_flag |
csma_state_t tal_csma_state |
CSMA state machine variable.
uint8_t* tal_frame_to_tx |
Pointer to the 15.4 frame created by the TAL to be handed over to the transceiver.
queue_t tal_incoming_frame_queue |
Queue that contains all frames that are uploaded from the trx, but have not be processed by the MCL yet.
tal_pib_t tal_pib |
buffer_t* tal_rx_buffer = NULL |
Pointer to receive buffer that can be used to upload a frame from the trx.
uint32_t tal_timestamp |
Timestamp The timestamping is only required for beaconing networks or if timestamping is explicitly enabled.