_slave_device_t | The slave device instance |
 A_BLOCK_LINK | |
 address_field_t | MAC Address type |
 aes_config | AES Configuration structure |
 afec_ch_config | AFEC channel configuration structure |
 afec_config | Analog-Front-End Controller configuration structure |
 afec_temp_sensor_config | AFEC Temperature Sensor configuration structure |
 app_payload_t | Application payload frame structure |
 AppCmdHeader_t | |
 AppCmdIdentify_t | |
 AppCmdPendingTableEntry_t | |
 AppCmdUartHeader_t | |
 AppCmdUartIdentify_t | |
 AppMessage_t | |
 archnames | |
 at25_cmd | SerialFlash transfers request prepared by the AT25 driver |
 block_status | |
 BLOCKING_QUEUE_PARAMETERS | |
 bmpfile_header | BMP (Windows) Header Format |
 BoardStatus | |
 can_bit_timing_t | |
 can_mb_conf_t | Define the struct for CAN message mailbox |
 chipid_data | Definition for chip id register data struct |
 chipidtype | Chip ID catalog information: Type ID and its description stream |
 cmcc_config | CMCC Configuration structure |
 corCoRoutineControlBlock | |
 COUNT_SEM_STRUCT | |
 crc_set_req_t | CRC set request frame structure to change the peer node's CRC settings |
 crc_set_rsp_t | CRC set response frame structure to send the status of crc_set_req |
 crc_stat_req_t | CRC status request frame structure to request the peer node's CRC settings |
 crc_stat_rsp_t | CRC status response frame structure to send the peer node's CRC settings |
 data_pkt_range_test_t | Data packet frame structure to send data in Range Measurement mode |
 DIR | |
 div_set_req_t | Antenna Diversity set request frame structure to change the peer node's antenna diversity settings |
 div_set_rsp_t | Antenna Diversity set response frame structure to send the status of div_set_req |
 div_stat_req_t | Antenna Diversity status request frame structure to request the peer node's antenna diversity settings |
 div_stat_rsp_t | Antenna Diversity status response frame structure to send the peer node's antenna diversity settings |
 dma_transfer_descriptor_t | DMA transfer descriptor structure, otherwise known as a Linked List Item (LLI) |
 ed_scan_result_t | ED scan result structure to hold the channel and its ED value |
 ethernetif | Helper struct to hold private data used to operate your ethernet interface |
 FATFS | |
 fifo_desc | FIFO descriptor used by FIFO driver |
 FIL | |
 FILINFO | |
 font | Font structure |
 frame_info_tag | Globally used frame information structure |
 frame_payload_t | General Command frame payload type |
 fs_file | |
 fsdata_file | |
 fsdata_file_noconst | |
 fsk_tag | |
 genclk_config | Hardware representation of a set of generic clock parameters |
 general_pkt_t | Union of all request and and response structures |
 gmac_dev_mem | GMAC device memory management struct |
 gmac_device | GMAC driver structure |
 gmac_options | Input parameters when initializing the gmac module mode |
 gmac_rx_descriptor | Receive buffer descriptor struct |
  gmac_rx_addr | |
   gmac_rx_addr_bm | |
  gmac_rx_status | |
   gmac_rx_status_bm | |
 gmac_tx_descriptor | Transmit buffer descriptor struct |
  gmac_tx_status | |
   gmac_tx_status_bm | |
 gts_char_tag | |
 HeapRegion | |
 http_state | |
 HttpCGI | |
 hx8347a_opt_t | Input parameters when initializing HX8347A driver |
 icmp6_echo_hdr | This is the ICMP6 header adapted for echo req/resp |
 icmp6_hdr | This is the standard ICMP6 header |
 icmp_echo_hdr | This is the standard ICMP header only that the u32_t data is split to two u16_t like ICMP echo needs it |
 ili9325_font | Font structure |
 ili9325_opt_t | Input parameters when initializing ili9325 driver |
 ili93xx_font | Font structure |
 ili93xx_opt_t | Input parameters when initializing ili9325 driver |
 in_addr | For compatibility with BSD code |
 ip_addr | |
 ip_addr2 | |
 ip_addr_packed | |
 ip_globals | |
 ip_hdr | |
 ip_pcb | |
 ksz8851snl_device | Ksz8851snl driver structure |
 leg_oqpsk_tag | |
 mac_assoc_req_tag | Association Request type |
 mac_assoc_response_tag | Association Response type |
 mac_beacon_payload_tag | Beacon Payload type |
 mac_coord_realign_tag | Coordinator Realignment type |
 mac_data_payload_tag | Data Payload type |
 mac_dev_gts_mgmt_tag | Device GTS table structure |
 mac_disassoc_req_tag | Disassociation Request type |
 mac_gts_desc_tag | |
 mac_gts_list_tag | |
 mac_gts_spec_tag | |
 mac_pan_gts_mgmt_tag | PANC GTS table structure |
 mac_pib_tag | |
 mcps_data_conf_tag | This is the MCPS-DATA.confirm message structure |
 mcps_data_ind_tag | This is the MCPS-DATA.indication message structure |
 mcps_data_req_tag | This is the MCPS-DATA.request message structure |
 mcps_purge_conf_tag | This is the MCPS-PURGE.confirm message structure |
 mcps_purge_req_tag | This is the MCPS-PURGE.request message structure |
 mem | The heap is made up as a list of structs of this type |
 membag | Internal structure used by membag to keep track of memory, with maximum 32 blocks per membag |
 memp | |
 mlme_associate_conf_tag | This is the MLME-ASSOCIATE.confirm message structure |
 mlme_associate_ind_tag | This is the MLME-ASSOCIATE.indication message structure |
 mlme_associate_req_tag | This is the MLME-ASSOCIATE.request message structure |
 mlme_associate_resp_tag | This is the MLME-ASSOCIATE.response message structure |
 mlme_beacon_notify_ind_tag | This is the MLME-BEACON-NOTIFY.indication message structure |
 mlme_comm_status_ind_tag | This is the MLME-COMM-STATUS.indication message structure |
 mlme_disassociate_conf_tag | This is the MLME-DISASSOCIATE.confirm message structure |
 mlme_disassociate_ind_tag | This is the MLME-DISASSOCIATE.indication message structure |
 mlme_disassociate_req_tag | This is the MLME-DISASSOCIATE.request message structure |
 mlme_get_conf_tag | This is the MLME-GET.confirm message structure |
 mlme_get_req_tag | This is the MLME-GET.request message structure |
 mlme_gts_conf_tag | This is the MLME-GTS.confirm message structure |
 mlme_gts_ind_tag | This is the MLME-GTS.indication message structure |
 mlme_gts_req_tag | This is the MLME-GTS.request message structure |
 mlme_orphan_ind_tag | This is the MLME-ORPHAN.indication message structure |
 mlme_orphan_resp_tag | This is the MLME-ORPHAN.response message structure |
 mlme_poll_conf_tag | This is the MLME-POLL.confirm message structure |
 mlme_poll_req_tag | This is the MLME-POLL.request message structure |
 mlme_reset_conf_tag | This is the MLME-RESET.confirm message structure |
 mlme_reset_req_tag | This is the MLME-RESET.request message structure |
 mlme_rx_enable_conf_tag | This is the MLME-RX-ENABLE.confirm message structure |
 mlme_rx_enable_req_tag | This is the MLME-RX-ENABLE.request message structure |
 mlme_scan_conf_tag | This is the MLME-SCAN.confirm message structure |
 mlme_scan_req_tag | This is the MLME-SCAN.request message structure |
 mlme_set_conf_tag | This is the MLME-SET.confirm message structure |
 mlme_set_req_tag | This is the MLME-SET.request message structure |
 mlme_start_conf_tag | This is the MLME-START.confirm message structure |
 mlme_start_req_tag | This is the MLME-START.request message structure |
 mlme_sync_loss_ind_tag | This is the MLME-SYNC-LOSS.indication message structure |
 mlme_sync_req_tag | This is the MLME-SYNC.request message structure |
 mr_oqpsk_tag | |
 nand_flash_ecc | NAND Flash ECC layer is called by upper layer, it will call the raw layer to do write/read operations, and do ECC check to the write/read result, it then will feedback the ECC check result to the upper layer |
 nand_flash_management | |
 nand_flash_map | |
 nand_flash_model | |
 nand_flash_raw | The raw NAND Flash layer drives hardware-specific Bus Read and Bus Write operations to communicate with the NAND Flash device |
 nand_flash_spare_scheme | |
 nand_flash_translation | |
 netbuf | |
 netif | Generic data structure used for all lwIP network interfaces |
 new_phy_tag | |
 node_ib_t | Structure to holds the information base for the node |
 NWK_DataInd_t | |
 NWK_DataReq_t | |
 NwkCommandAck_t | |
 NwkCommandRouteError_t | |
 NwkCommandRouteReply_t | |
 NwkCommandRouteRequest_t | |
 NwkDuplicateRejectionEntry_t | |
 NwkFrame_t | |
 NwkFrameHeader_t | |
 NwkFrameMulticastHeader_t | |
 NwkIb_t | |
 ofdm_tag | |
 oqpsk_tag | |
 param_value_t | Parameter value types |
 parse_tag | |
 pbuf | |
 pdc_packet | PDC data packet for transfer |
 peer_conf_t | Peer confirm frame structure used in Peer Search process |
 peer_info_rsp_t | Peer information response frame structure to send the peer details |
 peer_req_t | Peer request frame structure used in Peer Search process |
 peer_rsp_t | Peer response frame structure used in Peer Search process |
 peer_search_receptor_arg_t | Structure to hold the peer device's short address and ieee address |
 peer_state_function_t | Structure to hold the the function pointers to handle various Peer Search Process tasks |
 PHY_DataInd_t | |
 phy_mode_tag | PHY mode structure |
 phy_tag | |
 pll_config | Hardware-specific representation of PLL configuration |
 print_event_msg_t | Print event message stucture to organize the prints |
 pwm_channel_t | Input parameters when configuring a PWM channel mode |
 pwm_clock_t | Input parameters when initializing PWM |
 qt_setup_block | Definitions for AT42QT2160 setup block |
 qt_status | Structure for QT2160 device-status, include: |
 QueueDefinition | |
 range_tx_t | |
 rate_tag | |
 remote_test_req_t | Remote Test Start Request Structure |
 result_req_t | Result request frame structure to request the results of the PER test |
 result_rsp_t | Result response frame structure to send the results of the PER test |
 rtouch_calibration_point_struct | Storage structure for calibration point (actual and raw positions) |
 rtouch_calibration_points_struct | Collection of the five calibration points required to compute calibration |
 rtouch_event_struct | User touch event structure |
 rtouch_point_struct | Point definition |
 sam_uart_opt | Option list for UART peripheral initialization |
 sam_usart_opt_t | Micro definition for LIN mode of SAMV71 |
 sbc_caching_mode_page | SBC-2 Caching mode page |
 sbc_rdwr_error_recovery_mode_page | SBC-2 Read-Write Error Recovery mode page |
 sbc_read_capacity10_data | SBC-2 READ CAPACITY (10) parameter data |
 sbc_slba_block_desc | SBC-2 Short LBA mode parameter block descriptor |
 scan_result_list_t | Union to force alignment of variable portion of scan confirm with wpan_pandescriptor_t |
 scsi_inquiry_data | SCSI Standard Inquiry data structure |
 scsi_mode_page_0_header | SCSI Page_0 Mode Page header (SPF not set) |
 scsi_mode_param_header10 | SCSI Mode Parameter Header used by MODE SELECT(10) and MODE SENSE(10) |
 scsi_mode_param_header6 | SCSI Mode Parameter Header used by MODE SELECT(6) and MODE SENSE(6) |
 scsi_request_sense_data | SCSI Standard Request sense data structure |
 sd_mmc_card | SD/MMC card information structure |
 sec_ctrl_tag | Structure containing auxiliary security header information |
 SEMAPHORE_PARAMETERS | |
 set_param_cb_t | Structure used for updating the parameters after sending them to peer |
 set_parm_req_t | Set paramter Request frame structure to set the the parameters like channel on peer node |
 sn65hvd234_ctrl_t | |
 spc_control_page_info_execpt | SPC-2 Informational exceptions control page See chapter 8.3.8 |
 spi_device | Polled SPI device definition |
 sswt_cb | Struct used for sys_sem_wait_timeout() to tell wether the time has run out or the semaphore has really become available |
 state_function_t | This structure forms the jump table to address various main states in this application |
 status_block_t | |
 StructCPtr | Structure of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers |
 StructCVPtr | Structure of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers |
 StructPtr | Structure of pointers to 64-, 32-, 16- and 8-bit unsigned integers |
 StructVPtr | Structure of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers |
 sun_phy_mode_tag | |
 sun_phy_tag | |
 sys_timeo | |
 sys_timeouts | |
 SYS_Timer_t | |
 tal_pib_tag | |
 tc_qdec_config | TC QDEC configuration structure |
 tc_qdec_pins_config | Configuration struct for the TCC module output pins |
 tc_qdec_results | TC QDEC configuration structure |
 tcpip_msg | |
 test_case | A test case |
 test_suite | A test suite |
 TimeoutlistPerThread | |
 timers_info | Timer for calling lwIP tmr functions without system |
 trx_config_params_t | Structure to hold all configurable parameter values |
 tskTaskControlBlock | |
 twi_options | Input parameters when initializing the TWI module mode |
 twi_packet | Information concerning the data transmission |
 uart_rs232_options | Input parameters when initializing RS232 and similar modes |
 udc_config_speed_t | Configuration descriptor and UDI link for one USB speed |
 udc_config_t | All information about the USB Device |
 udc_desc_t | Structure for USB Device Configuration Descriptor |
 udc_string_desc_t | USB device string descriptor Structure used to transfer ASCII strings to USB String descriptor structure |
 udd_ctrl_request_t | Global variable to give and record information of the setup request management |
 udi_api_t | UDI API |
 udi_cdc_comm_desc_t | Communication Class interface descriptor |
 udi_cdc_data_desc_t | Data Class interface descriptor |
 udi_hid_generic_desc_t | Interface descriptor structure for HID generic |
 udi_hid_generic_report_desc_t | Report descriptor for HID generic |
 udi_hid_kbd_desc_t | Interface descriptor structure for HID keyboard |
 udi_hid_kbd_report_desc_t | Report descriptor for HID keyboard |
 udi_hid_mouse_desc_t | Interface descriptor structure for HID mouse |
 udi_hid_mouse_report_desc_t | Report descriptor for HID mouse |
 udi_hid_multi_touch_desc_t | Interface descriptor structure for HID multi-touch |
 udi_hid_multi_touch_report_desc_t | Report descriptor for HID multi-touch |
 udi_msc_desc_t | Interface descriptor structure for MSC |
 udi_phdc_desc_t | |
 udi_phdc_fnctext_desc_t | |
 udi_phdc_metadata_t | |
 udi_vendor_desc_t | Interface descriptor structure for vendor Class interface |
 Union16 | 16-bit union |
 Union32 | 32-bit union |
 Union64 | 64-bit union |
 UnionCPtr | Union of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers |
 UnionCVPtr | Union of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers |
 UnionPtr | Union of pointers to 64-, 32-, 16- and 8-bit unsigned integers |
 UnionVPtr | Union of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers |
 usart_iso7816_opt_t | |
 usart_spi_device | Polled SPI device definition |
 usart_spi_opt_t | |
 usb_association_desc_t | Standard USB Interface Association Descriptor structure |
 usb_cdc_acm_desc_t | CDC ACM Functional Descriptor |
 usb_cdc_call_mgmt_desc_t | CDC Call Management Functional Descriptor |
 usb_cdc_control_signal_t | Control signal structure |
 usb_cdc_hdr_desc_t | CDC Header Functional Descriptor |
 usb_cdc_line_coding_t | Line Coding structure |
 usb_cdc_notify_msg_t | |
 usb_cdc_notify_serial_state_t | Hardware handshake support (cdc spec 1.1 chapter 6.3.5) |
 usb_cdc_union_desc_t | CDC Union Functional Descriptor |
 usb_conf_desc_t | Standard USB configuration descriptor structure |
 usb_dev_bos_desc_t | USB Device BOS descriptor structure |
 usb_dev_capa_ext_desc_t | USB Device Capabilities - USB 2.0 Extension Descriptor structure |
 usb_dev_desc_t | Standard USB device descriptor structure |
 usb_dev_lpm_desc_t | USB Device LPM Descriptor structure |
 usb_dev_qual_desc_t | Standard USB device qualifier descriptor structure |
 usb_ep_desc_t | Standard USB endpoint descriptor structure |
 usb_hid_descriptor_t | HID Descriptor |
 usb_iad_desc_t | Standard USB association descriptor structure |
 usb_iface_desc_t | Standard USB interface descriptor structure |
 usb_msc_cbw | |
 usb_msc_csw | |
 usb_phdc_classfnct_desc_t | PHDC Class Function Descriptor |
 usb_phdc_fnctext_desc_t | PHDC Function Extension Descriptor Note: The wDevSpecializations fields must follow this struct |
 usb_phdc_fnctext_singlespec_desc_t | PHDC Function Extension Descriptor with single specification |
 usb_phdc_meta_data_1_desc_t | |
 usb_phdc_meta_data_desc_t | PHDC Meta-Data Descriptor Note: The optional meta-data field (0 to 253B) can follow this struct |
 usb_phdc_metadata_msg_1_t | |
 usb_phdc_metadata_msg_t | PHDC Meta-Data Message Note: The optional meta-data field (0 to EPx_size-21) can follow this struct |
 usb_phdc_qos_desc_t | PHDC QoS Descriptor |
 usb_setup_req_t | A USB Device SETUP request |
 usb_str_desc_t | A standard USB string descriptor structure |
 usb_str_lgid_desc_t | |
 waveconfig_t | [tc_capture_selection] |
 wpan_addr_spec_tag | Device address specification structure |
 wpan_pandescriptor_tag | PAN descriptor information structure |
 xCOMMAND_INPUT_LIST | |
 xCOMMAND_LINE_INPUT | |
 xEventGroupDefinition | |
 xLIST | |
 xLIST_ITEM | |
 xMEMORY_REGION | |
 xMINI_LIST_ITEM | |
 xRTOS_HEAP | |
 xSTATIC_EVENT_GROUP | |
 xSTATIC_LIST | |
 xSTATIC_LIST_ITEM | |
 xSTATIC_MINI_LIST_ITEM | |
 xSTATIC_QUEUE | |
 xSTATIC_STREAM_BUFFER | |
 xSTATIC_TCB | |
 xSTATIC_TIMER | |
 xSTREAM_BUFFER | |
 xTASK_PARAMETERS | |
 xTASK_PARAMTERS | |
 xTASK_STATUS | |
 xTIME_OUT | |