Structure for QT2160 device-status, include:
* * QtStatus[0] - General Status * bit0 - SDET : This bit is set if a touch is detected on the slider. * bit1 - CC : This Common Change bit is set if all the selected * keys have a signal change of more than half the * detection threshold, NTHR. * bit6 - CYCLE OVERRUN : This bit is set if the cycle time more than 16ms. * bit7 - RESET : This bit is set after a reset * * QtStatus[1] - Key Status * bits 0 - 7 : Detect status for keys 0 to 7 (Touched keys report as 1) * * QtStatus[2] - Key Status * bits 0 - 7 : Detect status for keys 8 to 15 (Touched keys report as 1) * * QtStatus[3] - Slider Touch Position * bits 0 - 7 : Last position of the touch on the slider * * QtStatus[4] - GPIO Read * bits 2 - 4 : indicates the state of GPIO1 to GPIO3 * that are configured as inputs * *
#include <QT2160.h>
Data Fields | |
uint8_t | general_status |
General Status. More... | |
uint8_t | gpio_read |
GPIO Read. More... | |
uint8_t | key_status_1 |
Key Status 1. More... | |
uint8_t | key_status_2 |
Key Status 2. More... | |
uint8_t | slider_position |
Slider Touch Position. More... | |
uint8_t qt_status::general_status |
General Status.
Referenced by demo_process_qt_status().
uint8_t qt_status::gpio_read |
GPIO Read.
uint8_t qt_status::key_status_1 |
Key Status 1.
uint8_t qt_status::key_status_2 |
Key Status 2.
uint8_t qt_status::slider_position |
Slider Touch Position.
Referenced by demo_process_qt_status().