Microchip® Advanced Software Framework

freertos-7.3.0/source/portable/memmang/heap_4.c File Reference
#include <stdlib.h>
#include "../../include/FreeRTOS.h"
#include "../../include/task.h"

Data Structures

struct  A_BLOCK_LINK
 
union  xRTOS_HEAP
 

Macros

#define heapMINIMUM_BLOCK_SIZE   ( ( size_t ) ( heapSTRUCT_SIZE * 2 ) )
 
#define MPU_WRAPPERS_INCLUDED_FROM_API_FILE
 

Typedefs

typedef struct A_BLOCK_LINK xBlockLink
 

Functions

static void prvHeapInit (void)
 
static void prvInsertBlockIntoFreeList (xBlockLink *pxBlockToInsert)
 
void * pvPortMalloc (size_t xWantedSize)
 
void vApplicationMallocFailedHook (void)
 
void vPortFree (void *pv)
 
void vPortInitialiseBlocks (void)
 
size_t xPortGetFreeHeapSize (void)
 

Variables

static const unsigned short heapSTRUCT_SIZE = ( sizeof( xBlockLink ) + portBYTE_ALIGNMENT - ( sizeof( xBlockLink ) % portBYTE_ALIGNMENT ) )
 
static xBlockLinkpxEnd = NULL
 
static size_t xFreeBytesRemaining = ( ( size_t ) configTOTAL_HEAP_SIZE ) & ( ( size_t ) ~portBYTE_ALIGNMENT_MASK )
 
static union xRTOS_HEAP xHeap
 
static xBlockLink xStart
 
static const size_t xTotalHeapSize = ( ( size_t ) configTOTAL_HEAP_SIZE ) & ( ( size_t ) ~portBYTE_ALIGNMENT_MASK )
 

#define heapMINIMUM_BLOCK_SIZE   ( ( size_t ) ( heapSTRUCT_SIZE * 2 ) )

Referenced by pvPortMalloc().

#define MPU_WRAPPERS_INCLUDED_FROM_API_FILE

typedef struct A_BLOCK_LINK xBlockLink

static void prvHeapInit ( void  )
static
static void prvInsertBlockIntoFreeList ( xBlockLink pxBlockToInsert)
static
void vApplicationMallocFailedHook ( void  )

vApplicationMallocFailedHook() will only be called if configUSE_MALLOC_FAILED_HOOK is set to 1 in FreeRTOSConfig.h. It is a hook function that will get called if a call to pvPortMalloc() fails. pvPortMalloc() is called internally by the kernel whenever a task, queue, timer or semaphore is created. It is also called by various parts of the demo application. If heap_1.c or heap_2.c are used, then the size of the heap available to pvPortMalloc() is defined by configTOTAL_HEAP_SIZE in FreeRTOSConfig.h, and the xPortGetFreeHeapSize() API function can be used to query the size of free heap space that remains (although it does not provide information on how the remaining heap might be fragmented).

vApplicationMallocFailedHook() will only be called if configUSE_MALLOC_FAILED_HOOK is set to 1 in FreeRTOSConfig.h. It is a hook function that will get called if a call to pvPortMalloc() fails. pvPortMalloc() is called internally by the kernel whenever a task, queue, timer or semaphore is created. It is also called by various parts of the demo application. If heap_1.c or heap_2.c are used, then the size of the heap available to pvPortMalloc() is defined by configTOTAL_HEAP_SIZE in FreeRTOSConfig.h, and the xPortGetFreeHeapSize() API function can be used to query the size of free heap space that remains (although it does not provide information on how the remaining heap might be fragmented).

vApplicationMallocFailedHook() will only be called if configUSE_MALLOC_FAILED_HOOK is set to 1 in FreeRTOSConfig.h. It is a hook function that will get called if a call to pvPortMalloc() fails. pvPortMalloc() is called internally by the kernel whenever a task, queue, timer or semaphore is created. It is also called by various parts of the demo application. If heap_1.c or heap_2.c are used, then the size of the heap available to pvPortMalloc() is defined by configTOTAL_HEAP_SIZE in FreeRTOSConfig.h, and the xPortGetFreeHeapSize() API function can be used to query the size of free heap space that remains (although it does not provide information on how the remaining heap might be fragmented).

Referenced by pvPortMalloc().

void vPortInitialiseBlocks ( void  )
size_t xPortGetFreeHeapSize ( void  )

const unsigned short heapSTRUCT_SIZE = ( sizeof( xBlockLink ) + portBYTE_ALIGNMENT - ( sizeof( xBlockLink ) % portBYTE_ALIGNMENT ) )
static
xBlockLink * pxEnd = NULL
static
size_t xFreeBytesRemaining = ( ( size_t ) configTOTAL_HEAP_SIZE ) & ( ( size_t ) ~portBYTE_ALIGNMENT_MASK )
static

Referenced by xPortGetFreeHeapSize().

union xRTOS_HEAP xHeap
static

Referenced by prvHeapInit().

xBlockLink xStart
static

Referenced by pvPortMalloc().

const size_t xTotalHeapSize = ( ( size_t ) configTOTAL_HEAP_SIZE ) & ( ( size_t ) ~portBYTE_ALIGNMENT_MASK )
static